This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User |
Registered User |
||
Line 7: | Line 7: | ||
STM32CubeProgrammer is the '''official''' STMicroelectronics tool '''to download firmware into STMicroelectronics boards'''. | STM32CubeProgrammer is the '''official''' STMicroelectronics tool '''to download firmware into STMicroelectronics boards'''. | ||
==STM32CubeProgrammer - Version v2. | ==STM32CubeProgrammer - Version v2.13.0== | ||
<onlyinclude> | <onlyinclude> | ||
{| class="st-table" width=98% | {| class="st-table" width=98% | ||
Line 15: | Line 15: | ||
| '''Download''' | | '''Download''' | ||
| colspan="2" | | | colspan="2" | | ||
'''Version v2. | '''Version v2.13.0''' | ||
* Browse [https://www.st.com/en/development-tools/stm32cubeprog.html here] link and follow instructions to download the package, you need a myST account. | * Browse [https://www.st.com/en/development-tools/stm32cubeprog.html here] link and follow instructions to download the package, you need a myST account. | ||
* Download the archive file on your host PC in a temporary directory | * Download the archive file on your host PC in a temporary directory | ||
Line 28: | Line 28: | ||
* Execute the Linux installer, which guides you through the installation process. | * Execute the Linux installer, which guides you through the installation process. | ||
<pre>$> ./SetupSTM32CubeProgrammer-2. | <pre>$> ./SetupSTM32CubeProgrammer-2.13.0.linux</pre> | ||
* The path to the STM32CubeProgrammer binary must be added to the PATH environment variable | * The path to the STM32CubeProgrammer binary must be added to the PATH environment variable | ||
** either in each Terminal program in which the STM32CubeProgrammer binary needs to be used, using the following command: | ** either in each Terminal program in which the STM32CubeProgrammer binary needs to be used, using the following command: |
Latest revision as of 12:53, 14 March 2023
STM32CubeProgrammer is the official STMicroelectronics tool to download firmware into STMicroelectronics boards.
1. STM32CubeProgrammer - Version v2.13.0[edit source]
STM32CubeProgrammer for Linux® host PC | STM32CubeProgrammer for Windows® host PC | |
---|---|---|
Download |
Version v2.13.0
| |
Installation |
$> ./SetupSTM32CubeProgrammer-2.13.0.linux
$> export PATH=<my STM32CubeProgrammer install directory>/bin:$PATH
$> ln -s <my STM32CubeProgrammer install directory>/bin/STM32_Programmer_CLI /home/bin/STM32_Programmer_CLI
|
|
User manual |
| |
Detailed release note |
|