Registered User mNo edit summary |
Registered User mNo edit summary |
||
Line 4: | Line 4: | ||
}}</noinclude> | }}</noinclude> | ||
== STM32MPU Embedded Software overview == | == STM32MPU Embedded Software overview == | ||
The diagram below shows [[STM32MPU Embedded Software distribution]] main components: | The diagram below shows [[:Category:STM32MPU_Embedded_Software_distribution|STM32MPU Embedded Software distribution]] main components: | ||
* The '''OpenSTLinux distribution''', running on the Arm<sup>®</sup> Cortex<sup>®</sup>-A, including: | * The '''OpenSTLinux distribution''', running on the Arm<sup>®</sup> Cortex<sup>®</sup>-A, including: | ||
** The '''OpenSTLinux BSP''' with: | ** The '''OpenSTLinux BSP''' with: |
Latest revision as of 11:55, 14 February 2023
1. STM32MPU Embedded Software overview[edit source]
The diagram below shows STM32MPU Embedded Software distribution main components:
- The OpenSTLinux distribution, running on the Arm® Cortex®-A, including:
- The OpenSTLinux BSP with:
- The boot chain based on TF-A and U-Boot.
- The OP-TEE secure OS running on the Arm® Cortex®-A in secure mode.
- The Linux® kernel running on the Arm® Cortex®-A in non-secure mode.
- The Linux middleware relies on the BSP to provide API to the Applications that typically interact with the user via the display, the touchscreen, etc.
- On OP-TEE side, the Trusted Applications (TA) relies on the OP-TEE core for secrets operations (not visible from the Linux and STM32Cube MPU Package)
- The OpenSTLinux BSP with:
- The STM32Cube MPU Package is running on the Arm® Cortex®-M, and so only available on STM32MP15x lines
: it is based on HAL drivers and middlewares, like STM32 microcontrollers, completed with coprocessor management for interaction with the Cortex-A.
The OpenSTLinux distribution is generated with OpenEmbedded build framework : the BSP components are modified open source software components, stored on github, whereas the middleware is directly inherited from communities. See our Open Source Software (OSS) philosophy just below for further information.
The figure below is clickable so that the user can directly jump to one of the sub-levels listed above.


- STM32CubeMP1 architecture
- OP-TEE overview
- TF-A overview
- U-Boot overview
- STM32 MPU Linux kernel overview
- Boot chain overview
- Linux application frameworks overview
- OpenSTLinux BSP architecture overview
- OpenSTLinux architecture overview
- Category:Platform configuration
- Security overview
- Arm Cortex-A7
- Arm Cortex-M4
- STM32MP13 microprocessor
- STM32MP15 microprocessor
2. Open Source Software (OSS) philosophy[edit source]
The Open source software source code is released under a license in which the copyright holder grants users the rights to study, change and distribute the software to anyone and for any purpose[1].
STMicroelectronics maximizes the using of open source software and contributes to those communities. Notice that, due to the software review life cycle, it can take some time before getting all developments accepted in the communities, so STMicroelectronics can also temporarily provide some source code on github[2], until it is merged in the targeted repository.
3. References[edit source]