Registered User mNo edit summary |
Registered User |
||
Line 12: | Line 12: | ||
== Local streaming == | == Local streaming == | ||
Here is an example of a local preview involving [[V4l2-ctl]] for JPEG pictures capture and [[Gst-play|gst-play]] GStreamer player for JPEG decoding and display. JPEG pictures are sent over a standard Linux pipe. | Here is an example of a local preview involving [[V4l2-ctl]] for JPEG pictures capture and [[Gst-play|gst-play]] GStreamer player for JPEG decoding and display. JPEG pictures are sent over a standard Linux pipe. | ||
{{Warning | If Weston is configured with a "weston" user instead of a "root" user, please use the following command: | |||
{{Board$}} su -l "weston" -c "your_weston_command" | |||
}} | |||
<br> | <br> |
Latest revision as of 18:18, 9 June 2022
1. Overview[edit source]
This article will explain how to stream camera content over network thanks to GStreamer application on top of V4L2 Linux® kernel framework.
Capturing compressed JPEG pictures is an efficient way to send camera images to any local or remote player; JPEG pictures require a limited bandwidth while being fully interoperable.
Find below some examples of command lines allowing to capture a continuous JPEG stream while playing it using various multimedia players, either local or remote.
2. Local streaming[edit source]
Here is an example of a local preview involving V4l2-ctl for JPEG pictures capture and gst-play GStreamer player for JPEG decoding and display. JPEG pictures are sent over a standard Linux pipe.
ExpandFor STM32MP135 line ![]() |
Capture JPEG pictures then decode & display them:
--stream-to=- 2>/dev/null | gst-play-1.0 "fd://0"v4l2-ctl --set-parm=30;v4l2-ctl --set-fmt-video=width=640,height=480,pixelformat=JPEG --stream-mmap --stream-count=-1
--stream-to=- tells V4l2-ctl to output binary captured content to standard output, which is then sent to pipe |.
Special URI fd://0 tells gst-play GStreamer player to read data from the pipe.
Note the 2>/dev/null right after the V4l2-ctl command to remove the logs from console output.
3. UDP streaming[edit source]
An internet connection is required, for example by plugging an ethernet cable on the:
STM32MP135x-DK Discovery kit ![]() |
CN4 Ethernet connector 1 or CN15 Ethernet connector 2 |
STM32MP157x-DKx Discovery kit ![]() |
CN8 Ethernet connector |
STM32MP157x-EV1 Evaluation board ![]() |
CN3 Ethernet connector |
ExpandFor STM32MP135 line ![]() |
Get the IP address aa.bb.cc.dd of the host PC using ifconfig command:
aa.bb.cc.dd Bcast:10.201.23.255 Mask:255.255.252.0 inet addr:127.0.0.1 Mask:255.0.0.0ifconfig | grep "inet addr" inet addr:
Then fill the host= udpsink property with this IP address on the remote side:
host=aa.bb.cc.dd port=5000v4l2-ctl --set-parm=30;v4l2-ctl --set-fmt-video=width=640,height=480,pixelformat=JPEG --stream-mmap --stream-count=-1 --stream-to=- 2>/dev/null | gst-launch-1.0 fdsrc ! jpegparse ! rtpjpegpay ! udpsink
Then play the UDP stream on host PC:
gst-launch-1.0 udpsrc port=5000 ! application/x-rtp, encoding-name=JPEG ! rtpjpegdepay ! jpegparse ! decodebin ! videoconvert ! autovideosink
A new window will popup on host PC displaying the camera content.