Registered User |
Registered User |
||
(10 intermediate revisions by 6 users not shown) | |||
Line 1: | Line 1: | ||
<noinclude> | <noinclude>{{ApplicableFor | ||
{{ | |MPUs list=STM32MP13x, STM32MP15x | ||
|MPUs checklist=STM32MP13x,STM32MP15x | |||
}}</noinclude> | |||
</noinclude> | |||
__TOC__ | __TOC__ | ||
Line 32: | Line 30: | ||
=== Initialize WLAN interface === | === Initialize WLAN interface === | ||
{{Board$}} ifconfig wlan0 192.168.43.135 broadcast 192.168.43.255 netmask 255.255.255.0 | |||
{{Board$}} ifconfig wlan0 up | {{Board$}} ifconfig wlan0 up | ||
{{Board$}} ifconfig wlan0 | |||
wlan0 Link encap:Ethernet HWaddr 60:F1:89:3F:F6:0E | wlan0 Link encap:Ethernet HWaddr 60:F1:89:3F:F6:0E | ||
inet addr:192.168.43.135 Bcast:192.168.43.255 Mask:255.255.255.0 | inet addr:192.168.43.135 Bcast:192.168.43.255 Mask:255.255.255.0 | ||
Line 109: | Line 111: | ||
* VI: CW 7-15, AIFSN 2, TXOP 3008 usec | * VI: CW 7-15, AIFSN 2, TXOP 3008 usec | ||
* VO: CW 3-7, AIFSN 2, TXOP 1504 usec | * VO: CW 3-7, AIFSN 2, TXOP 1504 usec | ||
== Automatic WiFi configuration at start up == | |||
===networkctl=== | |||
Systemd has a specific service for the network named '''systemd-networkd''', this service comes with the tool '''networkctl''' which allows to show the status of each network interface. | |||
{{Board$}} networkctl --no-pager | |||
IDX LINK TYPE OPERATIONAL SETUP | |||
1 lo loopback carrier unmanaged | |||
2 eth0 ether routable configured | |||
3 sit0 sit no-carrier unmanaged | |||
4 ip6tnl0 tunnel6 no-carrier unmanaged | |||
5 wlan0 wlan no-carrier unmanaged | |||
6 wlan1 wlan no-carrier unmanaged | |||
6 links listed. | |||
We can see that the '''eth0''' interface is managed by networked via the information '''configured''' and the interface is used ('''routable'''). | |||
===How to set a wireless configuration with networkd=== | |||
The goal is to configure an wlan network interface via systemd-networkd configuration. <br/> | |||
All the network configurations are stored on '''/lib/systemd/network''' or '''/etc/systemd/network''' <br/> | |||
Create the file dedicated to wireless interface "/lib/systemd/network/51-wireless.network" : | |||
{{Board$}} echo "[Match]" > /lib/systemd/network/51-wireless.network | |||
{{Board$}} echo "Name=wlan0" >> /lib/systemd/network/51-wireless.network | |||
{{Board$}} echo "[Network]" >> /lib/systemd/network/51-wireless.network | |||
{{Board$}} echo "DHCP=ipv4" >> /lib/systemd/network/51-wireless.network | |||
Check content is as follow | |||
{{Board$}} cat /lib/systemd/network/51-wireless.network | |||
[Match] | |||
Name=wlan0 | |||
[Network] | |||
DHCP=ipv4 | |||
For attaching this wireless interface to a specific network, we need to have some information like SSID of network and password.<br/> | |||
To see the list of wireless network available: | |||
{{Board$}} ifconfig wlan0 up | |||
{{Board$}} iw dev wlan0 scan |grep SSID | |||
SSID: NETWORK1 | |||
SSID: NETWORK2 | |||
Associate the wireless network to wireless interface, here wlan0: | |||
{{Board$}} mkdir -p /etc/wpa_supplicant/ | |||
echo "ctrl_interface=/var/run/wpa_supplicant" > /etc/wpa_supplicant/wpa_supplicant-wlan0.conf | |||
echo "eapol_version=1" >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf | |||
echo "ap_scan=1" >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf | |||
echo "fast_reauth=1" >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf | |||
echo "" >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf | |||
wpa_passphrase SSID_OF_NETWORK PASSWORD_OF_NETWORK >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf | |||
Where '''SSID_OF_NETWORK''' '''PASSWORD_OF_NETWORK''' correspond to the SSID and password of wireless network.<br/> | |||
{{Info|the name of file on /etc/wpa_supplicant must contains the name of wireless interface: wpa_supplicant-'''wlan0'''.conf}} | |||
<br/> | |||
To enable and start the wireless configuration: | |||
{{Board$}} systemctl enable wpa_supplicant@wlan0.service | |||
systemctl restart systemd-networkd.service | |||
systemctl restart wpa_supplicant@wlan0.service | |||
== Wlan Network attachment (without system which manage systemd-networkd configuration) == | == Wlan Network attachment (without system which manage systemd-networkd configuration) == | ||
{{Warning| dhclient is not available in the OpenSTLinux because system.networkd already inbeds a dhcp client. On OSTL, it is recommended to follow the chapter #Automatic_WiFi_configuration_at_start_up}} | |||
=== Configure your WiFi connection === | === Configure your WiFi connection === | ||
Configure WiFi connection by using '''wpa_supplicant''' tool | Configure WiFi connection by using '''wpa_supplicant''' tool | ||
Line 186: | Line 253: | ||
* Note : Enter <CTRL+C> to terminate the ping session. | * Note : Enter <CTRL+C> to terminate the ping session. | ||
<noinclude> | |||
[[Category:WLAN]] | |||
{{PublicationRequestId | 10175 | 2019-01-07 |AlainF}} | |||
</noinclude> | |||
< | |||
Latest revision as of 18:23, 11 April 2023
Even if the example is related to the RTL8723BU chip (this chip calls for a WiFi (minimally 802.11g/n) and Bluetooth 4.0 LE), most of the commands are generic ones and can be applied to any platform.
1. ifconfig[edit source]
Verify the wlan0 interface is present (that means drivers have been started and the WiFi firmware loaded):
1.1. Check WLAN interface[edit source]
RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)ifconfig -a lo Link encap:Local Loopback LOOPBACK MTU:65536 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:1 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:0 (0.0 B) TX bytes:10 (10.0 B)wlan0 Link encap:Ethernet HWaddr 60:F1:89:3F:F6:0E BROADCAST MULTICAST MTU:1500 Metric:1
1.2. Initialize WLAN interface[edit source]
ifconfig wlan0 192.168.43.135 broadcast 192.168.43.255 netmask 255.255.255.0
ifconfig wlan0 up
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 /* UP indicate that your interface is UP */ RX packets:19 errors:0 dropped:0 overruns:0 frame:0 TX packets:19 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:1774 (1.7 KiB) TX bytes:2326 (2.2 KiB)ifconfig wlan0 wlan0 Link encap:Ethernet HWaddr 60:F1:89:3F:F6:0E inet addr:192.168.43.135 Bcast:192.168.43.255 Mask:255.255.255.0
2. iw[edit source]
The next phase is to scan for any wireless access points with the command:
2.1. Scan available SSID (AP)[edit source]
- Get only SSID name
iw dev wlan0 scan |grep SSID
SSID: NETWORK1
SSID: NETWORK2
- List full SSID information
iw dev wlan0 scan
BSS 00:23:5e:4a:28:f9(on wlan0)
TSF: 0 usec (0d, 00:00:00)
freq: 2412
beacon interval: 100 TUs
capability: ESS ShortPreamble ShortSlotTime (0x0421)
signal: -72.00 dBm
last seen: 0 ms ago
SSID: NETWORK1
Supported rates: 1.0* 2.0* 5.5* 6.0 9.0 11.0* 12.0 18.0
DS Parameter set: channel 1
TIM: DTIM Count 0 DTIM Period 1 Bitmap Control 0x0 Bitmap[0] 0x2
Country: FR Environment: Indoor/Outdoor
Channels [1 - 13] @ 20 dBm
BSS Load:
* station count: 1
* channel utilisation: 30/255
* available admission capacity: 23437 [*32us]
ERP: <no flags>
Extended supported rates: 24.0 36.0 48.0 54.0
WMM: * Parameter version 1
* u-APSD
* BE: CW 15-1023, AIFSN 3
* BK: CW 15-1023, AIFSN 7
* VI: CW 7-15, AIFSN 2, TXOP 3008 usec
* VO: CW 3-7, AIFSN 2, TXOP 1504 usec
BSS 00:23:5e:96:57:20(on wlan0)
TSF: 0 usec (0d, 00:00:00)
freq: 2412
beacon interval: 100 TUs
capability: ESS Privacy ShortPreamble ShortSlotTime (0x0431)
signal: -66.00 dBm
last seen: 0 ms ago
SSID: NETWORK2
Supported rates: 1.0* 2.0* 5.5* 6.0 9.0 11.0* 12.0 18.0
DS Parameter set: channel 1
Country: FR Environment: Indoor/Outdoor
Channels [1 - 13] @ 20 dBm
BSS Load:
* station count: 8
* channel utilisation: 48/255
* available admission capacity: 23437 [*32us]
ERP: <no flags>
RSN: * Version: 1
* Group cipher: CCMP
* Pairwise ciphers: CCMP
* Authentication suites: IEEE 802.1X 00-40-96:0
* Capabilities: 4-PTKSA-RC 4-GTKSA-RC (0x0028)
Extended supported rates: 24.0 36.0 48.0 54.0
WMM: * Parameter version 1
* u-APSD
* BE: CW 15-1023, AIFSN 3
* BK: CW 15-1023, AIFSN 7
* VI: CW 7-15, AIFSN 2, TXOP 3008 usec
* VO: CW 3-7, AIFSN 2, TXOP 1504 usec
3. Automatic WiFi configuration at start up[edit source]
3.1. networkctl[edit source]
Systemd has a specific service for the network named systemd-networkd, this service comes with the tool networkctl which allows to show the status of each network interface.
networkctl --no-pager
IDX LINK TYPE OPERATIONAL SETUP
1 lo loopback carrier unmanaged
2 eth0 ether routable configured
3 sit0 sit no-carrier unmanaged
4 ip6tnl0 tunnel6 no-carrier unmanaged
5 wlan0 wlan no-carrier unmanaged
6 wlan1 wlan no-carrier unmanaged
6 links listed.
We can see that the eth0 interface is managed by networked via the information configured and the interface is used (routable).
3.2. How to set a wireless configuration with networkd[edit source]
The goal is to configure an wlan network interface via systemd-networkd configuration.
All the network configurations are stored on /lib/systemd/network or /etc/systemd/network
Create the file dedicated to wireless interface "/lib/systemd/network/51-wireless.network" :
DHCP=ipv4" >> /lib/systemd/network/51-wireless.networkecho "[Match]" > /lib/systemd/network/51-wireless.network echo "Name=wlan0" >> /lib/systemd/network/51-wireless.network echo "[Network]" >> /lib/systemd/network/51-wireless.network echo "
Check content is as follow
DHCP=ipv4cat /lib/systemd/network/51-wireless.network [Match] Name=wlan0 [Network]
For attaching this wireless interface to a specific network, we need to have some information like SSID of network and password.
To see the list of wireless network available:
ifconfig wlan0 up
iw dev wlan0 scan |grep SSID
SSID: NETWORK1
SSID: NETWORK2
Associate the wireless network to wireless interface, here wlan0:
mkdir -p /etc/wpa_supplicant/
echo "ctrl_interface=/var/run/wpa_supplicant" > /etc/wpa_supplicant/wpa_supplicant-wlan0.conf
echo "eapol_version=1" >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf
echo "ap_scan=1" >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf
echo "fast_reauth=1" >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf
echo "" >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf
wpa_passphrase SSID_OF_NETWORK PASSWORD_OF_NETWORK >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf
Where SSID_OF_NETWORK PASSWORD_OF_NETWORK correspond to the SSID and password of wireless network.
To enable and start the wireless configuration:
systemctl enable wpa_supplicant@wlan0.service
systemctl restart systemd-networkd.service
systemctl restart wpa_supplicant@wlan0.service
4. Wlan Network attachment (without system which manage systemd-networkd configuration)[edit source]
4.1. Configure your WiFi connection[edit source]
Configure WiFi connection by using wpa_supplicant tool
- Check current configuration
cat /etc/wpa_supplicant.conf
ctrl_interface=/var/run/wpa_supplicant
ctrl_interface_group=0
update_config=1
network={
key_mgmt=NONE
}
- Set the WiFi network name and password
wpa_passphrase <your_ssid_name> <your_ssid_key> >> /etc/wpa_supplicant.conf
- Check new configuration
psk="your_ssid_key" }cat /etc/wpa_supplicant.conf ctrl_interface=/var/run/wpa_supplicant ctrl_interface_group=0 update_config=1 network={ ssid="your_ssid_name"
4.1.1. Connect to SSID[edit source]
wpa_supplicant -B -iwlan0 -c /etc/wpa_supplicant.conf
Successfully initialized wpa_supplicant
4.1.2. link to SSID[edit source]
RX: 501 bytes (3 packets) TX: 4056 bytes (22 packets) signal: -75 dBm tx bitrate: 12.0 MBit/s bss flags: short-preamble short-slot-time dtim period: 1 beacon int: 100iw wlan0 link SSID: NETWORK1 freq: 2462
4.1.3. Assign IP address to WLAN interface[edit source]
Use the DHCP client to obtain an address (assuming wireless network (associated to) has a DHCP server):
dhclient wlan0
Use the ip command to verify the IP address assigned by the DHCP. The IP address is 192.168.43.135 from below.
UP qlen 1000 link/ether 74:e5:43:a1:ce:65 brd ff:ff:ff:ff:ff:ff inet 192.168.43.135/24 brd 192.168.1.255 scope global wlan0 inet6 fe80::76e5:43ff:fea1:ce65/64 scope link valid_lft forever preferred_lft foreverip addr show wlan0 3: wlan0: mtu 1500 qdisc mq state
4.1.4. Check connectivity[edit source]
The most basic connectivity test is to use the “ping” command. In this example, the wireless router (associated to) has an IP address of 192.168.43.1:
ping 192.168.43.1
PING 192.168.43.1 (192.168.43.1): 56 data bytes
64 bytes from 192.168.43.1: seq=0 ttl=64 time=14.905 ms
64 bytes from 192.168.43.1: seq=1 ttl=64 time=30.387 ms
64 bytes from 192.168.43.1: seq=2 ttl=64 time=20.462 ms
- Note : Enter <CTRL+C> to terminate the ping session.