Registered User mNo edit summary |
Registered User mNo edit summary |
||
(One intermediate revision by one other user not shown) | |||
Line 1: | Line 1: | ||
<noinclude>{{ApplicableFor | |||
|MPUs list=STM32MP13x, STM32MP15x | |||
|MPUs checklist=STM32MP13x, STM32MP15x | |||
}}</noinclude> | |||
== Article purpose == | == Article purpose == | ||
This article explains how the Arm<sup>®</sup> TrustZone<sup>®</sup> execution context is used for on an STM32 MPU-based platform.<br> | This article explains how the Arm<sup>®</sup> TrustZone<sup>®</sup> execution context is used for on an STM32 MPU-based platform.<br> | ||
== Introduction == | == Introduction == | ||
The STM32 MPU is based on the Arm<sup>®</sup> Cortex<sup>®</sup>-A core, which is using the Arm<sup>®</sup> TrustZone<ref>https://www.arm.com/why-arm/technologies/trustzone-for-cortex-a</ref> architecture that enables context isolation: the '''normal world''' holds the applications whereas the '''secure world''' isolates all the trusted applications and core secure services so that they can safely manipulate platform secret data. The MPU includes | The STM32 MPU is based on the Arm<sup>®</sup> Cortex<sup>®</sup>-A core, which is using the Arm<sup>®</sup> TrustZone<ref>https://www.arm.com/why-arm/technologies/trustzone-for-cortex-a</ref> architecture that enables context isolation: the '''normal world''' holds the applications whereas the '''secure world''' isolates all the trusted applications and core secure services so that they can safely manipulate platform secret data. The MPU includes firewall mechanisms that allow the secure world to forbid read/write accesses from the normal world to given peripherals.<br> | ||
Arm-v7A defines PL0, PL1 and PL2 privilege levels: | Arm-v7A defines PL0, PL1 and PL2 privilege levels: | ||
Line 14: | Line 19: | ||
{{ReviewsComments | [[User:Ludovic Bergonzi|Ludovic Bergonzi]] ([[User talk:Ludovic Bergonzi|talk]]) 19:25, 13 November 2022 (CET) <br /> In the figure, consider using fewer capital letters: "Normal world", "Secure world", "Trusted applications", Secure monitor", "TrustZone<sup>®</sup> environment".}} | {{ReviewsComments | [[User:Ludovic Bergonzi|Ludovic Bergonzi]] ([[User talk:Ludovic Bergonzi|talk]]) 19:25, 13 November 2022 (CET) <br /> In the figure, consider using fewer capital letters: "Normal world", "Secure world", "Trusted applications", Secure monitor", "TrustZone<sup>®</sup> environment".}} | ||
The '''normal world''' is used to run rich OSs such as the [[STM32 MPU Linux kernel overview|Linux<sup>®</sup> kernel]] and its [[Linux application frameworks overview|applications framework]].<br> | The '''normal world''' is used to run rich OSs such as the [[STM32 MPU Linux kernel overview|Linux<sup>®</sup> kernel]] and its [[Linux application frameworks overview|applications framework]].<br> | ||
The '''secure world''' runs a TEE as the secure OS (for example [[ | The '''secure world''' runs a TEE as the secure OS (for example [[OP-TEE_overview|OP-TEE OS]]), including a secure monitor. | ||
The TrustZone environment is a complete system solution that is not limited to the Cortex<sup>®</sup> context. It provides a bus and peripheral infrastructure to the MPU to ensure that the secure world relies on a completely secured pipe when it controls a secure peripheral. The assignment of the peripherals to a given world is done through a | The TrustZone environment is a complete system solution that is not limited to the Cortex<sup>®</sup> context. It provides a bus and peripheral infrastructure to the MPU to ensure that the secure world relies on a completely secured pipe when it controls a secure peripheral. The assignment of the peripherals to a given world is done through a firewall mechanism, which is set up during the secure world initialization. | ||
Dedicated secure and normal contexts also impact the debugging facilities: depending on the targeted user, the debug can be opened to both worlds (for instance for a secure-aware developer), to the normal world only (for a Linux<sup>®</sup> developer), or completely closed (for the end user). This is achieved by configuring the | Dedicated secure and normal contexts also impact the debugging facilities: depending on the targeted user, the debug can be opened to both worlds (for instance for a secure-aware developer), to the normal world only (for a Linux<sup>®</sup> developer), or completely closed (for the end user). This is achieved by configuring the debug control. | ||
Some internal or external peripherals can be used by the secure world to support cryptographic operations | Some internal or external peripherals can be used by the secure world to support cryptographic operations. | ||
== References == | == References == |
Latest revision as of 18:19, 30 January 2023
1. Article purpose[edit source]
This article explains how the Arm® TrustZone® execution context is used for on an STM32 MPU-based platform.
2. Introduction[edit source]
The STM32 MPU is based on the Arm® Cortex®-A core, which is using the Arm® TrustZone[1] architecture that enables context isolation: the normal world holds the applications whereas the secure world isolates all the trusted applications and core secure services so that they can safely manipulate platform secret data. The MPU includes firewall mechanisms that allow the secure world to forbid read/write accesses from the normal world to given peripherals.
Arm-v7A defines PL0, PL1 and PL2 privilege levels:
- PL0 is the lowest software execution level (unprivileged calls allowed for applications).
- PL1 is the execution level for the OS.
- PL1 (secure) is also the privilege level for secure monitor execution, to switch from the secure to the normal world.
- PL2 is dedicated to the hypervisor (only non-secure).
The normal world is used to run rich OSs such as the Linux® kernel and its applications framework.
The secure world runs a TEE as the secure OS (for example OP-TEE OS), including a secure monitor.
The TrustZone environment is a complete system solution that is not limited to the Cortex® context. It provides a bus and peripheral infrastructure to the MPU to ensure that the secure world relies on a completely secured pipe when it controls a secure peripheral. The assignment of the peripherals to a given world is done through a firewall mechanism, which is set up during the secure world initialization.
Dedicated secure and normal contexts also impact the debugging facilities: depending on the targeted user, the debug can be opened to both worlds (for instance for a secure-aware developer), to the normal world only (for a Linux® developer), or completely closed (for the end user). This is achieved by configuring the debug control.
Some internal or external peripherals can be used by the secure world to support cryptographic operations.
3. References[edit source]