Registered User mNo edit summary |
Registered User mNo edit summary |
||
(17 intermediate revisions by 4 users not shown) | |||
Line 3: | Line 3: | ||
|MPUs checklist=STM32MP13x,STM32MP15x | |MPUs checklist=STM32MP13x,STM32MP15x | ||
}}</noinclude> | }}</noinclude> | ||
==Article purpose== | ==Article purpose== | ||
This article introduces the Linux<sup>®</sup> | This article introduces the Linux<sup>®</sup>, U-Boot and OP-TEE drivers for the [[ADC_internal_peripheral|ADC internal peripheral]]. It answers the following questions: | ||
* Which ADC features are supported by the driver | * Which ADC features are supported by the driver. | ||
* How to configure, use and debug the driver | * How to configure, use and debug the driver. | ||
* What is the driver structure, and where the source code can be found. | * What is the driver structure, and where the source code can be found. | ||
== Short description == | == Short description == | ||
The ADC internal peripheral is supported in Linux | The ADC internal peripheral is supported in Linux, U-boot and OP-TEE software components through dedicated drivers. Refer to [[ADC_internal_peripheral|ADC internal peripheral]] to know the actual support of an ADC particular instance, depending on STM32 MPU device and execution context (here U-Boot, OP-TEE or Linux context). | ||
===U-Boot driver === | ===U-Boot driver === | ||
The U-Boot driver is based on the adc-uclass framework. This framework offers an API <ref name="stm32mp151_dtsi">{{CodeSource | U-Boot | include/adc.h | U-Boot adc API}}</ref> which can be used to implement ADC client applications. | The U-Boot driver is based on the adc-uclass framework. This framework offers an API <ref name="stm32mp151_dtsi">{{CodeSource | U-Boot | include/adc.h | U-Boot adc API}}</ref> which can be used to implement ADC client applications. | ||
</br> | </br> | ||
The U-Boot driver supports one shot conversions in single and scan modes. It uses poll mechanism to monitor the end of ADC conversions, interrupts or DMA being not supported. | The U-Boot driver supports one shot conversions in single and scan modes. It uses poll mechanism to monitor the end of ADC conversions, interrupts, or DMA being not supported. | ||
===OP-TEE driver === | |||
This chapter is only applicable for '''{{EcosystemRelease | revision=4.1.0 | range=and after}}''' with {{MicroprocessorDevice | device=13}}. | |||
The OP-TEE driver is based on the OP-TEE ADC framework. This framework offers an API which can be used to implement ADC client applications.</br> | |||
The OP-TEE driver supports one shot or repetitive conversions in single and scan modes. The ADC watchdogs can be configured and enabled, to trigger tamper signals, in given voltage ranges. | |||
It uses a poll mechanism to monitor the end of ADC conversions, interrupts or DMA being not supported. | |||
===Linux kernel driver === | ===Linux kernel driver === | ||
The ADC Linux<sup>®</sup> driver (kernel space) is based on the [[IIO overview|IIO framework]].</br> | The ADC Linux<sup>®</sup> driver (kernel space) is based on the [[IIO overview|IIO framework]].</br> | ||
It supports two modes: | It supports two modes: | ||
# '''IIO direct mode''': single capture on a channel (using interrupts) | # '''IIO direct mode''': single capture on a channel (using interrupts). | ||
# '''IIO triggered buffer mode''': capture on one or more channels (preferably using DMA).<br/>It uses the hardware triggers available in IIO. See [[TIM Linux driver]] and [[LPTIM Linux driver]] for more details. | # '''IIO triggered buffer mode''': capture on one or more channels (preferably using DMA).<br/>It uses the hardware triggers available in IIO. See [[TIM Linux driver]] and [[LPTIM Linux driver]] for more details. | ||
Line 34: | Line 40: | ||
* '''Linear calibration''' ({{MicroprocessorDevice | device=15}} only) | * '''Linear calibration''' ({{MicroprocessorDevice | device=15}} only) | ||
The linear calibration is SoC dependent. This calibration is time consuming and does not change over time because it is | The linear calibration is SoC dependent. This calibration is time consuming and does not change over time because it is not voltage or temperature dependent. It can be then done only once, on first boot. | ||
{{Info| To minimize clock and voltage disturbances, the linear calibration is performed in U-Boot, when there is a minimal CPU activity. The ADC is kept active during the handover between U-Boot and Linux kernel, which allows the ADC Linux driver to retrieve the linear calibration factors from the ADC registers.}} | {{Info| To minimize clock and voltage disturbances, the linear calibration is performed in U-Boot, when there is a minimal CPU activity. The ADC is kept active during the handover between U-Boot and Linux kernel, which allows the ADC Linux driver to retrieve the linear calibration factors from the ADC registers.}} | ||
Line 65: | Line 71: | ||
[*] adc - Access Analog to Digital Converters info and data | [*] adc - Access Analog to Digital Converters info and data | ||
</pre> | </pre> | ||
===OP-TEE configuration === | |||
This chapter is only applicable for '''{{EcosystemRelease | revision=4.1.0 | range=and after}}''' with {{MicroprocessorDevice | device=13}}. | |||
The ADC OP-TEE driver can be activated by enabling the build directives CFG_DRIVERS_ADC (ADC framework) and CFG_STM32_ADC (STM32 ADC driver). | |||
Refer to [[How_to_configure_OP-TEE | How to configure OP-TEE]] article for details on OP-TEE configuration. | |||
===Linux kernel configuration === | ===Linux kernel configuration === | ||
The | The ADC Linux driver can be activated in the kernel configuration using the Linux [[Menuconfig or how to configure kernel|Menuconfig tool]] (enable both CONFIG_STM32_ADC_CORE and CONFIG_STM32_ADC). | ||
<pre> | <pre> | ||
Device Drivers ---> | Device Drivers ---> | ||
Line 77: | Line 90: | ||
===Device tree === | ===Device tree === | ||
Refer to the [[ADC device tree configuration]] article where the configuration of ADC Linux kernel | Refer to the [[ADC device tree configuration]] article where the configuration of ADC Linux kernel, OP-TEE and U-boot drivers is explained. | ||
==How to use== | ==How to use== | ||
===U-Boot driver=== | ===U-Boot driver=== | ||
The | The analog-to-digital converters information and data can be accessed through the ADC command line tool. For that, the command line interface must be enabled in U-Boot configuration. This interface makes use of U-Boot ADC API <ref name="stm32mp151_dtsi">{{CodeSource | U-Boot | include/adc.h | U-Boot adc API}}</ref>. | ||
{{Board$}} {{highlight|adc}} | {{Board$}} {{highlight|adc}} | ||
Line 89: | Line 102: | ||
adc single <name> <channel> - Get Single data of ADC device channel | adc single <name> <channel> - Get Single data of ADC device channel | ||
adc scan <name> [channel mask] - Scan all [or masked] ADC channels | adc scan <name> [channel mask] - Scan all [or masked] ADC channels | ||
===OP-TEE driver=== | |||
This chapter is only applicable for '''{{EcosystemRelease | revision=4.1.0 | range=and after}}''' with {{MicroprocessorDevice | device=13}}. | |||
An application using ADC services, needs to register itself as a consumer of ADC channels, as shown in example Device Tree below. | |||
adc_consumer { | |||
compatible = "adc-consumer"; | |||
io-channels = <&adc2 14>, <&adc2 16>; {{highlight|/* Consumer of adc2 channels 14 & 16 */}} | |||
}; | |||
The corresponding consumer device can use the OP-TEE ADC framework API <ref name="adc optee api">{{CodeSource | OP-TEE_OS | core/include/drivers/adc.h | OP-TEE ADC framework API}}</ref>, to configure the ADC and launch conversions, as shown in code sample below. | |||
<pre> | |||
static TEE_Result adc_consumer_probe(const void *fdt, int node, const void *compat_data __unused) | |||
{ | |||
struct adc_consumer **cons = NULL; | |||
... | |||
adc_consumer_get_all(fdt, node, &nb_cons, &cons); | |||
for (i = 0; i < nb_cons; i++) | |||
adc_consumer_read_processed(cons[i], &mv); | |||
... | |||
} | |||
static const struct dt_device_match adc_consumer_match_table[] = { | |||
{ .compatible = "adc-consumer" }, | |||
}; | |||
</pre> | |||
===Linux kernel driver === | ===Linux kernel driver === | ||
Line 109: | Line 148: | ||
adc48003000_lincalfact3=1ff7e9b8 | adc48003000_lincalfact3=1ff7e9b8 | ||
... | ... | ||
===In OP-TEE=== | |||
This chapter is only applicable for '''{{EcosystemRelease | revision=4.1.0 | range=and after}}'''. | |||
Refer to [[How_to_debug_OP-TEE | How to debug OP-TEE]] for details about debug means in OP-TEE. | |||
===In Linux kernel === | ===In Linux kernel === | ||
Line 130: | Line 174: | ||
adc12 1 1 0 196607910 0 0 | adc12 1 1 0 196607910 0 0 | ||
* '''regulator'''<ref name="Regulator overview">[[Regulator overview]]</ref> tree and usage can be verified ( | * '''regulator'''<ref name="Regulator overview">[[Regulator overview]]</ref> tree and usage can be verified (for example, use count, open count or regulator reference voltage) as follows: | ||
{{Board$}} {{highlight|cat /sys/kernel/debug/regulator/regulator_summary}} | {{Board$}} {{highlight|cat /sys/kernel/debug/regulator/regulator_summary}} | ||
regulator use open bypass voltage current min max | regulator use open bypass voltage current min max | ||
Line 159: | Line 203: | ||
===U-Boot === | ===U-Boot === | ||
The ADC source code is composed of: | The ADC source code is composed of: | ||
* {{CodeSource | U-Boot | drivers | * {{CodeSource | U-Boot | drivers/adc/stm32-adc-core.c | stm32-adc-core driver}} to handle common resources such as clock (selection, prescaler), [[Regulator overview|regulator]] used as reference voltage, interrupt and common registers. | ||
* {{CodeSource | U-Boot | drivers/adc/stm32-adc.c | stm32-adc driver}} to handle the resources available for each ADC such as channel configuration. | * {{CodeSource | U-Boot | drivers/adc/stm32-adc.c | stm32-adc driver}} to handle the resources available for each ADC such as channel configuration. | ||
===OP-TEE driver=== | |||
This chapter is only applicable for '''{{EcosystemRelease | revision=4.1.0 | range=and after}}'''. | |||
The ADC source code is composed of: | |||
* {{CodeSource | OP-TEE_OS | core/drivers/adc/stm32_adc_core.c | stm32_adc_core driver}} to handle common resources such as clock (selection, prescaler), regulator used as reference voltage and common registers. | |||
* {{CodeSource | OP-TEE_OS | core/drivers/adc/stm32_adc.c | stm32_adc driver}} to handle the resources available for each ADC such as calibration and channel configuration. | |||
===Linux kernel === | ===Linux kernel === | ||
The ADC source code is composed of: | The ADC source code is composed of: | ||
* {{CodeSource | Linux kernel | drivers/iio/adc/stm32-adc-core.c | stm32-adc-core driver}} to handle common resources such as clock (selection, prescaler), [[Regulator overview|regulator]] used as reference voltage, interrupt and common registers. | * {{CodeSource | Linux kernel | drivers/iio/adc/stm32-adc-core.c | stm32-adc-core driver}} to handle common resources such as clock (selection, prescaler), [[Regulator overview|regulator]] used as reference voltage, interrupt, and common registers. | ||
* {{CodeSource | Linux kernel | drivers/iio/adc/stm32-adc.c | stm32-adc driver}} to handle the resources available for each ADC such as channel configuration and buffer handling. | * {{CodeSource | Linux kernel | drivers/iio/adc/stm32-adc.c | stm32-adc driver}} to handle the resources available for each ADC such as channel configuration and buffer handling. | ||
Line 172: | Line 223: | ||
<noinclude> | <noinclude> | ||
[[Category:IIO]] | [[Category:IIO]] | ||
{{PublicationRequestId | 9337 | {{PublicationRequestId | 24108| 2022-07-27 |9337 - 2018-10-23 - AnneJ}} | ||
{{ArticleBasedOnModel | OpenSTLinux drivers article model}} | {{ArticleBasedOnModel | OpenSTLinux drivers article model}} | ||
</noinclude> | </noinclude> |
Latest revision as of 10:50, 2 December 2022
1. Article purpose[edit source]
This article introduces the Linux®, U-Boot and OP-TEE drivers for the ADC internal peripheral. It answers the following questions:
- Which ADC features are supported by the driver.
- How to configure, use and debug the driver.
- What is the driver structure, and where the source code can be found.
2. Short description[edit source]
The ADC internal peripheral is supported in Linux, U-boot and OP-TEE software components through dedicated drivers. Refer to ADC internal peripheral to know the actual support of an ADC particular instance, depending on STM32 MPU device and execution context (here U-Boot, OP-TEE or Linux context).
2.1. U-Boot driver[edit source]
The U-Boot driver is based on the adc-uclass framework. This framework offers an API [1] which can be used to implement ADC client applications.
The U-Boot driver supports one shot conversions in single and scan modes. It uses poll mechanism to monitor the end of ADC conversions, interrupts, or DMA being not supported.
2.2. OP-TEE driver[edit source]
This chapter is only applicable for ecosystem release ≥ unknown revision 4.1.0 with STM32MP13x lines
.
The OP-TEE driver is based on the OP-TEE ADC framework. This framework offers an API which can be used to implement ADC client applications.
The OP-TEE driver supports one shot or repetitive conversions in single and scan modes. The ADC watchdogs can be configured and enabled, to trigger tamper signals, in given voltage ranges.
It uses a poll mechanism to monitor the end of ADC conversions, interrupts or DMA being not supported.
2.3. Linux kernel driver[edit source]
The ADC Linux® driver (kernel space) is based on the IIO framework.
It supports two modes:
- IIO direct mode: single capture on a channel (using interrupts).
- IIO triggered buffer mode: capture on one or more channels (preferably using DMA).
It uses the hardware triggers available in IIO. See TIM Linux driver and LPTIM Linux driver for more details.
2.4. Calibration handover between U-Boot and Linux kernel drivers[edit source]
This chapter is only applicable for ecosystem release ≥ v4.0.0 .
The U-boot and Linux kernel drivers implement calibration support to improve the ADC accuracy. The recommendations to enhance ADC accuracy can be found in the application note AN2834. The ADC internal peripheral offers two kind of calibration:
- Offset calibration
This calibration is fast and may vary over time depending on voltage and temperature variations. The offset single-ended and differential calibration is performed on each boot in U-boot driver, and each time, new conversions are launched in the Linux kernel driver.
The linear calibration is SoC dependent. This calibration is time consuming and does not change over time because it is not voltage or temperature dependent. It can be then done only once, on first boot.
3. Configuration[edit source]
3.1. U-Boot configuration[edit source]
The ADC U-Boot driver can be activated in the U-Boot configuration using the U-Boot Menuconfig tool (enable CONFIG_STM32_ADC).
ADC driverDevice Drivers ---> [*] Enable STMicroelectronics STM32
The ADC command line interface can be activated by enabling CMD_ADC flag.
Command line interface --->
Device access commands --->
[*] adc - Access Analog to Digital Converters info and data
3.2. OP-TEE configuration[edit source]
This chapter is only applicable for ecosystem release ≥ unknown revision 4.1.0 with STM32MP13x lines
.
The ADC OP-TEE driver can be activated by enabling the build directives CFG_DRIVERS_ADC (ADC framework) and CFG_STM32_ADC (STM32 ADC driver).
Refer to How to configure OP-TEE article for details on OP-TEE configuration.
3.3. Linux kernel configuration[edit source]
The ADC Linux driver can be activated in the kernel configuration using the Linux Menuconfig tool (enable both CONFIG_STM32_ADC_CORE and CONFIG_STM32_ADC).
Device Drivers --->
<*> Industrial I/O support --->
Analog to digital converters --->
<*> STMicroelectronics STM32 adc core
<*> STMicroelectronics STM32 adc
3.4. Device tree[edit source]
Refer to the ADC device tree configuration article where the configuration of ADC Linux kernel, OP-TEE and U-boot drivers is explained.
4. How to use[edit source]
4.1. U-Boot driver[edit source]
The analog-to-digital converters information and data can be accessed through the ADC command line tool. For that, the command line interface must be enabled in U-Boot configuration. This interface makes use of U-Boot ADC API [1].
adc Usage: adc list - list ADC devices adc info <name> - Get ADC device info adc single <name> <channel> - Get Single data of ADC device channel adc scan <name> [channel mask] - Scan all [or masked] ADC channels
4.2. OP-TEE driver[edit source]
This chapter is only applicable for ecosystem release ≥ unknown revision 4.1.0 with STM32MP13x lines
.
An application using ADC services, needs to register itself as a consumer of ADC channels, as shown in example Device Tree below.
/* Consumer of adc2 channels 14 & 16 */ };adc_consumer { compatible = "adc-consumer"; io-channels = <&adc2 14>, <&adc2 16>;
The corresponding consumer device can use the OP-TEE ADC framework API [2], to configure the ADC and launch conversions, as shown in code sample below.
TEE_Result adc_consumer_probe(const void *fdt, int node, const void *compat_data __unused) { struct adc_consumer **cons = NULL; ... adc_consumer_get_all(fdt, node, &nb_cons, &cons); for (i = 0; i < nb_cons; i++) adc_consumer_read_processed(cons[i], &mv); ... } static const struct dt_device_match adc_consumer_match_table[] = { { .compatible = "adc-consumer" }, };static
4.3. Linux kernel driver[edit source]
In "IIO direct mode", the conversion result can be read directly from sysfs (refer to How to do a simple ADC conversion using the sysfs interface).
In "IIO triggered buffer mode", the configuration must be performed using sysfs first. Then, character device (/dev/iio:deviceX) is used to read data (refer to Convert one or more channels using triggered buffer mode).
5. How to trace and debug[edit source]
5.1. In U-Boot[edit source]
Refer to U-Boot - How to debug for details about debug means in U-Boots.
- Linear calibration factors for ecosystem release ≥ v4.0.0
The ADC linear calibration factors are saved as persistent environment variables named "adc<addr>_lincalfact<index>". These variables can be displayed through the printenv command (STM32MP15x lines only):
printenv adc48003000_lincalfact1=1fe80602 adc48003000_lincalfact2=1da7c9ff adc48003000_lincalfact3=1ff7e9b8 ...
5.2. In OP-TEE[edit source]
This chapter is only applicable for ecosystem release ≥ unknown revision 4.1.0 .
Refer to How to debug OP-TEE for details about debug means in OP-TEE.
5.3. In Linux kernel[edit source]
Refer to How to trace with dynamic debug for how to enable the debug logs in the driver and in the framework.
Refer to How to debug with debugfs for how to access information on ADC driver.
The ADC has system wide dependencies towards other key resources:
- runtime power management can be disabled, for example it may be forced on via power/control sysfs entry:
ADC device after autosuspend_delay_ms echo on > power/control # force the kernel to resume the ADC device (e.g. keep clocks and regulators enabled)cd /sys/devices/platform/soc/48003000.adc/48003000.adc:adc@0 cat power/autosuspend_delay_ms 2000 cat power/control auto # kernel is allowed to automatically suspend the
- clock[3] usage can be verified by reading clk_summary:
cat /sys/kernel/debug/clk/clk_summary | grep adc adc12_k 1 1 0 24000000 0 0 adc12 1 1 0 196607910 0 0
- regulator[4] tree and usage can be verified (for example, use count, open count or regulator reference voltage) as follows:
cat /sys/kernel/debug/regulator/regulator_summary regulator use open bypass voltage current min max ------------------------------------------------------------------------------- v3v3 4 5 0 3300mV 0mA 3300mV 3300mV vdda 1 2 0 2900mV 0mA 2900mV 2900mV 40017000.dac 0mV 0mV 48003000.adc 0mV 0mV
- pinctrl[5] usage can be verified by reading pinmux-pins:
cat pinmux-pins | grep adc pin 92 (PF12): device 48003000.adc function analog group PF12 # check pin is assigned to ADC and is configured as "analog"cd /sys/kernel/debug/pinctrl/soc\:pin*@50002000/
- interrupts can be verified by reading "interrupts":
cat /proc/interrupts CPU0 CPU1 56: 2 0 dummy 0 Edge 48003000.adc:adc@0
- Linear calibration factors for ecosystem release ≥ v4.0.0
The Linear calibration factors can be checked through debugfs (STM32MP15x lines only):
cat /sys/kernel/debug/iio/iio:device*/lincalfact* 527955453 521648626 ...
6. Source code location[edit source]
6.1. U-Boot[edit source]
The ADC source code is composed of:
- stm32-adc-core driver to handle common resources such as clock (selection, prescaler), regulator used as reference voltage, interrupt and common registers.
- stm32-adc driver to handle the resources available for each ADC such as channel configuration.
6.2. OP-TEE driver[edit source]
This chapter is only applicable for ecosystem release ≥ unknown revision 4.1.0 .
The ADC source code is composed of:
- stm32_adc_core driver to handle common resources such as clock (selection, prescaler), regulator used as reference voltage and common registers.
- stm32_adc driver to handle the resources available for each ADC such as calibration and channel configuration.
6.3. Linux kernel[edit source]
The ADC source code is composed of:
- stm32-adc-core driver to handle common resources such as clock (selection, prescaler), regulator used as reference voltage, interrupt, and common registers.
- stm32-adc driver to handle the resources available for each ADC such as channel configuration and buffer handling.
7. References[edit source]