Registered User mNo edit summary |
Registered User mNo edit summary |
||
(8 intermediate revisions by 4 users not shown) | |||
Line 1: | Line 1: | ||
{{ | <noinclude>{{ApplicableFor | ||
|MPUs list=STM32MP13x, STM32MP15x | |||
|MPUs checklist=STM32MP13x,STM32MP15x | |||
}}</noinclude> | |||
== Article purpose == | == Article purpose == | ||
The purpose of this article is to explain how to configure the ''timer (TIM)''<ref name="TIM internal peripheral"> [[TIM internal peripheral]]</ref> ''' when the peripheral is assigned to Linux<sup>®</sup> OS''': | The purpose of this article is to explain how to configure the ''timer (TIM)''<ref name="TIM internal peripheral"> [[TIM internal peripheral]]</ref> ''' when the peripheral is assigned to Linux<sup>®</sup> OS''': | ||
Line 8: | Line 11: | ||
The configuration is performed using the '''device tree mechanism'''<ref> [[Device tree]]</ref>. | The configuration is performed using the '''device tree mechanism'''<ref> [[Device tree]]</ref>. | ||
It is used by the [[TIM Linux driver]] that registers relevant information in [[PWM overview|PWM]] | It is used by the [[TIM Linux driver]] that registers relevant information in [[PWM overview|PWM]], [[IIO overview|IIO]] and <span style="color: {{STLightBlue}};">counter</span> frameworks. | ||
If the peripheral is assigned to another execution context, refer to [[How to assign an internal peripheral to a runtime context]] article for guidelines on peripheral assignment and configuration. | If the peripheral is assigned to another execution context, refer to [[How to assign an internal peripheral to a runtime context]] article for guidelines on peripheral assignment and configuration. | ||
== DT bindings documentation == | == DT bindings documentation == | ||
The ''TIM internal peripheral''<ref name="TIM internal peripheral"/> is a multifunction device (MFD) | The ''TIM internal peripheral''<ref name="TIM internal peripheral"/> is a multifunction device (MFD), providing several functions represented by a separate compatible string: | ||
* ''st,stm32-timers'' deals with core resources. (e.g. registers, clock, DMAs) | |||
* '' | * ''st,stm32-pwm'' deals with PWM resources. (e.g. PWM input/output pins) | ||
* ''st,stm32-timer-trigger'' deals with trigger resources (e.g. trigger output connected to other STM32 internal peripherals) | |||
* ''st,stm32-timer-counter'' deals with quadrature encoder resources and external events counter. | |||
The required and optional configuration properties of these functions are documented in ''STM32 TIM MFD device tree bindings''<ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/mfd/st,stm32-timers.yaml | Documentation/devicetree/bindings/mfd/mfd/st,stm32-timers.yaml}}</ref> | |||
== DT configuration == | == DT configuration == | ||
Line 46: | Line 47: | ||
}; | }; | ||
timer@'''0''' { | timer@'''0''' { | ||
compatible = "st,stm32h7-timer-trigger"; | compatible = "st,stm32h7-timer-trigger"; | ||
{{highlight|/* trigger identifier (e.g. 0 for TIM1 triggers, 1 for TIM2... */}} | {{highlight|/* trigger identifier (e.g. 0 for TIM1 triggers, 1 for TIM2... */}} | ||
reg = <'''0'''>; | reg = <'''0'''>; | ||
}; | |||
counter { | |||
compatible = "st,stm32-timer-counter"; | |||
}; | }; | ||
}; | }; | ||
Line 67: | Line 70: | ||
The example below shows how to configure '''TIM1 channel 1''' to act as: | The example below shows how to configure '''TIM1 channel 1''' to act as: | ||
* '''PWM output on PE9''', e.g. TIM1_CH1 ([[Pinctrl_device_tree_configuration|See pinctrl device tree configuration]] and [[GPIO internal peripheral]]) | * '''PWM output on PE9''', e.g. TIM1_CH1 ([[Pinctrl_device_tree_configuration|See pinctrl device tree configuration]] and [[GPIO internal peripheral]]) | ||
* PWM device tree provider (e.g. TIM1_CH1) used by a device tree consumer (e.g. like "pwm-leds"<ref name="pwm-leds">{{CodeSource | Linux kernel | Documentation/devicetree/bindings/leds/leds-pwm. | * PWM device tree provider (e.g. TIM1_CH1) used by a device tree consumer (e.g. like "pwm-leds"<ref name="pwm-leds">{{CodeSource | Linux kernel | Documentation/devicetree/bindings/leds/leds-pwm.yaml}}, PWM LEDs device tree bindings</ref>). | ||
{{highlight|/* select TIM1_CH1 alternate function 1 on 'PE9' */}} | {{highlight|/* select TIM1_CH1 alternate function 1 on 'PE9' */}} | ||
Line 203: | Line 206: | ||
==== TIM configured as quadrature encoder interface ==== | ==== TIM configured as quadrature encoder interface ==== | ||
The example below shows how to configure '''TIM1''' to interface with a quadrature encoder: | The example below shows how to configure '''TIM1''' to interface with a quadrature encoder: | ||
* '''Configure PE9 and | * '''Configure PE9 and PE11 as encoder input pins''', e.g. TIM1_CH1, TIM1_CH2 ([[Pinctrl_device_tree_configuration|see pinctrl device tree configuration]] and [[GPIO internal peripheral]]) | ||
{{Info|On the STM32MP157X-DKX discovery board, TIM1_CH1 and TIM1_CH2 signals are accessible via the D6 and D10 pins of the [[STM32MP157x-DKx_-_hardware_description#Arduino_Uno_connector|Arduino Uno connector]].}} | |||
tim1_in_pins_a: tim1-in-pins-0 { | tim1_in_pins_a: tim1-in-pins-0 { | ||
pins { | pins { | ||
pinmux = <STM32_PINMUX('E', 9, AF1)>, /* TIM1_CH1 */ | pinmux = <STM32_PINMUX('E', 9, AF1)>, /* TIM1_CH1 */ | ||
<STM32_PINMUX(' | <STM32_PINMUX('E', 11, AF1)>; /* TIM1_CH2 */ | ||
bias-disable; | bias-disable; | ||
}; | }; | ||
Line 216: | Line 219: | ||
pins { | pins { | ||
pinmux = <STM32_PINMUX('E', 9, ANALOG)>, /* TIM1_CH1 */ | pinmux = <STM32_PINMUX('E', 9, ANALOG)>, /* TIM1_CH1 */ | ||
<STM32_PINMUX(' | <STM32_PINMUX('E', 11, ANALOG)>; /* TIM1_CH2 */ | ||
}; | }; | ||
}; | }; | ||
Line 224: | Line 227: | ||
/delete-property/dmas; {{highlight|/* spare all DMA channels since they are not required for quadrature encoder interface */}} | /delete-property/dmas; {{highlight|/* spare all DMA channels since they are not required for quadrature encoder interface */}} | ||
/delete-property/dma-names; | /delete-property/dma-names; | ||
counter { | |||
pinctrl-0 = <&tim1_in_pins_a>; {{highlight|/* configure TIM1_CH1 and TIM1_CH2 as encoder input pins */}} | pinctrl-0 = <&tim1_in_pins_a>; {{highlight|/* configure TIM1_CH1 and TIM1_CH2 as encoder input pins */}} | ||
pinctrl-1 = <&tim1_in_pins_sleep_a>; | pinctrl-1 = <&tim1_in_pins_sleep_a>; | ||
Line 233: | Line 236: | ||
==How to configure the DT using STM32CubeMX== | ==How to configure the DT using STM32CubeMX== | ||
The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree# | The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree#STM32_MPU|platform configuration device tree]] files.<br /> | ||
The STM32CubeMX may not support all the properties described in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. If so, the tool inserts '''user sections''' in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to [[STM32CubeMX]] user manual for further information. | The STM32CubeMX may not support all the properties described in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. If so, the tool inserts '''user sections''' in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to [[STM32CubeMX]] user manual for further information. | ||
Latest revision as of 16:14, 28 October 2022
1. Article purpose[edit source]
The purpose of this article is to explain how to configure the timer (TIM)[1] when the peripheral is assigned to Linux® OS:
- Configuring the timer peripheral to enable PWM, trigger or quadrature encoder.
- Configuring the board, e.g. TIM pins.
The configuration is performed using the device tree mechanism[2].
It is used by the TIM Linux driver that registers relevant information in PWM, IIO and counter frameworks.
If the peripheral is assigned to another execution context, refer to How to assign an internal peripheral to a runtime context article for guidelines on peripheral assignment and configuration.
2. DT bindings documentation[edit source]
The TIM internal peripheral[1] is a multifunction device (MFD), providing several functions represented by a separate compatible string:
- st,stm32-timers deals with core resources. (e.g. registers, clock, DMAs)
- st,stm32-pwm deals with PWM resources. (e.g. PWM input/output pins)
- st,stm32-timer-trigger deals with trigger resources (e.g. trigger output connected to other STM32 internal peripherals)
- st,stm32-timer-counter deals with quadrature encoder resources and external events counter.
The required and optional configuration properties of these functions are documented in STM32 TIM MFD device tree bindings[3]
3. DT configuration[edit source]
This hardware description is a combination of both STM32 microprocessor and board device tree files. Refer to Device tree for more explanations about device tree file split.
The STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.
3.1. DT configuration (STM32 level)[edit source]
TIM nodes are declared in stm32mp151.dtsi[4].
DT root node (e.g. timers1...) and DT child nodes describe the TIM features such as:
- PWM
- trigger and quadrature encoder
They also describe hardware parameters such as registers address, clock and DMA.
/* timer common resources */ compatible = "st,stm32-timers"; ... pwm { /* PWM*/ compatible = "st,stm32-pwm"; }; timer@0 { compatible = "st,stm32h7-timer-trigger"; /* trigger identifier (e.g. 0 for TIM1 triggers, 1 for TIM2... */ reg = <0>; }; counter { compatible = "st,stm32-timer-counter"; }; };timers1: timer@address {
![]() |
This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user. |
3.2. DT configuration (board level)[edit source]
This part is used to configure and enable the TIM hardware used on the board:
- Enabling DT root node for the TIM instances in use (e.g timers1...) by setting status = "okay";
- Enabling DT child node(s) for the feature(s) in use (PWM input/output, trigger and quadrature encoder) by setting status = "okay";
- Configuring pins in use via pinctrl through pinctrl-0, pinctrl-1 and pinctrl-names.
To enable PWM capture on the board (optional), DMA must be configured:
- Enable DMA channel(s) corresponding to the PWM input(s) by setting dmas = <...>, <...>; and matching dma-names = "ch1", "ch3";.
When PWM capture isn't used, it's recommended to disable DMA channels by default, to spare them for other usage:
- Disable DMA channels by setting /delete-property/dmas and /delete-property/dma-names
3.3. DT configuration examples[edit source]
3.3.1. TIM configured in PWM mode[edit source]
The example below shows how to configure TIM1 channel 1 to act as:
- PWM output on PE9, e.g. TIM1_CH1 (See pinctrl device tree configuration and GPIO internal peripheral)
- PWM device tree provider (e.g. TIM1_CH1) used by a device tree consumer (e.g. like "pwm-leds"[5]).
/* select TIM1_CH1 alternate function 1 on 'PE9' */ pwm1_pins_a: pwm1-0 { pins { pinmux = <STM32_PINMUX('E', 9, AF1)>; bias-pull-down; drive-push-pull; slew-rate = <0>; }; }; /* configure 'PE9' as analog input in low-power mode */ pwm1_sleep_pins_a: pwm1-sleep-0 { pins { pinmux = <STM32_PINMUX('E', 9, ANALOG)>; }; };
File:Info.png | The PWM output doesn't require any DMA channel. Disable them if they are configured by default in the .dtsi file. |
/* PWM DT provider on TIM1: "pwm1" */ &timers1 { status = "okay"; /* spare all DMA channels since they are not needed for PWM output */ /delete-property/dmas; /delete-property/dma-names; /* define pwm1 label */ pwm1: pwm { /* configure PWM pins on TIM1_CH1 */ pinctrl-0 = <&pwm1_pins_a>; pinctrl-1 = <&pwm1_sleep_pins_a>; pinctrl-names = "default", "sleep"; /* enable PWM on TIM1 */ status = "okay"; }; };
- PWM DT user example
File:Info.png | The TIM PWM DT user specifier encodes 3 cells:
|
/* PWM DT user on TIM1_CH1: "pwm1", example with "pwm-leds"[5] */ pwmleds { compatible = "pwm-leds"; example { label = "stm32-pwm-leds-example"; /* Use pwm1 channel 0 (e.g. TIM1_CH1) */ /* period in nanoseconds (500000), normal polarity (0) */ pwms = <&pwm1 0 500000 0>; max-brightness = <127>; }; }; };/ { ...
3.3.2. TIM configured in PWM mode and trigger source[edit source]
The example below shows how to configure TIM1 channel 1 to act as:
- PWM output on PE9, e.g. TIM1_CH1 (See pinctrl device tree configuration and GPIO internal peripheral)
- trigger source (synchronous with PWM) for other internal peripheral such as STM32 ADC
/* select TIM1_CH1 alternate function 1 on 'PE9' */ pwm1_pins_a: pwm1-0 { pins { pinmux = <STM32_PINMUX('E', 9, AF1)>; bias-pull-down; drive-push-pull; slew-rate = <0>; }; }; /* configure 'PE9' as analog input in low-power mode */ pwm1_sleep_pins_a: pwm1-sleep-0 { pins { pinmux = <STM32_PINMUX('E', 9, ANALOG)>; }; };
File:Info.png | The PWM output doesn't require any DMA channel. Disable them if they are configured by default in the .dtsi file. |
okay"; /* spare all DMA channels since they are not needed for PWM output */ /delete-property/dmas; /delete-property/dma-names; pwm { /* configure PWM on TIM1_CH1 */ pinctrl-0 = <&pwm1_pins_a>; pinctrl-1 = <&pwm1_sleep_pins_a>; pinctrl-names = "default", "sleep"; /* enable PWM on TIM1 */ status = "okay"; }; timer@0 { /* enable trigger on TIM1 */ status = "okay"; }; };&timers1 { status = "
3.3.3. TIM configured in PWM input capture mode[edit source]
The example below shows how to configure TIM1 channel 1 in PWM input capture mode (e.g. period and duty cycle):
- Configure PWM input on PE9, e.g. TIM1_CH1 (See pinctrl device tree configuration and GPIO internal peripheral)
/* select TIM1_CH1 alternate function 1 on 'PE9' */ pwm1_in_pins_a: pwm1-in-0 { pins { pinmux = <STM32_PINMUX('E', 9, AF1)>; bias-disable; }; }; /* configure 'PE9' as analog input in low-power mode */ pwm1_in_sleep_pins_a: pwm1-in-sleep-0 { pins { pinmux = <STM32_PINMUX('E', 9, ANALOG)>; }; };
A DMA channel is required and must be configured depending on the PWM input channel:
- Select DMA channel 1, "ch1", to capture PWM input channel 1 and/or 2
- Select DMA channel 3, "ch3", to capture PWM input channel 3 and/or 4
- Select both "ch1" and "ch3" dmas to enable capture on all PWM input channels
okay"; /* Enable DMA "ch1" for PWM input on TIM1_CH1 */ dmas = <&dmamux1 11 0x400 0x5>; dma-names = "ch1"; pwm { /* configure PWM input pins, e.g. TIM1_CH1 */ pinctrl-0 = <&pwm1_in_pins_a>; pinctrl-1 = <&pwm1_in_sleep_pins_a>; pinctrl-names = "default", "sleep"; /* enable PWM on TIM1 */ status = "okay"; }; };&timers1 { status = "
File:Info.png | DMA channels 1 and/or 3 for each TIM can be picked from the "dmas" list in stm32mp151.dtsi[4] file |
3.3.4. TIM configured as quadrature encoder interface[edit source]
The example below shows how to configure TIM1 to interface with a quadrature encoder:
- Configure PE9 and PE11 as encoder input pins, e.g. TIM1_CH1, TIM1_CH2 (see pinctrl device tree configuration and GPIO internal peripheral)
File:Info.png | On the STM32MP157X-DKX discovery board, TIM1_CH1 and TIM1_CH2 signals are accessible via the D6 and D10 pins of the Arduino Uno connector. |
tim1_in_pins_a: tim1-in-pins-0 {
pins {
pinmux = <STM32_PINMUX('E', 9, AF1)>, /* TIM1_CH1 */
<STM32_PINMUX('E', 11, AF1)>; /* TIM1_CH2 */
bias-disable;
};
};
tim1_in_pins_sleep_a: tim1-in-pins-sleep-0 {
pins {
pinmux = <STM32_PINMUX('E', 9, ANALOG)>, /* TIM1_CH1 */
<STM32_PINMUX('E', 11, ANALOG)>; /* TIM1_CH2 */
};
};
okay"; /delete-property/dmas; /* spare all DMA channels since they are not required for quadrature encoder interface */ /delete-property/dma-names; counter { pinctrl-0 = <&tim1_in_pins_a>; /* configure TIM1_CH1 and TIM1_CH2 as encoder input pins */ pinctrl-1 = <&tim1_in_pins_sleep_a>; pinctrl-names = "default", "sleep"; status = "okay"; /* enable Encoder interface mode on TIM1 */ }; };&timers1 { status = "
4. How to configure the DT using STM32CubeMX[edit source]
The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX may not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.
5. References[edit source]
Please refer to the following links for additional information:
- ↑ Jump up to: 1.0 1.1 TIM internal peripheral
- ↑ Device tree
- ↑ Documentation/devicetree/bindings/mfd/mfd/st,stm32-timers.yaml
- ↑ Jump up to: 4.0 4.1 stm32mp151.dtsi , STM32.dtsi file
- ↑ Jump up to: 5.0 5.1 Documentation/devicetree/bindings/leds/leds-pwm.yaml , PWM LEDs device tree bindings