This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User mNo edit summary |
Registered User mNo edit summary |
||
(4 intermediate revisions by 2 users not shown) | |||
Line 1: | Line 1: | ||
<noinclude>{{ApplicableFor | |||
|MPUs list=STM32MP15x | |||
|MPUs checklist=STM32MP13x,STM32MP15x | |||
}}</noinclude> | |||
MB1263 board overview. | MB1263 board overview. | ||
== Board overview == | == Board overview == | ||
'''Daughterboard MB1263''' (STM32MP157x 18x18 with PMIC and DDR3), revision C-0.1: part of the | '''Daughterboard MB1263''' (STM32MP157x 18x18 with PMIC and DDR3), revision C-0.1: part of the {{Board | type=157x-EV1}}. | ||
{{ | {{ | ||
Line 21: | Line 25: | ||
rect 415 84 472 106 [[#LED 6 | ST-LINK/V2-1 LED (bicolor LD6)]] | rect 415 84 472 106 [[#LED 6 | ST-LINK/V2-1 LED (bicolor LD6)]] | ||
rect 380 106 472 156 [[#ST-LINK USB | USB micro-B (ST-LINK/V2-1)]] | rect 380 106 472 156 [[#ST-LINK USB | USB micro-B (ST-LINK/V2-1)]] | ||
rect 130 252 251 374 [[#STM32MP157x | | rect 130 252 251 374 [[#STM32MP157x | STM32MP157x 18x18]] | ||
rect 291 274 363 348 [[#eMMC | eMMC]] | rect 291 274 363 348 [[#eMMC | eMMC]] | ||
rect 130 395 204 614 [[#DDR3L | 2 x DDR3L 16 bits]] | rect 130 395 204 614 [[#DDR3L | 2 x DDR3L 16 bits]] | ||
Line 44: | Line 48: | ||
<noinclude> | <noinclude> | ||
{{ | {{PublicationRequestId | 7568 | 2018-06-19 | AlainF}} | ||
[[Category:STM32MP15 Evaluation boards]] | [[Category:STM32MP15 Evaluation boards]] | ||
[[Category:ST boards]] | [[Category:ST boards]] | ||
</noinclude> | </noinclude> |
Latest revision as of 09:37, 25 October 2022
MB1263 board overview.
1. Board overview[edit source]
Daughterboard MB1263 (STM32MP157x 18x18 with PMIC and DDR3), revision C-0.1: part of the STM32MP157x-EV1 Evaluation board .
Details of some LEDs:
- LD1: green if power connection established
- LD6: red flashing if ST-LINK/V2-1 connection not established, else green
- LD2, LD3, LD4, LD5: some user LEDs are used to reflect the system activity, whereas the others are left free and can be directly used by the application, as explained in the LEDs and buttons on STM32 MPU boards article
2. Links[edit source]