Registered User No edit summary |
Registered User mNo edit summary |
||
(3 intermediate revisions by one other user not shown) | |||
Line 1: | Line 1: | ||
<noinclude> | <noinclude>{{ApplicableFor | ||
{{ | |MPUs list=STM32MP13x, STM32MP15x | ||
|MPUs checklist=STM32MP13x,STM32MP15x | |||
}}</noinclude> | |||
</noinclude> | |||
== Article purpose == | == Article purpose == | ||
This article provides the basic information needed to start using the Linux kernel tool: '''ip''' <ref name=ipmanpage/>. | This article provides the basic information needed to start using the Linux kernel tool: '''ip''' <ref name=ipmanpage/>. | ||
Line 19: | Line 14: | ||
{{highlight|'''ip''' replaces the deprecated command [[Ifconfig|ifconfig]]}} | {{highlight|'''ip''' replaces the deprecated command [[Ifconfig|ifconfig]]}} | ||
|| {{Y}} || {{Y}} || {{Y}} | || {{Y}} || {{Y}} || {{Y}} | ||
| | || {{Y}} || {{Y}} || {{Y}} | ||
|- | |- | ||
</onlyinclude> | </onlyinclude> | ||
Line 30: | Line 25: | ||
/sbin/ip | /sbin/ip | ||
It is integrated into the Weston image distribution by using the following meta-st package recipie to enable the iproute2 module: ''meta-st/meta-st-openstlinux/recipes-st/packagegroups/packagegroup-framework-tools.bb''. | It is integrated into the Weston image distribution by using the following meta-st package recipie to enable the iproute2 module: <code>''meta-st/meta-st-openstlinux/recipes-st/packagegroups/packagegroup-framework-tools.bb''</code>. | ||
RDEPENDS_packagegroup-framework-tools-network-base = "\ | RDEPENDS_packagegroup-framework-tools-network-base = "\ | ||
ethtool \ | ethtool \ | ||
Line 37: | Line 32: | ||
=== Using the STM32MPU Embedded Software distribution for Android™ === | === Using the STM32MPU Embedded Software distribution for Android™ === | ||
{{ | '''ip''' is installed by default (/system/bin/ip) and is ready to be used with all STM32MPU software packages for Android™. | ||
{{Board$}} which ip | |||
/system/bin/ip | |||
It is integrated in Android image distribution through Android base makefile: <code>''build/make/target/product/core_minimal.mk''</code>: | |||
# Base modules (will move elsewhere, previously user tagged) | |||
PRODUCT_PACKAGES += \ | |||
BackupRestoreConfirmation \ | |||
CompanionDeviceManager \ | |||
... | |||
ims-common \ | |||
{{green|'''ip \'''}} | |||
ip-up-vpn \ | |||
... | |||
== Getting started == | == Getting started == | ||
{{Android | Need to enable root access rights for any changes | |||
*Using ADB shell is ADB link available: | |||
{{PC$}} adb root | |||
{{PC$}} adb shell | |||
{{Board$}} ... | |||
*Using uart console shell: | |||
{{Board$}} su | |||
{{Board$}} ... | |||
}} | |||
* To check network interfaces | * To check network interfaces | ||
{{Board$}} ip addr show | {{Board$}} ip addr show | ||
Line 109: | Line 127: | ||
| Documentation | | Documentation | ||
|} | |} | ||
<noinclude> | |||
{{ ArticleBasedOnModel | Trace and debug tools article model }} | |||
{{ PublicationRequestId | 9716 | 22Nov'18 }} | |||
[[Category:Linux monitoring tools]] | |||
</noinclude> |
Latest revision as of 13:44, 24 October 2022
1. Article purpose[edit source]
This article provides the basic information needed to start using the Linux kernel tool: ip [1].
2. Introduction[edit source]
The following table provides a brief description of the tool, as well as its availability depending on the software packages:
: this tool is either present (ready to use or to be activated), or can be integrated and activated on the software package.
: this tool is not present and cannot be integrated, or it is present but cannot be activated on the software package.
Tool | STM32MPU Embedded Software distribution | STM32MPU Embedded Software distribution for Android™ | ||||||
---|---|---|---|---|---|---|---|---|
Name | Category | Purpose | Starter Package | Developer Package | Distribution Package | Starter Package | Developer Package | Distribution Package |
ip | Monitoring tools | ip[1] shows / manipulates routing, devices, policy routing and tunnels of network interfaces. ip replaces the deprecated command ifconfig |
![]() |
![]() |
![]() |
![]() |
![]() |
![]() |
3. Installing the trace and debug tool on your target board[edit source]
3.1. Using the STM32MPU Embedded Software distribution[edit source]
ip is installed by default (/sbin/ip) and is ready to be used with all STM32MPU software packages.
which ip
/sbin/ip
It is integrated into the Weston image distribution by using the following meta-st package recipie to enable the iproute2 module: meta-st/meta-st-openstlinux/recipes-st/packagegroups/packagegroup-framework-tools.bb
.
iproute2 \ "RDEPENDS_packagegroup-framework-tools-network-base = "\ ethtool \
3.2. Using the STM32MPU Embedded Software distribution for Android™[edit source]
ip is installed by default (/system/bin/ip) and is ready to be used with all STM32MPU software packages for Android™.
which ip
/system/bin/ip
It is integrated in Android image distribution through Android base makefile: build/make/target/product/core_minimal.mk
:
ip \ ip-up-vpn \ ...# Base modules (will move elsewhere, previously user tagged) PRODUCT_PACKAGES += \ BackupRestoreConfirmation \ CompanionDeviceManager \ ... ims-common \
4. Getting started[edit source]
![]() |
Below information is related to the Android™ distribution Need to enable root access rights for any changes
adb root
adb shell
...
su
...
|
- To check network interfaces
UP,LOWER_UP> mtu 65536 qdisc noqueue state UNKNOWN group default qlen 1000 link/loopback 00:00:00:00:00:00 brd 00:00:00:00:00:00 inet 127.0.0.1/8 scope host lo valid_lft forever preferred_lft forever inet6 ::1/128 scope host valid_lft forever preferred_lft forever 2: can0: <NOARP,ECHO> mtu 16 qdisc noop state DOWN group default qlen 10 link/can 3: eth0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc mq state UP group default qlen 1000 link/ether 00:80:e1:42:43:65 brd ff:ff:ff:ff:ff:ff inet 192.168.1.237/22 brd 192.168.3.255 scope global dynamic eth0 valid_lft 172057sec preferred_lft 172057sec inet 192.168.0.4/32 scope global eth0 valid_lft forever preferred_lft forever inet6 fe80::280:e1ff:fe42:4365/64 scope link valid_lft forever preferred_lft forever 4: sit0@NONE: <NOARP> mtu 1480 qdisc noop state DOWN group default qlen 1000 link/sit 0.0.0.0 brd 0.0.0.0ip addr show 1: lo: <LOOPBACK,
- To assign an IP address to an interface
ip addr add 192.168.1.53 dev eth0
- To remove an IP adress
ip addr del 192.168.1.53 dev eth0
- To enable an interface
ip link set eth0 up
- To disable an interface
ip link set eth0 down
- To check a route table
ip route show
default via 192.168.3.254 dev eth0 proto dhcp src 192.168.1.237 metric 1024
192.168.0.0/22 dev eth0 proto kernel scope link src 192.168.1.237
192.168.3.254 dev eth0 proto dhcp scope link src 192.168.1.237 metric 1024
- To add a static route
ip route add 192.168.2.0/16 via 192.168.1.1 dev eth0
- To remove a static route
ip route del 192.168.2.0/16
- To set the default gateway
ip route add default via 192.168.1.1
5. To go further[edit source]
Some usage examples are available for reference[2].
6. References[edit source]
- Useful external links
Document link | Document Type | Description |
---|---|---|
IP Command example | Standard | Documentation from tecmint |
ifconfig vs ip | Standard | Documentation |