Registered User m (Replaced content with "<noinclude> {{ArticleMainWriter | RomualdJ}} {{ArticleApprovedVersion | Jean-ChristopheT | Nobody | No previous approved version | Automatic approval (article under constr...") Tag: Replaced |
Registered User |
||
(33 intermediate revisions by 9 users not shown) | |||
Line 1: | Line 1: | ||
<noinclude>{{ApplicableFor | |||
|MPUs list=STM32MP13x, STM32MP15x | |||
|MPUs checklist=STM32MP13x, STM32MP15x | |||
}}</noinclude> | |||
{{InternalInfo|This article provides the user with the information needed to measure the boot time, and then implement first-level optimization (roughly a 50% gain). Fine tuning is outside the scope of this article.}} | |||
== Article purpose == | |||
The purpose of this document is to provide information on how to measure and improve the boot-time<ref>Sometimes referred to as startup-time.</ref> of a typical {{MicroprocessorDevice | device=1}} Linux system. This article is not an exhaustive list of possible optimizations, and those that are considered insufficiently reliable for industrial use are intentionally omitted. | |||
== Overview == | |||
On a typical STM32MP1 Linux system, the [[Boot chain overview|boot-chain]] is performed, respectively, by: the ROM code, TF-A, U-Boot, the Linux kernel, and the user-land<ref>Sometimes referred to as user-space.</ref>. All these components except the ROM code can be | |||
modified, and thus configured to start more quickly. For each of them, the procedure is the same: features that are not required | |||
at boot-time must be initiated after system boot (or disabled), and features that improve the boot time must be enabled. | |||
== Measuring boot-time == | |||
Before optimizing the performance of any piece of software, the time duration of each part must be considered so that the effort can be focused effectively. | |||
=== Using a serial console === | |||
One of the easiest way to measure the boot-time of a Linux system is to observe traces emitted on a serial console using timing software, such as [https://github.com/tbird20d/grabserial serialgrab] or like the script [[Media:measure-timing.txt|measure-timing.txt]] based on [https://git.pengutronix.de/cgit/tools/microcom microcom] and [http://p2f.tuxfamily.org p2f]. | |||
For example: | |||
{{PC$}} microcom -p /dev/ttyACM0 | bash Measure-timing.txt | |||
Waiting for board reset... | |||
NOTICE: Model: STMicroelectronics STM32MP157C eval daughter on eval mother | |||
NOTICE: Board: MB1263 Var1 Rev.C-01 | |||
… | |||
U-Boot 2018.11-stm32mp-r2 (Nov 14 2018 - 16:10:06 +0000) | |||
CPU: STM32MP157AAA Rev.B | |||
Model: STMicroelectronics STM32MP157C eval daughter on eval mother | |||
… | |||
Starting kernel ... | |||
[ 0.000000] Booting Linux on physical CPU 0x0 | |||
… | |||
Freeing unused kernel memory: 1024K | |||
Run /sbin/init as init process | |||
… | |||
ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 2.6-openstlinux-4.19-thud-mp1-19-02-20 stm32mp1 ttySTM0 | |||
stm32mp1 login: | |||
Timing results: | |||
FSBL: 1.23s | |||
SSBL: 2.34s | |||
Linux: 2.34s | |||
init: 1.23s | |||
total: 7.14s | |||
Note: these are illustrative figures since the boot-time depends on too many parameters to provide meaningful figures here. | |||
=== Using hardware timers === | |||
When measuring traces from a serial console is not precise enough, or when traces are not available, it is possible to use hardware timers. Some components of the boot chain provide timing information based on hardware timers; for instance with [[U-Boot overview#U-Boot configuration|U-Boot]], the following options can be enabled: | |||
CONFIG_BOOTSTAGE=y | |||
CONFIG_BOOTSTAGE_REPORT=y | |||
This prints on the serial console — just before booting the OS — something similar to the output below (illustrative figures): | |||
Starting kernel ... | |||
Timer summary in microseconds (11 records): | |||
Mark Elapsed Stage | |||
0 0 reset | |||
123,456 123,456 board_init_f | |||
2,345,678 2,222,222 board_init_r | |||
3,456,789 1,111,111 id=64 | |||
3,567,890 111,101 id=65 | |||
3,678,901 111,011 main_loop | |||
4,567,890 888,989 bootm_start | |||
4,678,901 111,011 id=15 | |||
4,789,012 110,111 start_kernel | |||
Accumulated time: | |||
23,456 dm_r | |||
567,890 dm_f | |||
Booting Linux on physical CPU 0x0 | |||
If the serial console is not available, this timing information can also be stored in the device-tree or in memory: | |||
CONFIG_BOOTSTAGE_FDT=y | |||
CONFIG_BOOTSTAGE_STASH=y | |||
It is possible to add this feature to boot-chain components that do not implement it by default, like TF-A. See the file <code>arch/arm/cpu/armv7/arch_timer.c</code> from U-Boot for an example. | |||
=== Using GPIOs === | |||
When the console is disabled, the boot-chain components can be modified to trigger events on GPIOs according to the current stage of the boot-process. Then a logical [https://sigrok.org/wiki/Supported_hardware#Logic_analyzers analyzer] can be used to measure the time between each such event. | |||
[[File:logical-analyser-example.png|thumb|none|Example of trace captured by Sigrok and displayed by PulseView.]] | |||
== Optimizing boot-time == | |||
=== TF-A === | |||
==== Configuration ==== | |||
The TF-A execution time can be noticeably reduced by disabling features that are not required. To achieve this, the right options have to be specified when building the TF-A; for instance with a system that boots exclusively from NAND logic connected through the FMC: | |||
{{PC$}} make STM32MP1_DEBUG_ENABLE=0 \ | |||
STM32MP1_UART_PROGRAMMER=0 \ | |||
STM32MP1_USB=0 \ | |||
STM32MP1_QSPI_NOR=0 \ | |||
STM32MP1_QSPI_NAND=0 \ | |||
STM32MP_FMC_NAND=1 \ | |||
STM32MP_EMMC=0 \ | |||
STM32MP_SDMMC=0 \ | |||
… | |||
These build options must of course be adjusted according to the expected usage and the TF-A version. | |||
==== I2C timing ==== | |||
I2C driver computes device timing at init, in order to guarantee correct data hold and setup times. The execution time of the computation algorithm is not so important, but with all associated device tree accesses, it can last several 10ms. It has to be done for each instance, so it can happen several times in the boot sequence. | |||
For specific needs, a hard-coded timing (and its related frequency) can be used in order to optimize boot performances. Dedicated fields can be added in the I2C instance related handle structure. Then, once retrieved, these boot values can be configured by the client, this avoids to compute timings (and to do several device tree accesses) on first init for each instance. | |||
=== U-Boot === | |||
==== Delay ==== | |||
Before loading the Linux kernel and its device tree, U-Boot, by default, waits one second for a potential user input. This behavior — | |||
undesirable when boot time is a concern — can be easily removed by specifying <code>bootdelay=0</code> in <code>include/configs/stm32mp1.h</code>. | |||
==== Configuration and device tree ==== | |||
More broadly, removing support for all unused devices from [[U-Boot overview#U-Boot configuration|U-Boot configuration]] and unused nodes | |||
from the device-tree drastically reduces the U-Boot execution time, since this eliminates the initialization time of those devices and the time to parse the device-tree. | |||
There are also a couple of U-Boot features that are specially designed to improve the boot-time, for example: | |||
CONFIG_MTD_UBI_FASTMAP=y | |||
CONFIG_SYS_MALLOC_CLEAR_ON_INIT=n | |||
Regarding support for UBI fastmap (for NOR and NAND storage media), please see the "Linux" section below for more information. | |||
==== Configuration access ==== | |||
By default U-Boot searches a boot configuration file <code>extlinux.conf</code> or a boot script <code>boot.scr.uimg</code> | |||
from a bootable partition ("bootfs" for OpenSTLinux), see [[U-Boot_overview#Generic_Distro_configuration]] for details. Such access to a file system on storage media can take a short of time, but fortunately it is possible to embed a boot command into the U-Boot binary instead. To do this, the whole U-Boot environment must be specified from scratch: | |||
CONFIG_USE_DEFAULT_ENV_FILE=y | |||
CONFIG_DEFAULT_ENV_FILE="path/to/env.txt" | |||
Or the U-Boot "distro" mode must be disabled: | |||
CONFIG_DISTRO_DEFAULTS=n | |||
In the latter case, be aware that if booting from an ext2/4 partition — typically when booting from an SD card or from eMMC — the following options must be explicitly selected (they were previously selected implicitly by CONFIG_DISTRO_DEFAULTS): | |||
CONFIG_CMD_EXT2=y | |||
CONFIG_CMD_EXT4=y | |||
In both cases only <code>CONFIG_ENV_IS_NOWHERE</code> must be set to <code>y</code> (remove all the other CONFIG_ENV_IS...) , and the environment variable <code>bootcmd</code> must contain the expected boot command, for example: | |||
CONFIG_BOOTCOMMAND="run bootcmd_ubi" | |||
bootcmd_ubi=env set bootargs ubi.mtd=UBI root=ubi0:boot \ | |||
rootfstype=ubifs rootwait \ | |||
rw console=ttySTM0,115200; \ | |||
ubi part UBI; \ | |||
ubifsmount ubi0:boot; \ | |||
ubifsload 0xc2000000 /zImage; \ | |||
ubifsload 0xc4000000 /stm32mp157c-ev1.dtb; \ | |||
bootz 0xc2000000 - 0xc4000000 | |||
=== Linux === | |||
==== Configuration and device-tree ==== | |||
For U-Boot, one of the most efficient ways to decrease the Linux boot time is to remove support for all unused devices from its configuration and device-tree, since this eliminates the time taken to initialize those devices. Also, support for devices and features that | |||
are required but not mandatory at boot-time can be compiled as [[Menuconfig or how to configure kernel|modules]], and then loaded by | |||
the user-land once the boot-process is done (see the "Init" subsection below). | |||
==== Traces ==== | |||
Linux boot traces have a size of about 2 Kbytes, so they take about 2 seconds to transfer on a serial link configured at 128 Kbit/s. If this is an issue, the following kernel parameters (<code>bootargs</code> variable in U-Boot) can be used to remove these traces: | |||
quiet loglevel=0 | |||
This is automatically done by U-Boot when silent mode is required (see CONFIG_SILENT_CONSOLE and CONFIG_SILENT_U_BOOT_ONLY): silent=1 in used U-Boot environment. | |||
==== UBI volume ==== | |||
When partitions such as "bootfs" and "rootfs" are stored on a UBI volume, the following two actions are highly recommended to greatly reduce | |||
the volume attachment time at boot-time, both by U-Boot and by the Linux kernel: | |||
1. Decrease the size of the UBI volume | |||
2. Enable the fastmap feature. For this, the <code>CONFIG_MTD_UBI_FASTMAP</code> option must be set to <code>y</code> | |||
both for Linux and U-Boot, and <code>ubi.fm_autoconvert=1</code> has to be added to the kernel boot parameters. Note that | |||
the very first boot is used to create the fastmap information, thus this one does not get faster. | |||
A lot of other volume/file-systems exist for Flash media, such as JFFS, LogFS, F2FS, and so on. Depending on the use-case, some may be faster than others. | |||
=== User-land === | |||
==== Init ==== | |||
The very first user-land process launched by the Linux kernel is <code>init</code>; it is in charge of launching other processes in the | |||
right order. As a consequence, removing all unnecessary services can greatly speed up this part of the boot-process. The way services can | |||
be removed highly depends on the system in use ([https://freedesktop.org/wiki/Software/systemd/ systemd], [https://wiki.gentoo.org/wiki/Project:OpenRC OpenRC] and so on), so please refer to its documentation. | |||
Ultimately, when no services are required, the <code>init</code> system can be replaced by the final application itself; either by storing its binary in <code>/sbin/init</code>, or by passing the following Linux boot parameter: | |||
init=/path/to/application/binary | |||
==== Framework ==== | |||
For graphical applications, the choice of display framework can seriously impact the startup time of the application itself. For | |||
instance, one could use the Linux [[DRM KMS overview|framebuffer]] instead of [[Wayland_Weston_overview|Weston]] or Xorg, since the | |||
former is set up faster than the latter. | |||
Likewise for video applications; if the boot-time is a concern, direct use of the [[V4L2 camera overview|V4L2 interface]] instead of higher-level interfaces such as [[GStreamer overview|GStreamer]] is recommended. | |||
== Conclusion == | |||
There is no universal recipe to improve the boot-time of a Linux system, since it depends on the contraints of the final use-case. However the universal rule is: '''always benchmark''', before and after optimizing. | |||
== Further reading == | |||
* https://www.e-consystems.com/Articles/Product-Design/Linux-Boot-Time-Optimization-Techniques.asp | |||
* https://www.toradex.com/blog/embedded-linux-boot-time-optimization | |||
* https://bootlin.com/blog/tag/boot-time | |||
* https://bootlin.com/doc/training/boot-time/boot-time-slides.pdf | |||
==References== | |||
<references/> | |||
<noinclude> | <noinclude> | ||
[[Category:How to customize software]] | [[Category:How to customize software]] | ||
{{PublicationRequestId | 12892 | 2019-08-01}} | |||
</noinclude> | </noinclude> | ||
Latest revision as of 14:11, 17 August 2022
1. Article purpose[edit source]
The purpose of this document is to provide information on how to measure and improve the boot-time[1] of a typical STM32MP1 Series Linux system. This article is not an exhaustive list of possible optimizations, and those that are considered insufficiently reliable for industrial use are intentionally omitted.
2. Overview[edit source]
On a typical STM32MP1 Linux system, the boot-chain is performed, respectively, by: the ROM code, TF-A, U-Boot, the Linux kernel, and the user-land[2]. All these components except the ROM code can be modified, and thus configured to start more quickly. For each of them, the procedure is the same: features that are not required at boot-time must be initiated after system boot (or disabled), and features that improve the boot time must be enabled.
3. Measuring boot-time[edit source]
Before optimizing the performance of any piece of software, the time duration of each part must be considered so that the effort can be focused effectively.
3.1. Using a serial console[edit source]
One of the easiest way to measure the boot-time of a Linux system is to observe traces emitted on a serial console using timing software, such as serialgrab or like the script measure-timing.txt based on microcom and p2f.
For example:
U-Boot 2018.11-stm32mp-r2 (Nov 14 2018 - 16:10:06 +0000) CPU: STM32MP157AAA Rev.B Model: STMicroelectronics STM32MP157C eval daughter on eval mother … Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 … Freeing unused kernel memory: 1024K Run /sbin/init as init process … ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 2.6-openstlinux-4.19-thud-mp1-19-02-20 stm32mp1 ttySTM0 stm32mp1 login: Timing results: FSBL: 1.23s SSBL: 2.34s Linux: 2.34s init: 1.23s total: 7.14smicrocom -p /dev/ttyACM0 | bash Measure-timing.txt Waiting for board reset... NOTICE: Model: STMicroelectronics STM32MP157C eval daughter on eval mother NOTICE: Board: MB1263 Var1 Rev.C-01 …
Note: these are illustrative figures since the boot-time depends on too many parameters to provide meaningful figures here.
3.2. Using hardware timers[edit source]
When measuring traces from a serial console is not precise enough, or when traces are not available, it is possible to use hardware timers. Some components of the boot chain provide timing information based on hardware timers; for instance with U-Boot, the following options can be enabled:
CONFIG_BOOTSTAGE=y
CONFIG_BOOTSTAGE_REPORT=y
This prints on the serial console — just before booting the OS — something similar to the output below (illustrative figures):
Linux on physical CPU 0x0Starting kernel ... Timer summary in microseconds (11 records): Mark Elapsed Stage 0 0 reset 123,456 123,456 board_init_f 2,345,678 2,222,222 board_init_r 3,456,789 1,111,111 id=64 3,567,890 111,101 id=65 3,678,901 111,011 main_loop 4,567,890 888,989 bootm_start 4,678,901 111,011 id=15 4,789,012 110,111 start_kernel Accumulated time: 23,456 dm_r 567,890 dm_f Booting
If the serial console is not available, this timing information can also be stored in the device-tree or in memory:
CONFIG_BOOTSTAGE_FDT=y
CONFIG_BOOTSTAGE_STASH=y
It is possible to add this feature to boot-chain components that do not implement it by default, like TF-A. See the file arch/arm/cpu/armv7/arch_timer.c
from U-Boot for an example.
3.3. Using GPIOs[edit source]
When the console is disabled, the boot-chain components can be modified to trigger events on GPIOs according to the current stage of the boot-process. Then a logical analyzer can be used to measure the time between each such event.
4. Optimizing boot-time[edit source]
4.1. TF-A[edit source]
4.1.1. Configuration[edit source]
The TF-A execution time can be noticeably reduced by disabling features that are not required. To achieve this, the right options have to be specified when building the TF-A; for instance with a system that boots exclusively from NAND logic connected through the FMC:
UART_PROGRAMMER=0 \ STM32MP1_USB=0 \ STM32MP1_QSPI_NOR=0 \ STM32MP1_QSPI_NAND=0 \ STM32MP_FMC_NAND=1 \ STM32MP_EMMC=0 \ STM32MP_SDMMC=0 \ …make STM32MP1_DEBUG_ENABLE=0 \ STM32MP1_
These build options must of course be adjusted according to the expected usage and the TF-A version.
4.1.2. I2C timing[edit source]
I2C driver computes device timing at init, in order to guarantee correct data hold and setup times. The execution time of the computation algorithm is not so important, but with all associated device tree accesses, it can last several 10ms. It has to be done for each instance, so it can happen several times in the boot sequence.
For specific needs, a hard-coded timing (and its related frequency) can be used in order to optimize boot performances. Dedicated fields can be added in the I2C instance related handle structure. Then, once retrieved, these boot values can be configured by the client, this avoids to compute timings (and to do several device tree accesses) on first init for each instance.
4.2. U-Boot[edit source]
4.2.1. Delay[edit source]
Before loading the Linux kernel and its device tree, U-Boot, by default, waits one second for a potential user input. This behavior —
undesirable when boot time is a concern — can be easily removed by specifying bootdelay=0
in include/configs/stm32mp1.h
.
4.2.2. Configuration and device tree[edit source]
More broadly, removing support for all unused devices from U-Boot configuration and unused nodes from the device-tree drastically reduces the U-Boot execution time, since this eliminates the initialization time of those devices and the time to parse the device-tree.
There are also a couple of U-Boot features that are specially designed to improve the boot-time, for example:
MTD_UBI_FASTMAP=y CONFIG_SYS_MALLOC_CLEAR_ON_INIT=nCONFIG_
Regarding support for UBI fastmap (for NOR and NAND storage media), please see the "Linux" section below for more information.
4.2.3. Configuration access[edit source]
By default U-Boot searches a boot configuration file extlinux.conf
or a boot script boot.scr.uimg
from a bootable partition ("bootfs" for OpenSTLinux), see U-Boot_overview#Generic_Distro_configuration for details. Such access to a file system on storage media can take a short of time, but fortunately it is possible to embed a boot command into the U-Boot binary instead. To do this, the whole U-Boot environment must be specified from scratch:
CONFIG_USE_DEFAULT_ENV_FILE=y
CONFIG_DEFAULT_ENV_FILE="path/to/env.txt"
Or the U-Boot "distro" mode must be disabled:
CONFIG_DISTRO_DEFAULTS=n
In the latter case, be aware that if booting from an ext2/4 partition — typically when booting from an SD card or from eMMC — the following options must be explicitly selected (they were previously selected implicitly by CONFIG_DISTRO_DEFAULTS):
CONFIG_CMD_EXT2=y
CONFIG_CMD_EXT4=y
In both cases only CONFIG_ENV_IS_NOWHERE
must be set to y
(remove all the other CONFIG_ENV_IS...) , and the environment variable bootcmd
must contain the expected boot command, for example:
CONFIG_BOOTCOMMAND="run bootcmd_ubi"
UBI root=ubi0:boot \ rootfstype=ubifs rootwait \ rw console=ttySTM0,115200; \ ubi part UBI; \ ubifsmount ubi0:boot; \ ubifsload 0xc2000000 /zImage; \ ubifsload 0xc4000000 /stm32mp157c-ev1.dtb; \ bootz 0xc2000000 - 0xc4000000bootcmd_ubi=env set bootargs ubi.mtd=
4.3. Linux[edit source]
4.3.1. Configuration and device-tree[edit source]
For U-Boot, one of the most efficient ways to decrease the Linux boot time is to remove support for all unused devices from its configuration and device-tree, since this eliminates the time taken to initialize those devices. Also, support for devices and features that are required but not mandatory at boot-time can be compiled as modules, and then loaded by the user-land once the boot-process is done (see the "Init" subsection below).
4.3.2. Traces[edit source]
Linux boot traces have a size of about 2 Kbytes, so they take about 2 seconds to transfer on a serial link configured at 128 Kbit/s. If this is an issue, the following kernel parameters (bootargs
variable in U-Boot) can be used to remove these traces:
quiet loglevel=0
This is automatically done by U-Boot when silent mode is required (see CONFIG_SILENT_CONSOLE and CONFIG_SILENT_U_BOOT_ONLY): silent=1 in used U-Boot environment.
4.3.3. UBI volume[edit source]
When partitions such as "bootfs" and "rootfs" are stored on a UBI volume, the following two actions are highly recommended to greatly reduce the volume attachment time at boot-time, both by U-Boot and by the Linux kernel:
1. Decrease the size of the UBI volume
2. Enable the fastmap feature. For this, the CONFIG_MTD_UBI_FASTMAP
option must be set to y
both for Linux and U-Boot, and ubi.fm_autoconvert=1
has to be added to the kernel boot parameters. Note that
the very first boot is used to create the fastmap information, thus this one does not get faster.
A lot of other volume/file-systems exist for Flash media, such as JFFS, LogFS, F2FS, and so on. Depending on the use-case, some may be faster than others.
4.4. User-land[edit source]
4.4.1. Init[edit source]
The very first user-land process launched by the Linux kernel is init
; it is in charge of launching other processes in the
right order. As a consequence, removing all unnecessary services can greatly speed up this part of the boot-process. The way services can
be removed highly depends on the system in use (systemd, OpenRC and so on), so please refer to its documentation.
Ultimately, when no services are required, the init
system can be replaced by the final application itself; either by storing its binary in /sbin/init
, or by passing the following Linux boot parameter:
init=/path/to/application/binary
4.4.2. Framework[edit source]
For graphical applications, the choice of display framework can seriously impact the startup time of the application itself. For instance, one could use the Linux framebuffer instead of Weston or Xorg, since the former is set up faster than the latter.
Likewise for video applications; if the boot-time is a concern, direct use of the V4L2 interface instead of higher-level interfaces such as GStreamer is recommended.
5. Conclusion[edit source]
There is no universal recipe to improve the boot-time of a Linux system, since it depends on the contraints of the final use-case. However the universal rule is: always benchmark, before and after optimizing.
6. Further reading[edit source]
- https://www.e-consystems.com/Articles/Product-Design/Linux-Boot-Time-Optimization-Techniques.asp
- https://www.toradex.com/blog/embedded-linux-boot-time-optimization
- https://bootlin.com/blog/tag/boot-time
- https://bootlin.com/doc/training/boot-time/boot-time-slides.pdf
7. References[edit source]