This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User No edit summary |
Registered User mNo edit summary |
||
(2 intermediate revisions by one other user not shown) | |||
Line 1: | Line 1: | ||
==Wayland logs== | <noinclude>{{ApplicableFor | ||
|MPUs list=STM32MP13x, STM32MP15x | |||
|MPUs checklist=STM32MP13x,STM32MP15x | |||
}}</noinclude> | |||
== Wayland logs == | |||
To get the logs of the wayland protocol messages, set this environment variable: | To get the logs of the wayland protocol messages, set this environment variable: | ||
{{Board$}} export WAYLAND_DEBUG=1 | {{Board$}} export WAYLAND_DEBUG=1 | ||
==Saving Weston logs in a file== | == Saving Weston logs in a file == | ||
Standard Weston logs are available in the '''/ | Standard Weston logs are available in the '''/home/weston/weston.log''' file when Weston is started with the "weston user" using the systemd service. | ||
{{Board$}} cat / | {{Board$}} cat /home/weston/weston.log | ||
==Displaying Weston logs on a console== | == Displaying Weston logs on a console == | ||
Start Weston with the following command: | Start Weston with the following command: | ||
{{Board$}} weston --tty=1 & | {{Board$}} weston --tty=1 & |
Latest revision as of 16:43, 9 June 2022
1. Wayland logs
To get the logs of the wayland protocol messages, set this environment variable:
export WAYLAND_DEBUG=1
2. Saving Weston logs in a file
Standard Weston logs are available in the /home/weston/weston.log file when Weston is started with the "weston user" using the systemd service.
cat /home/weston/weston.log
3. Displaying Weston logs on a console
Start Weston with the following command:
weston --tty=1 &
All Weston logs are then displayed on the console.