Registered User No edit summary |
Registered User mNo edit summary |
||
(7 intermediate revisions by 2 users not shown) | |||
Line 1: | Line 1: | ||
<noinclude>{{ApplicableFor | |||
|MPUs list=STM32MP13x, STM32MP15x | |||
|MPUs checklist=STM32MP13x,STM32MP15x | |||
}}</noinclude> | |||
== Article purpose == | == Article purpose == | ||
This article explains how to record audio via the kernel [[ALSA overview|ALSA]] audio framework in '''Linux® OS''' context. | This article explains how to record audio via the kernel [[ALSA overview|ALSA]] audio framework in '''Linux® OS''' context. | ||
Line 6: | Line 10: | ||
The [[ALSA overview|ALSA]] framework exposes audio devices associated to the board audio hardware interfaces. | The [[ALSA overview|ALSA]] framework exposes audio devices associated to the board audio hardware interfaces. | ||
The application audio streams are routed by default through the | The application audio streams are routed by default through the PulseAudio sound server. PulseAudio exposes audio profiles, which are mapped on the ALSA sound card audio devices. The PulseAudio server provides a command line interface to list audio profiles and to select one, in order to record from a specific audio interface. | ||
{{Warning|The applications interacting with Weston framework have to be launched as "Weston" user instead of "root" user. The Pulseaudio commands can, for instance, be launched as follows: | |||
su -l "weston" -c "pactl info" | |||
}} | |||
The audio record examples in following sections are based on [[ALSA_overview#How_to_use|ALSA utilities]]. Some input paths are configured through ALSA controls. These configurations are detailed in [[Soundcard_configuration|sound card configuration]] article. If an error is issued when running an example, please refer to [[Audio troubleshooting grid]] article for debug. | The audio record examples in following sections are based on [[ALSA_overview#How_to_use|ALSA utilities]]. Some input paths are configured through ALSA controls. These configurations are detailed in [[Soundcard_configuration|sound card configuration]] article. If an error is issued when running an example, please refer to [[Audio troubleshooting grid]] article for debug. | ||
Line 21: | Line 29: | ||
==== Record via PulseAudio ==== | ==== Record via PulseAudio ==== | ||
* '''Configure Pulseaudio :''' | * '''Configure Pulseaudio :''' | ||
Change Pulseaudio default input source to 'analog_input': | Change Pulseaudio default input source to 'analog_input': | ||
{{Info|The Pulseaudio analog_input is defined in /etc/pulse/system.pa configuration file.}} | {{Info|The Pulseaudio analog_input is defined in /etc/pulse/system.pa configuration file.}} | ||
{{Board$}} | {{Board$}} pactl set-default-source analog_input | ||
* '''Start audio record :''' | * '''Start audio record :''' | ||
{{Info|The Pulseaudio device is the default one, so "-D pulse" option can be omitted in the record command.}} | {{Info|The Pulseaudio device is the default one, so "-D pulse" option can be omitted in the record command.}} | ||
{{Board$}} arecord -d 10 /tmp/rec.wav | {{Board$}} arecord -d 10 /tmp/rec.wav | ||
=== Audio record from digital microphone input === | === Audio record from digital microphone input === | ||
Line 56: | Line 49: | ||
==== Record multiple digital microphones from a virtual ALSA device ==== | ==== Record multiple digital microphones from a virtual ALSA device ==== | ||
Start stereo audio record from 'multi' ALSA device: | Start stereo audio record from 'multi' ALSA device: | ||
{{Info|'multi' device, based on ALSA multi plugin<ref>[https://www.alsa-project.org/alsa-doc/alsa-lib/pcm_plugins.html | {{Info|'multi' device, based on ALSA multi plugin<ref>[https://www.alsa-project.org/alsa-doc/alsa-lib/pcm_plugins.html ALSA PCM plugins]</ref>, has to be defined in /etc/asound.conf file.}} | ||
{{Board$}} arecord -D multi -r 16000 -f S32_LE -c 2 -d 10 /tmp/rec.wav | {{Board$}} arecord -D multi -r 16000 -f S32_LE -c 2 -d 10 /tmp/rec.wav | ||
==== Record via PulseAudio ==== | ==== Record via PulseAudio ==== | ||
* '''Configure Pulseaudio''' | * '''Configure Pulseaudio''' | ||
Change Pulseaudio default input source to 'dmic1_input': | Change Pulseaudio default input source to 'dmic1_input': | ||
{{Info|The Pulseaudio dmic1_input is defined in /etc/pulse/system.pa configuration file.}} | {{Info|The Pulseaudio dmic1_input is defined in /etc/pulse/system.pa configuration file.}} | ||
{{Board$}} | {{Board$}} pactl set-default-source dmic1_input | ||
* '''Start audio record :''' | * '''Start audio record :''' | ||
Line 73: | Line 65: | ||
=== Audio record from S/PDIF input === | === Audio record from S/PDIF input === | ||
{{Warning|The support of S/PDIF input is board dependent. Please, check available inputs with "''arecord -l''" command.}} | {{Warning|The support of S/PDIF input is board dependent. Please, check available inputs with "''arecord -l''" command.}} | ||
==== Get IEC958 status bits ==== | |||
Some restrictions may apply to IEC958 control, depending on the SPDIFRX device configuration as it is explained in [[SPDIFRX device tree configuration]] and [[SPDIFRX Linux driver]] articles. | |||
{{Board$}} amixer -c STM32MP1EV cget iface=PCM,name='IEC958 Capture Default' | |||
==== Record from ALSA device ==== | ==== Record from ALSA device ==== | ||
Line 81: | Line 78: | ||
==== Record via PulseAudio ==== | ==== Record via PulseAudio ==== | ||
* '''Configure Pulseaudio''' | * '''Configure Pulseaudio''' | ||
Change Pulseaudio default input source to 'iec958_input': | Change Pulseaudio default input source to 'iec958_input': | ||
{{Info|The Pulseaudio iec958_input is defined in /etc/pulse/system.pa configuration file.}} | {{Info|The Pulseaudio iec958_input is defined in /etc/pulse/system.pa configuration file.}} | ||
{{Board$}} | {{Board$}} pactl set-default-source iec958_input | ||
* '''Start audio record :''' | * '''Start audio record :''' |
Latest revision as of 13:35, 8 June 2022
1. Article purpose[edit source]
This article explains how to record audio via the kernel ALSA audio framework in Linux® OS context. The examples below, show how to record audio from the different audio hardware interfaces of the STM32MPU boards.
2. Audio record overview[edit source]
The ALSA framework exposes audio devices associated to the board audio hardware interfaces.
The application audio streams are routed by default through the PulseAudio sound server. PulseAudio exposes audio profiles, which are mapped on the ALSA sound card audio devices. The PulseAudio server provides a command line interface to list audio profiles and to select one, in order to record from a specific audio interface.
The audio record examples in following sections are based on ALSA utilities. Some input paths are configured through ALSA controls. These configurations are detailed in sound card configuration article. If an error is issued when running an example, please refer to Audio troubleshooting grid article for debug.
3. Examples[edit source]
3.1. Audio record from headset microphone input[edit source]
3.1.1. Record from ALSA device[edit source]
Start audio record from 'record_codec' ALSA device:
arecord -D record_codec -f S16_LE -d 10 /tmp/rec.wav
3.1.2. Record via PulseAudio[edit source]
- Configure Pulseaudio :
Change Pulseaudio default input source to 'analog_input':
pactl set-default-source analog_input
- Start audio record :
arecord -d 10 /tmp/rec.wav
3.2. Audio record from digital microphone input[edit source]
3.2.1. Record from ALSA device[edit source]
Start mono audio record from 'record_dfsdm0' ALSA device:
arecord -D record_dfsdm0 -r 16000 -f S32_LE -c 1 -d 10 /tmp/rec.wav
3.2.2. Record multiple digital microphones from a virtual ALSA device[edit source]
Start stereo audio record from 'multi' ALSA device:
arecord -D multi -r 16000 -f S32_LE -c 2 -d 10 /tmp/rec.wav
3.2.3. Record via PulseAudio[edit source]
- Configure Pulseaudio
Change Pulseaudio default input source to 'dmic1_input':
pactl set-default-source dmic1_input
- Start audio record :
arecord -r 48000 -f S32_LE -c 2 -d 10 /tmp/rec.wav
3.3. Audio record from S/PDIF input[edit source]
3.3.1. Get IEC958 status bits[edit source]
Some restrictions may apply to IEC958 control, depending on the SPDIFRX device configuration as it is explained in SPDIFRX device tree configuration and SPDIFRX Linux driver articles.
amixer -c STM32MP1EV cget iface=PCM,name='IEC958 Capture Default'
3.3.2. Record from ALSA device[edit source]
Start audio record from 'record_spdif' ALSA device:
arecord -D record_spdif -f S32_LE -c 2 -r 48000 -d 10 /tmp/rec.wav
3.3.3. Record via PulseAudio[edit source]
- Configure Pulseaudio
Change Pulseaudio default input source to 'iec958_input':
pactl set-default-source iec958_input
- Start audio record :
arecord -r 48000 -f S32_LE -c 2 -d 10 /tmp/rec.wav
4. References[edit source]