deleted>Frq08988 mNo edit summary |
Registered User mNo edit summary |
||
(11 intermediate revisions by 4 users not shown) | |||
Line 1: | Line 1: | ||
<noinclude> | <noinclude>{{ApplicableFor | ||
{{ | |MPUs list=STM32MP15x | ||
|MPUs checklist=STM32MP13x, STM32MP15x | |||
}}</noinclude> | |||
</noinclude> | |||
==Article purpose== | ==Article purpose== | ||
The purpose of this article is to: | The purpose of this article is to: | ||
* briefly introduce the PWR peripheral and its main features | * briefly introduce the PWR peripheral and its main features | ||
* indicate the level of security supported by this hardware block | * indicate the level of security supported by this hardware block | ||
* explain how it can be allocated to the | * explain how it can be allocated to the runtime contexts and linked to the corresponding software components | ||
* explain, when necessary, how to configure the PWR peripheral. | * explain, when necessary, how to configure the PWR peripheral. | ||
Line 16: | Line 13: | ||
The '''PWR''' peripheral is used to control the device power supply configuration.<br /> | The '''PWR''' peripheral is used to control the device power supply configuration.<br /> | ||
It has 6 input pins (named wakeup pins) which can be programmed to wake the system up from low power. | It has 6 input pins (named wakeup pins) which can be programmed to wake the system up from low power. The wakeup pins are listed with '''WKUP''' prefix in the [[STM32MP15 resources#DS12505|STM32MP15 Datasheet]]. | ||
These pins can be used by the Cortex<sup>®</sup>-A7 non secure (via Cortex<sup>®</sup>-A7 secure services) or the Cortex<sup>®</sup>-M4. | These pins can be used by the Cortex<sup>®</sup>-A7 non secure (via Cortex<sup>®</sup>-A7 secure services) or the Cortex<sup>®</sup>-M4. | ||
Line 32: | Line 29: | ||
==Peripheral usage and associated software== | ==Peripheral usage and associated software== | ||
===Boot time=== | ===Boot time=== | ||
The PWR is closely configured together with [[RCC internal peripheral|RCC]] by all the [[Boot | The PWR is closely configured together with [[RCC internal peripheral|RCC]] by all the [[Boot chain overview|boot components]]: the ROM code, the FSBL, the SSBL and up to Linux<sup>®</sup> kernel. Its configuration is carried by the [[Device tree|device tree]]. | ||
===Runtime=== | ===Runtime=== | ||
Line 39: | Line 36: | ||
* the Cortex<sup>®</sup>-A7 secure controls all secure registers (cf. TZEN description above) with [[OP-TEE overview|PWR OP-TEE driver]]. | * the Cortex<sup>®</sup>-A7 secure controls all secure registers (cf. TZEN description above) with [[OP-TEE overview|PWR OP-TEE driver]]. | ||
and | and | ||
* the Cortex<sup>®</sup>-A7 non-secure mainly controls it via the [[Regulator overview|regulator framework]] in Linux | * the Cortex<sup>®</sup>-A7 non-secure mainly controls it via the [[Regulator overview|regulator framework]] and the [[Interrupt overview|interrupt framework]] in Linux | ||
and | and | ||
* the Cortex<sup>®</sup>-M4 controls it in STM32Cube with [[STM32CubeMP1 architecture|PWR HAL driver]] | * the Cortex<sup>®</sup>-M4 controls it in STM32Cube with [[STM32CubeMP1 architecture|PWR HAL driver]] | ||
Line 46: | Line 43: | ||
====Software frameworks==== | ====Software frameworks==== | ||
{{: | {{:STM32MP15_internal_peripherals_software_table_template}} | ||
| Power & Thermal | | Power & Thermal | ||
| [[PWR internal peripheral|PWR]] | | [[STM32MP15 PWR internal peripheral|PWR]] | ||
| [[OP-TEE_overview|OP-TEE PWR driver]] | | [[OP-TEE_overview|OP-TEE PWR driver]] | ||
| [[Regulator overview|Linux regulator framework]] | | [[Regulator overview|Linux regulator framework]] | ||
Line 60: | Line 57: | ||
====Peripheral assignment==== | ====Peripheral assignment==== | ||
{{: | {{:STM32MP15_internal_peripherals_assignment_table_template}} | ||
<onlyinclude> | <onlyinclude> | ||
| rowspan="1" | Power & Thermal | | rowspan="1" | Power & Thermal | ||
| rowspan="1" | [[PWR internal peripheral|PWR]] | | rowspan="1" | [[STM32MP15 PWR internal peripheral|PWR]] | ||
| PWR | | PWR | ||
| <span title="system peripheral" style="font-size:21px">✓</span> | | <span title="system peripheral" style="font-size:21px">✓</span> | ||
Line 80: | Line 77: | ||
==References== | ==References== | ||
<references/> | <references/> | ||
<noinclude> | |||
[[Category:Power and Thermal peripherals|PWR internal peripheral STM32MP15]] | |||
{{ArticleBasedOnModel | Internal peripheral article model}} | |||
{{PublicationRequestId | 9334 | 2018-10-31| AlainF}} | |||
</noinclude> |
Latest revision as of 15:25, 1 February 2022
1. Article purpose
The purpose of this article is to:
- briefly introduce the PWR peripheral and its main features
- indicate the level of security supported by this hardware block
- explain how it can be allocated to the runtime contexts and linked to the corresponding software components
- explain, when necessary, how to configure the PWR peripheral.
2. Peripheral overview
The PWR peripheral is used to control the device power supply configuration.
It has 6 input pins (named wakeup pins) which can be programmed to wake the system up from low power. The wakeup pins are listed with WKUP prefix in the STM32MP15 Datasheet.
These pins can be used by the Cortex®-A7 non secure (via Cortex®-A7 secure services) or the Cortex®-M4.
The PWR peripheral provides 2 output hardware lines named PWR_ON and PWR_LP:
- In STPMIC1 configuration, PWR_ON allows to select the register bank (active or low power). PWR_LP is not used.
- In the power discrete solution they drive VDDcore which feeds the Cortex®-A7, the Cortex®-M4 and the peripherals. They also control the DDR power supplies (VDD_DDR, VREF_DDR, VTT_DDR).
2.1. Features
Refer to the STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to see which features are implemented.
2.2. Security support
The PWR is secure aware with the security control managed via RCC TZEN bit.
3. Peripheral usage and associated software
3.1. Boot time
The PWR is closely configured together with RCC by all the boot components: the ROM code, the FSBL, the SSBL and up to Linux® kernel. Its configuration is carried by the device tree.
3.2. Runtime
3.2.1. Overview
The PWR peripheral is shared at runtime:
- the Cortex®-A7 secure controls all secure registers (cf. TZEN description above) with PWR OP-TEE driver.
and
- the Cortex®-A7 non-secure mainly controls it via the regulator framework and the interrupt framework in Linux
and
- the Cortex®-M4 controls it in STM32Cube with PWR HAL driver
A concurrent control from each context is possible because the described management is realized via independent registers.
3.2.2. Software frameworks
Domain | Peripheral | Software components | Comment | ||
---|---|---|---|---|---|
OP-TEE | Linux | STM32Cube | |||
Power & Thermal | PWR | OP-TEE PWR driver | Linux regulator framework | STM32Cube PWR driver |
3.2.3. Peripheral configuration
The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the STM32CubeMX tool for all internal peripherals, and then manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article.
3.2.4. Peripheral assignment
Click on the right to expand the legend...
Domain | Peripheral | Runtime allocation | Comment | |||
---|---|---|---|---|---|---|
Instance | Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) |
Cortex-M4 (STM32Cube) | |||
Power & Thermal | PWR | PWR | ✓ | ✓ | ✓ |
4. How to go further
The PWR is interfaced with the hardware debug port (HDP) of the STM32MP15. This link offers the flexibility to observe the main PWR state signals on debug pins.
Please refer to STM32MP15 reference manuals for the exact list of signals that can be monitored.
5. References