This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User No edit summary |
Registered User mNo edit summary |
||
Line 5: | Line 5: | ||
! STM32MP15 release !! Release note | ! STM32MP15 release !! Release note | ||
|- | |- | ||
| STM32MP15-Ecosystem-v1. | | STM32MP15-Ecosystem-v1.2.0 || [[STM32CubeMP1_Package_release_note_-_v1.2.0]] | ||
|- | |- | ||
| STM32MP15-Ecosystem-v1.1.0 || | | STM32MP15-Ecosystem-v1.1.0 || {{EcosystemFlow/Archives | custom=Basic | flow=v1 | page=STM32CubeMP1_Package_release_note_-_v1.1.0}} | ||
|- | |- | ||
| STM32MP15-Ecosystem-v1. | | STM32MP15-Ecosystem-v1.0.0 || {{EcosystemFlow/Archives | custom=Basic | flow=v1 | page=STM32CubeMP1_Package_release_note_-_v1.0.0}} | ||
|} | |} | ||
Revision as of 14:20, 24 June 2020
STM32CubeMP1 Package release note - v1.2.0
1. Archives 
STM32MP15 release | Release note |
---|---|
STM32MP15-Ecosystem-v1.2.0 | STM32CubeMP1_Package_release_note_-_v1.2.0 |
STM32MP15-Ecosystem-v1.1.0 | STM32CubeMP1_Package_release_note_-_v1.1.0 page for the v1 ecosystem releases (in archived wiki) |
STM32MP15-Ecosystem-v1.0.0 | STM32CubeMP1_Package_release_note_-_v1.0.0 page for the v1 ecosystem releases (in archived wiki) |