Last edited 2 years ago

STM32MP1 Platform trace and debug environment overview: Difference between revisions

Registered User
mNo edit summary
Registered User
mNo edit summary
Line 43: Line 43:
rect 458 390 555 454 [[U-Boot - How to debug | U-Boot]]
rect 458 390 555 454 [[U-Boot - How to debug | U-Boot]]
rect 684 228 800 476 [[STM32CubeMP1 Package | STM32CubeMP1 Package]]
rect 684 228 800 476 [[STM32CubeMP1 Package | STM32CubeMP1 Package]]
rect 78 320 197 380 [[Getting started with ST boards | ComPort connector]]
rect 78 320 197 380 [[:Category:STM32 MPU boards | ComPort connector]]
rect 504 152 625 212 [[Getting started with ST boards | Network link]]
rect 504 152 625 212 [[:Category:STM32 MPU boards | Network link]]
rect 936 328 1058 392 [[Getting started with ST boards | JTag connector]]
rect 936 328 1058 392 [[:Category:STM32 MPU boards | JTag connector]]
rect 1005 411 1124 474 [[Getting started with ST boards | Trace connector]]
rect 1005 411 1124 474 [[:Category:STM32 MPU boards | Trace connector]]
rect 1071 497 1190 559 [[Getting started with ST boards | IOProbe connector]]
rect 1071 497 1190 559 [[:Category:STM32 MPU boards | IOProbe connector]]
rect 672 73 910 139 [[:Category:HW probes]]
rect 672 73 910 139 [[:Category:HW probes]]
<!--
<!--

Revision as of 11:30, 12 December 2019

The block diagram below shows the STM32MP1 Platform trace and debug environment components and their possible interfaces:

  • The STM32MPU Embedded Software package (see STM32MPU Embedded Software architecture overview) that includes:
    • The OpenSTLinux BSP and application frameworks components, running on the Arm® Cortex®-A core
    • The STM32Cube MPU Package running on the Arm® Cortex®-M core
  • The STM32MPU peripherals shared between Cortex®-A and Cortex®-M cores (such as GPIO, I2C and SPI)
  • The user interfaces or tools, which allow to interact with different trace and debug Tools, such as:
    • The remote shell using terminal console
    • The debugger tools (such as GDB)
    • The graphical IDE (such as GDBGUI or SystemWorkbench)
  • The trace and debug interfaces or hardware paths that provide access to trace and debug components through:
    • The network interface (e.g. Ethernet)
    • The communication port (e.g UART)
    • The hardware connector interfaces:
      • JTag port
      • Trace port to access ETM, STM, ITM and SWD
      • I/O probes to access HDP
  • The hardware probes such as ST-Link.


This block diagram also illustrates the Arm® debugging modes:

  • Invasive debug: debug process that allows the control and monitoring of the processor. Most debug features are considered invasive because they enable you to halt the processor and modify its state.
  • Non-invasive debug: debug process that allows the monitoring of the processor but not the control. The embedded trace macrocell (ETM) interface and the performance monitor registers are non-invasive debug features.


Click the figure below to directly jump to the component you want to trace, monitor or debug:

  • By selecting a hardware component, you will be redirected to the corresponding hardware board article in order to check if the hardware connector is supported on your board.
  • By selecting a target software component, you will be be redirected to an article that explains in details how to trace, monitor or debug this component.
  • By selecting a host software component, you will be redirected to an article that explains how to use this remote tool.


Remote shellGDBLinux kernelLinux applicationsOP-TEEOP-TEETF-AU-BootSTM32CubeMP1 PackageComPort connectorNetwork linkJTag connectorTrace connectorIOProbe connectorCategory:HW probes
STM32MP1 Platform trace and debug environment overview.
STM32MP1 Platform trace and debug environment overview legend.png