This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies."Revision ID" is a predefined property of type Number. This property is pre-deployed (also known as special property) and comes with additional administrative privileges but can be used just like any other user-defined property.
C
92068 +
91855 +
96138 +
93021 +
36777 +
93525 +
73532 +
94431 +
90561 +
81938 +
D
85406 +
91791 +
92069 +
93610 +
92509 +
92511 +
93604 +
94257 +
92598 +
92070 +
90537 +
90535 +
94065 +
93815 +
94067 +
66223 +
75159 +
94069 +
92194 +
94395 +
60970 +
92008 +
33119 +
92874 +
92003 +
93621 +
94531 +
94564 +
94534 +
89409 +
94537 +
69390 +
66265 +
96181 +
55416 +
50937 +
51448 +
84355 +
79611 +
79415 +
93913 +
86379 +
86388 +
86386 +
66270 +
41030 +
65470 +
73923 +
86170 +
66237 +
69402 +
88749 +
66271 +
65458 +
90209 +
90237 +
88706 +
95452 +
92709 +
84549 +
93527 +
96151 +
E
88178 +
88179 +
87837 +
87838 +
87839 +
87957 +
87961 +
87963 +
87965 +
87966 +
95628 +
95625 +
95622 +
87015 +
92918 +
93612 +
93614 +
93570 +
61556 +
93173 +
94006 +
71203 +
93439 +
93403 +
93404 +
94188 +
94568 +
93408 +
91867 +
92071 +
91864 +
65457 +
79405 +
78001 +
92072 +
91870 +
91873 +
91876 +
79407 +
46548 +
93705 +
93871 +
93894 +
87933 +
73931 +
50094 +
F
93619 +
93596 +
90560 +
90557 +
92742 +
88680 +