Difference between revisions of "Getting started/STM32MP1 boards/STM32MP157x-EV1/Let's start/Populate the target and boot the image"

[unchecked revision] [quality revision]
m (Populate the SDCard)
m (Boot the board)
 
STM32MP157C-EV1.png
Let's start Develop on Arm® Cortex®-A7
Step category in.png Unpack the board Step.png Populate the target and boot the image Step.png Execute basic commands Step.png Use the demo launcher Step category out.png


1 Overview[edit]

This step explains how to get the Starter Package, then install and boot the STM32MP15 Evaluation boards with the Starter Package.

2 Open a terminal[edit]

Open a terminal on the host computer.

Ubuntu terminal

All the commands preceded by PC $> have to be executed from the host computer terminal.

  • Create your STM32MPU workspace directory on the host computer:
PC $> mkdir $HOME/STM32MPU_workspace
PC $> cd $HOME/STM32MPU_workspace

3 Check the host computer Internet access[edit]

  • An Internet access through http and https protocols must be provided.

The command below enables checking for Internet access through http/https protocols:

PC $> wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You may need to set up a proxy."

If an 'OK' message is returned, the network is correctly configured.
In this case, skip the rest of this section.

Otherwise, a proxy for http/https protocols is required.
The best solution is to set this proxy through the shell variables http_proxy and https_proxy:

PC $> export http_proxy=http://<MyProxyLogin>:<MyProxyPassword>@<MyProxyServerUrl>:<MyProxyPort>
PC $> export https_proxy=http://<MyProxyLogin>:<MyProxyPassword>@<MyProxyServerUrl>:<MyProxyPort>

Check again the Internet access using the command:

PC $> wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You may need to set up a proxy."

4 Install the tools[edit]

4.1 STM32CubeProgrammer[edit]

  • Create your STM32MPU tools directory on the host computer:
PC $> mkdir $HOME/STM32MPU_workspace/STM32MPU-Tools
PC $> mkdir $HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z
  • Create a temporary directory in your STM32MPU workspace:
PC $> mkdir $HOME/STM32MPU_workspace/tmp
Warning.png ecosystem release ≥ v3.0.0 More info.png requires STM32CubeProgrammer V2.7 or higher.
  • Uncompress the archive file to get the STM32CubeProgrammer installers:
PC $> cd $HOME/STM32MPU_workspace/tmp
PC $> unzip SetupSTM32CubeProgrammer.zip
  • Execute the Linux® installer, which guides you through the installation process. Select "$HOME/STM32MPU-Tools/STM32CubeProgrammer-x.y.z" as installation directory when it is requested by the installer.
PC $> ./SetupSTM32CubeProgrammer-x.y.z.linux

The screenshots below have been obtained with STM32CubeProgrammer V2.7.0. They are provided as examples:

Splash screen
Welcome page
Installation path
  • Add the STM32CubeProgrammer binary path to your PATH environment variable:
export PATH=$HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z/bin:$PATH
  • Check that the STM32CubeProgrammer tool is properly installed and accessible:
PC $> STM32_Programmer_CLI --h
     -------------------------------------------------------------------
                       STM32CubeProgrammer vx.y.z                  
     -------------------------------------------------------------------

4.2 USB serial link[edit]

  • Install the libusb on your host computer:
PC $> sudo apt-get install libusb-1.0-0
  • To allow STM32CubeProgrammer to access the USB port through low-level commands, proceed as follows:
PC $> cd $HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z/Drivers/rules
PC $> sudo cp *.* /etc/udev/rules.d/

5 Download the image[edit]

The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found here.

Warning.png To download a package, it is recommended to be logged in to your "myst" account [1]. If, trying to download, you encounter a “403 error”, you could try to empty your browser cache to workaround the problem. We are working on the resolution of this problem.
We apologize for this inconvenience
Warning.png Only microSD cards SanDisk Class 10 and UHS Speed Class 1 are verified. Others are not recommended.
  • Create your STM32MP15 Starter Package directory on the host computer:
PC $> mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0
PC $> mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Starter-Package
PC $> cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Starter-Package
  • Download the STM32MP15-Ecosystem-v3.0.0 Starter Package to the following directory:
    $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Starter-Package
  • Uncompress the tarball file to get the binaries for the different partitions of the image, and the Flash layout files
PC $> tar xvf en.FLASH-stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31.tar.xz


6 Populate the SDCard[edit]

  • Set the boot switches (located at the back of the board) to the OFF position:
boot switches position to flash the board
  • Connect the PC to CN16/USB_OTG port of the STM32MP157x-EV1 mother board through the USB Type A to Type C cable.
  • Power up the board.
  • Press the reset button to reset the board.
  • Launch STM32CubeProgrammer to get the GUI :
STM32CubeProgrammer GUI


  • On the right of the window, select USB (instead of STLINK, set by default) from the connection picklist, and click the "Refresh" button. The serial number is displayed if the USB has been detected.
Select USB for connection with board
  • Click "Connect"
  • Select the "Open File" tab and choose the "FlashLayout_sdcard_stm32mp157c-ev1-trusted.tsv" file or the "FlashLayout_sdcard_stm32mp157f-ev1-trusted.tsv"" file (depending on the board) in the Starter Package installation folder ("$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Starter-Package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/images/stm32mp1/flashlayout_st-image-weston/trusted")
  • Fill the "Binaries Path" by browsing to the $[Starter_Pack_Path]/images/stm32mp1 folder.
open .tsv and fill Binaries Path
  • Click "Download" to launch the flashing process.
  • A progress bar indicates the process progress until a completion pop-up message is displayed.

7 Boot the board[edit]

  • Set the boot switches (located at the back of the board) to the ON position.
boot switches position to boot the board
  • Power on the board.
  • Press the "Reset" button to reset the board.
  • After few seconds, the board starts and automatically goes through the following screens are automatically displayed:
Warning.png The very first boot after flashing takes about 2 minutes so be patient. It takes less than 20 seconds afterwards.
UBoot splash screen
Linux splash screen
Weston desktop
GTK demo launcher


Back button.png Overview button.png Next button.png



<bookshelf src="Book:Getting started" />

{|class="st-table"  style="text-align:center; margin: auto"
| colspan="9" style="border-style: hidden;" | [[Image:STM32MP157C-EV1.png‎ | 65px | link=]]
|-
| colspan="4" style="border-style: hidden; text-align:left;" | [[Getting started/STM32MP1 boards/STM32MP157x-EV1/Let's start | {{GSModuleCurrent|Let's start}}]]
| colspan="5" style="border-style: hidden; text-align:right;" | [[Getting started/STM32MP1 boards/STM32MP157x-EV1/Develop on Arm® Cortex®-A7 |{{GSModuleNext|Develop on Arm® Cortex®-A7}}]]
|-
| style="border-style: hidden;" | [[Image:step_category_in.png|link=]]
| style="border-style: hidden; width:110px;" | [[Getting started/STM32MP1 boards/STM32MP157x-EV1/Let's start/Unpack the STM32MP157x-EV1 board | {{GSStepNext|Unpack the board}}]]
| style="border-style: hidden;" | [[Image:step.png|link=]]
| style="border-style: hidden; width:110px;" | [[Getting started/STM32MP1 boards/STM32MP157x-EV1/Let's start/Populate the target and boot the image | {{GSStepCurrent|Populate the target and boot the image}}]]
| style="border-style: hidden;" | [[Image:step.png|link=]]
| style="border-style: hidden; width:110px;" | [[Getting started/STM32MP1 boards/STM32MP157x-EV1/Let's start/Execute basic commands |{{GSStepNext|Execute basic commands}}]]
| style="border-style: hidden;" | [[Image:step.png|link=]]
| style="border-style: hidden; width:110px;" | [[Getting started/STM32MP1 boards/STM32MP157x-EV1/Let's start/Use the demo launcher | {{GSStepNext|Use the demo launcher}}]]
| style="border-style: hidden;" | [[Image:step_category_out.png|link=]]
|}<br>

==Overview==
This step explains how to get the Starter Package, then install and boot the STM32MP15 Evaluation boards with the Starter Package.

{{:Populate the target and boot the image}}

==Populate the SDCard==

* Set the boot switches (located at the back of the board) to the OFF position:
[[File: STM32MP157x-EVx_jumper_flash.jpg|frame|center|link=|boot switches position to flash the board]]

* Connect the PC to CN16/USB_OTG port of the STM32MP157x-EV1 mother board through the USB Type A to Type C cable.
* Power up the board.
* Press the reset button to reset the board.
* Launch '''STM32CubeProgrammer''' to get the GUI : 
[[File: STM32CubePro GUI_27.png|800px|center|STM32CubeProgrammer GUI]]

* On the right of the window, '''select USB''' (instead of STLINK, set by default) from the connection picklist, and click the "Refresh" button. The serial number is displayed if the USB has been detected. 

[[File: STM32CubePro SelectUSB_27.png|800px|center|Select USB for connection with board]]

*Click "Connect"

* Select the "Open File" tab and choose the "FlashLayout_sdcard_stm32mp157{{highlight|c}}-ev1-trusted.tsv" file or the "FlashLayout_sdcard_stm32mp157{{Highlight|f}}-ev1-trusted.tsv"" file (depending on the board) in the Starter Package installation folder ("$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Starter-Package/{{EcosystemRelease/Package | revision=latest | package=Images package | request=path}}/flashlayout_st-image-weston/trusted")

* Fill the "Binaries Path" by browsing to the $[Starter_Pack_Path]/images/stm32mp1 folder.

[[File: STM32CubePro EV1 TSV and Binary_27.png|800px|center|open .tsv and fill Binaries Path]]

* Click "Download" to launch the flashing process. 
* A progress bar indicates the process progress until a completion pop-up message is displayed.

==Boot the board==
* Set the boot switches (located at the back of the board) to the ON position.
[[File: STM32MP157x-EVx_jumper_boot.jpg|frame|center|link=|boot switches position to boot the board]]
* Power on the board.
* Press the "Reset"  button to reset the board.
* After few seconds, the board starts and automatically goes through the following screensthe following screens are automatically displayed:
{{Warning | The very first boot after flashing takes about 2 minutes so be patient. It takes less than 20 seconds afterwards. }}

[[File: STM32MP1_uboot_splashscreen.png|thumb|upright=2|center|link=|UBoot splash screen]]
[[File: STM32MP1_psplash.png|thumb|upright=2|center|link=|Linux splash screen]]
[[File: STM32MP1_weston_desktop.png|thumb|upright=2|center|link=|Weston desktop]]
[[File: STM32MP1_gtk_demo_launcher.png|thumb|upright=2|center|link=|GTK demo launcher]]
<br>

{| class="st-table" style="margin: auto"
| style="border-style: hidden; width:120px; text-align:left" | [[Image:back_button.png|link=Getting started/STM32MP1 boards/STM32MP157x-EV1/Let's start/Unpack the STM32MP157x-EV1 board]]
| style="border-style: hidden; width:360px; text-align:center" | [[Image:overview_button.png|link=Getting started/STM32MP1 boards/STM32MP157x-EV1]]
| style="border-style: hidden; width:120px; text-align:right" | [[Image:next_button.png|link=Getting started/STM32MP1 boards/STM32MP157x-EV1/Let's start/Execute basic commands]]
|}
<noinclude>

[[Category:STM32MP157x-EV1 - Let's start | 02]]
{{DISPLAYTITLE:{{SUBPAGENAME}}}}
__NOTOC__
{{PublicationRequestId | 19647 | 2021-04-19}}</noinclude>
Line 54: Line 54:
 
* Power on the board.
 
* Power on the board.
 
* Press the "Reset"  button to reset the board.
 
* Press the "Reset"  button to reset the board.
* After few seconds, the board starts and the following screens are automatically displayed:
+
* After few seconds, the board starts and automatically goes through the following screens:
 
{{Warning | The very first boot after flashing takes about 2 minutes so be patient. It takes less than 20 seconds afterwards. }}
 
{{Warning | The very first boot after flashing takes about 2 minutes so be patient. It takes less than 20 seconds afterwards. }}