Registered User m (→Boot the board) |
Registered User |
||
(24 intermediate revisions by 5 users not shown) | |||
Line 1: | Line 1: | ||
<bookshelf src="Book:Getting started" /> | <bookshelf src="Book:Getting started" /> | ||
<noinclude>{{ApplicableFor | |||
|MPUs list=STM32MP15x | |||
|MPUs checklist=STM32MP13x, STM32MP15x | |||
}}</noinclude> | |||
{| class="st-table" style="text-align:center; margin: auto" | {| class="st-table" style="text-align:center; margin: auto" | ||
| colspan="9" style="border-style: hidden;" | [[Image:STM32MP157X-DK2.png | 80px | link=]] | | colspan="9" style="border-style: hidden;" | [[Image:STM32MP157X-DK2.png | 80px | link=]] | ||
Line 18: | Line 23: | ||
<br> | <br> | ||
==Overview== | ==Overview== | ||
This | This step explains how to get the Starter Package, then install and boot the STM32MP15 Discovery kit with the Starter Package. | ||
{{:Populate the target and boot the image}} | {{:Populate the target and boot the image}} | ||
==Populate the SDCard== | ==Populate the SDCard== | ||
* Set the boot switches (located at the back of the board) to the | * Set the boot switches (located at the back of the board) to the OFF position. | ||
[[File: STM32MP157C-DK2_jumper_flash.jpg|frame|center|link=|boot switches position to flash the board]] | [[File: STM32MP157C-DK2_jumper_flash.jpg|frame|center|link=|boot switches position to flash the board]] | ||
* Connect | * Connect the PC to the CN7/USB_OTG port of the STM32MP157x-DK2 board through the USB Type A to Type C cable. | ||
* Power | * Power on the board. | ||
* Press the reset button to reset the board | * Press the reset button to reset the board. | ||
* Launch '''STM32CubeProgrammer''' to get the GUI | * Launch '''STM32CubeProgrammer''' to get the GUI: | ||
[[File: STM32CubePro GUI.png|800px|center|STM32CubeProgrammer GUI]] | [[File:STM32CubePro GUI 210.png|800px|center|STM32CubeProgrammer GUI]] | ||
* On the right, select USB ( | * On the right of the window, select USB (instead of STLINK, set by default) in the connection picklist and click the "Refresh" button. The serial number is displayed if the USB is detected. Then click "Connect". | ||
[[File: STM32CubePro SelectUSB.png|800px|center|Select USB for connection with board]] | [[File:STM32CubePro GUI 210 SelectUSB.png|800px|center|Select USB for connection with board]] | ||
* | * Select the "Open File" tab and choose the "FlashLayout_sdcard_stm32mp157{{Highlight|x}}-dk2-optee.tsv" file in the Starter Package installation folder ("$HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v4.0.0/Starter-Package/{{EcosystemRelease/Package | revision=latest| package=Images package | request=path}}/flashlayout_st-image-weston/optee") | ||
* Fill the "Binaries Path" by browsing to the $[Starter_Pack_Path]/images/stm32mp1 folder. | |||
* Click | [[File:STM32CubePro GUI 210 FileSelectedOptee.png|800px|center|open .tsv and fill Binaries Path]] | ||
* | |||
* Click "Download" to start the flashing process. | |||
* A progress bar indicates the process progress until a completion pop-up message is displayed. | |||
==Boot the board== | ==Boot the board== | ||
* Set the boot switches (located at the back of the board) to the ON position | * Set the boot switches (located at the back of the board) to the ON position: | ||
[[File: STM32MP157C-DK2_jumper_boot.jpg|frame|center|link=|boot switches position to boot the board]] | [[File: STM32MP157C-DK2_jumper_boot.jpg|frame|center|link=|boot switches position to boot the board]] | ||
* Power | * Power on the board. | ||
* Press the "Reset "button to reset the board | * Press the "Reset "button to reset the board. | ||
* After few seconds, the board starts and automatically goes through the following screens | * After few seconds, the board starts and automatically goes through the following screens | ||
{{Warning | | |||
{{Warning | The very first boot after flashing takes about 2 minutes so be patient. It takes less than 20 seconds afterwards. }} | |||
[[File: STM32MP1_uboot_splashscreen.png|thumb|upright=2|center|link=|UBoot splash screen]] | [[File: STM32MP1_uboot_splashscreen.png|thumb|upright=2|center|link=|UBoot splash screen]] | ||
Line 58: | Line 65: | ||
[[File: STM32MP1_gtk_demo_launcher.png|thumb|upright=2|center|link=|GTK demo launcher]] | [[File: STM32MP1_gtk_demo_launcher.png|thumb|upright=2|center|link=|GTK demo launcher]] | ||
:* If the board power supply | :* If the board power supply does not supply enough current (3A), the red LED indicates the issue following the rules below: | ||
:::{| | :::{| | ||
! | ! LED blinking mode | ||
! | ! Console message | ||
! | ! Boot process | ||
|- | |- | ||
| | | Twice | ||
| WARNING 500mA power supply detected | | WARNING 500mA power supply detected | ||
Current too low, use a 3A power supply! | Current too low, use a 3A power supply! | ||
Line 95: | Line 102: | ||
__NOTOC__ | __NOTOC__ | ||
[[Category:STM32MP157x-DK2 - let's start | 02]] | [[Category:STM32MP157x-DK2 - let's start | 02]] | ||
{{PublicationRequestId | | {{PublicationRequestId | 19647 | 2021-04-19}} | ||
</noinclude> | </noinclude> |
Revision as of 17:11, 23 June 2022
1. Overview[edit | edit source]
This step explains how to get the Starter Package, then install and boot the STM32MP15 Discovery kit with the Starter Package.
2. Open a terminal[edit | edit source]
Open a terminal on the host computer.

All the commands preceded by PC $> have to be executed from the host computer terminal.
- Create your STM32MPU workspace directory on your host computer
PC $> mkdir $HOME/STM32MPU_workspace PC $> cd $HOME/STM32MPU_workspace
3. Check the host computer Internet access[edit | edit source]
- An Internet access through http and https protocols must be provided.
The command below allows to check for Internet access through http/https protocols:
PC $> wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You may need to set up a proxy."
If an 'OK' message is returned, the network is well configured.
In such case, skip the rest of this section.
Any other likely situation indicates the need for a proxy for http/https protocols.
The best solution to set a proxy for http/https protocols is via the shell variables http_proxy and https_proxy:
PC $> export http_proxy=http://<MyProxyLogin>:<MyProxyPassword>@<MyProxyServerUrl>:<MyProxyPort> PC $> export https_proxy=http://<MyProxyLogin>:<MyProxyPassword>@<MyProxyServerUrl>:<MyProxyPort>
Check again the Internet access with command:
PC $> wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You may need to set up a proxy."
4. Install the tools[edit | edit source]
4.1. STM32CubeProgrammer[edit | edit source]
![]() |
|
- Create your STM32MPU tools directory on your host computer
PC $> mkdir $HOME/STM32MPU_workspace/STM32MPU-Tools PC $> mkdir $HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z
- Create a temporary directory in your STM32MPU workspace
PC $> mkdir $HOME/STM32MPU_workspace/tmp
- Download latest STM32CubeProgrammer in the following directory
$HOME/STM32MPU_workspace/tmp
![]() |
ecosystem release v2.0.0 ![]() |
- Uncompress the archive file to get the STM32CubeProgrammer installers
PC $> cd $HOME/STM32MPU_workspace/tmp PC $> unzip SetupSTM32CubeProgrammer.zip
- Execute the Linux installer, which guides you through the installation process. Select "$HOME/STM32MPU-Tools/STM32CubeProgrammer-x.y.z" as the installation directory, when it's requested by the installer
PC $> ./SetupSTM32CubeProgrammer-x.y.z.linux
Screenshots, done with STM32CubeProgrammer V2.2.0, are given as examples below:

- Add the STM32CubeProgrammer binary path to your PATH environment variable
export PATH=$HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z/bin:$PATH
- Check that the STM32CubeProgrammer tool is properly installed and accessible
PC $> STM32_Programmer_CLI --h ------------------------------------------------------------------- STM32CubeProgrammer vx.y.z -------------------------------------------------------------------
4.2. USB serial link[edit | edit source]
- Install the libusb on your host computer
PC $> sudo apt-get install libusb-1.0-0
- To allow STM32CubeProgrammer to access the USB port through low-level commands, proceed as follows
PC $> cd $HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z/Drivers/rules PC $> sudo cp *.* /etc/udev/rules.d/
5. Download the image[edit | edit source]
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found here.
![]() |
To download a package, it is recommended to be logged in to your "myst" account [1]. If, trying to download, you encounter a “403 error”, you could try to empty your browser cache to workaround the problem. We are working on the resolution of this problem. We apologize for this inconvenience |
For ecosystem release v2.0.0
[edit | edit source]
- Create your STM32MP15 Starter Package directory on your host computer
PC $> mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.0.0 PC $> mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.0.0/Starter-Package PC $> cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.0.0/Starter-Package
- Download the STM32MP15-Ecosystem-v2.0.0 Starter Package to the following directory:
$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.0.0/Starter-Package - Uncompress the tarball file to get the binaries for the different partitions of the image, and the Flash layout files
PC $> tar xvf en.FLASH-stm32mp1-openstlinux-5-4-dunfell-mp1-20-06-24.tar.xz
6. Populate the SDCard[edit | edit source]
- Set the boot switches (located at the back of the board) to the OFF position.

- Connect the PC to the CN7/USB_OTG port of the STM32MP157x-DK2 board through the USB Type A to Type C cable.
- Power on the board.
- Press the reset button to reset the board.
- Launch STM32CubeProgrammer to get the GUI:
- On the right of the window, select USB (instead of STLINK, set by default) in the connection picklist and click the "Refresh" button. The serial number is displayed if the USB is detected. Then click "Connect".
- Select the "Open File" tab and choose the "FlashLayout_sdcard_stm32mp157x-dk2-optee.tsv" file in the Starter Package installation folder ("$HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v4.0.0/Starter-Package/stm32mp1-openstlinux-5.4-dunfell-mp1-20-06-24/images/stm32mp1/flashlayout_st-image-weston/optee")
- Fill the "Binaries Path" by browsing to the $[Starter_Pack_Path]/images/stm32mp1 folder.
- Click "Download" to start the flashing process.
- A progress bar indicates the process progress until a completion pop-up message is displayed.
7. Boot the board[edit | edit source]
- Set the boot switches (located at the back of the board) to the ON position:

- Power on the board.
- Press the "Reset "button to reset the board.
- After few seconds, the board starts and automatically goes through the following screens
![]() |
The very first boot after flashing takes about 2 minutes so be patient. It takes less than 20 seconds afterwards. |
- If the board power supply does not supply enough current (3A), the red LED indicates the issue following the rules below:
LED blinking mode Console message Boot process Twice WARNING 500mA power supply detected Current too low, use a 3A power supply!
Continue and red LED stays ON 3 times WARNING 1500mA power supply detected Current too low, use a 3A power supply!
Continue and red LED stays ON forever ERROR USB TYPE-C connection in unattached mode Check that USB TYPE-C cable is correctly plugged
stop forever USB TYPE-C charger not compliant with USB specification stop