Registered User mNo edit summary |
Registered User No edit summary |
||
Line 23: | Line 23: | ||
<br> | <br> | ||
{{:Modify, rebuild and reload a firmware}} | {{:Modify, rebuild and reload a firmware | board_type=STM32MP157C-DK2}} | ||
<br> | <br> |
Revision as of 18:34, 5 March 2019
![]() | ||||||
Develop on Arm® Cortex®-M4 | What's next | |||||
![]() |
Install the IDE | ![]() |
Install STM32Cube MP1 package | ![]() |
Modify, rebuild and reload a firmware | ![]() |
1. Overview[edit | edit source]
This stage explains how to modify, rebuild, and reload an STM32MP1 Arm® Cortex®-M4 coprocessor firmware.
It proposes to customize the STM32MP1Cube package application example OpenAMP_TTY_Echo
using STM32CubeIDE.
2. Disconnect the "minicom" console[edit | edit source]
- If
minicom
is already opened, please disconnect it to use the STM32CubeIDE built-in serial console.
Ctrl + A then Q
3. Open STM32CubeIDE[edit | edit source]
- Start STM32CubeIDE.
- Choose a workspace (default is fine).
- Notice information provided in the
Information Center page
and close it. (You can open it later.)

- Go into your workspace projet view.

4. Import an existing example in STM32CubeIDE[edit | edit source]
- In the
File
menu, selectImport
. Then, chooseExisting Project into Workspace
.
- Browse and select the
OpenAMP_TTY_echo
application example in the folder matching your board :
$HOME/STM32MPU_workspace/STM32MPU-Ecosystem-v6.1.06.1.0/Developer-Package/STM32Cube_FW_MP1_V1.7.0/Projects/STM32MP157C-DK2/Applications/OpenAMP/OpenAMP_TTY_echo/STM32CubeIDE
or
$HOME/STM32MPU_workspace/STM32MPU-Ecosystem-v6.1.0/Developer-Package/STM32Cube_FW_MP1_V1.7.0/Projects/STM32MP157C-EV1/Applications/OpenAMP/OpenAMP_TTY_echo/STM32CubeIDE
- STM32CubeIDE brings a specific project structure for dual-core devices such as STM32MP1. A top-level project contains sub-projects for each core.
- Here, the
OpenAMP_TTY_echo
top project contains theOpenAMP_TTY_echo_CM4
sub-project. Keep the two projects selected and click onFinish
.
- The
OpenAMP_TTY_echo
project is open, and you can browse inside using the left panel.
5. Build the firmware[edit | edit source]
- In the
OpenAMP_TTY_Echo_CM4
project, click theBuild
button (the little hammer in the toolbar).

- "Build" is finished with no errors.

6. Check connection to the target[edit | edit source]
STM32CubeIDE requires a connection to Linux running on an STM32MP1 device though serial connection.
This connection is automatically detected and configured when you connect the cable to the ST-Link port and the board has booted.
You can check if you can get the Linux log and prompt by clicking on the STM32 butterfly
button :
The connection is correct if the Linux log or prompt is displayed in the console window.

Your board might be connected to the PC by Ethernet, either using RJ45 (point-to-point or VLAN) or USB0 EthernetOverUSB gadget (point-to-point connection with PC using TypeA-TypeC cable). The screenshot below uses the second solution.
When a serial connection is established, STM32CubeIDE automatically detects the board IP address and displays it in the Serial Target widget status
window in the bottom right part of the screen.
In case of different statuses such as busy
or console in use
, check that you have no other terminal connected and close the console.
In case of a different status such as Stopped
, right-click on it and select Start
.
7. Start Debug Session[edit | edit source]
- Click on your
OpenAMP_TTY_echo_CM4
project to select it.
- If not already created, create your debug configuration by right-clicking on
OpenAMP_TTY_echo_CM4
and selectingDebug As
andSTM32 C/C++ Application
. It will open theEdit Configuration
window.

- Check if the IP address is correctly filled (1). Otherwise, you can force detection using the button on the right (2).
- Ensure the
Thru Linux core
(production mode)" is selected (3). - When the configuration is correct, the
Debug
button (5) becomes active, and you can launch the debug session. Otherwise, an error message appears in area (4).
STM32CubeIDE needs to use a serial connection to the board to manage firmware download.
If the console is open, it will request your approval to close it. Answer yes
.
The debug in "production mode" adds the Cortex-M firmware transfer to the embedded Linux. In case of network usage, some specific pop-up appears:
- The
SSH Password
must be completed: the default one isroot
.
- the
RSA key
must be approved.
After firmware download, STM32CubeIDE switches into the Debug Perspective
.
In "production mode", the firmware does not break at main. GDB is simply attached to the running target. You can then use all features of the debugger.
![]() |
To benefit of the best GDB debug experience it's recommended to upgrade the onboard ST-Link version with the latest release. You can simply do it from STM32CubeIDE using menu Help -> ST-Link Upgrade
|
For further information, refer to STM32CubeIDE documentation avaialble inmy.st.com
8. Test the firmware[edit | edit source]
The OpenAMP_TTY_echo_CM firmware performs the following:
- CPU2(CM4) initializes OpenAMP middleware, which initializes and configures the IPCC peripheral through HAL and sets up the OpenAMP-RPMsg framework infrastructure.
- CPU2(CM4) creates two RPMsg channels for two virtual UART instances (UART0 and UART1).
- CPU2(CM4) waits for messages from CPU1(CA7) on both channels.
- When CPU2(CM4) receives a message on one Virtual UART instance/RPMsg channel, it sends the message back to CPU1(CA7) on the same virtual UART instance.
Reopen the serial console of STM32CubeIDE and enter following commands :
- Initialize the
ttyRPMSG0
configuration.
stty -onlcr -echo -F /dev/ttyRPMSG0
- Read constantly the ttyRPMSG0 channel in background.
cat /dev/ttyRPMSG0 &
- Send a message on one ttyRPMSG0 channel and receive the echo on the same ttyRPMSG0 channel.
echo "Hello Virtual UART0" > /dev/ttyRPMSG0
Hello Virtual UART0
- You can perform the same steps with the ttyRPMSG1 channel.
- Terminate the STM32CubeIDE debug session will stop the firmware.
9. Modify the firmware[edit | edit source]
The original firmware example receives a message for the host on one channel and acknowledges by returning the same message to the host on the same channel.
As it is not obvious on which channel the message is received on, we propose modifying the firmware to add an indication to identify the channel receiving the message.
To do this, please modify the original main.c
code as follows:
char msg_to_transmit[MAX_BUFFER_SIZE]; int msg_size = 0; VirtUart0RxMsg = RESET; msg_size = snprintf(msg_to_transmit, MAX_BUFFER_SIZE, "Channel RPMSG0: "); msg_size += snprintf(msg_to_transmit + msg_size, MAX_BUFFER_SIZE, "%s\n", VirtUart0ChannelBuffRx); log_info("size of the message to transmit = %d bytes\n", msg_size); VIRT_UART_Transmit(&huart0, (uint8_t*)msg_to_transmit, msg_size); } if (VirtUart1RxMsg) { char msg_to_transmit[MAX_BUFFER_SIZE]; uint16_t msg_size = 0; VirtUart1RxMsg = RESET; msg_size = snprintf(msg_to_transmit, MAX_BUFFER_SIZE, "Channel RPMSG1: "); msg_size += snprintf(msg_to_transmit + msg_size, MAX_BUFFER_SIZE, "%s\n", VirtUart1ChannelBuffRx); log_info("size of the message to transmit = %d bytes\n", msg_size); VIRT_UART_Transmit(&huart1, (uint8_t*)msg_to_transmit, msg_size); } /* USER CODE BEGIN 3 */ } /* USER CODE END 3 *//* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { OPENAMP_check_for_message(); /* USER CODE END WHILE */ if (VirtUart0RxMsg) {
- Save your modifications.
10. Testing the modified firmware[edit | edit source]
10.1. Relaunch debug session[edit | edit source]
- By clicking on the
Debug
button, STM32CubeIDE relaunches the debug session after performing an incremental build to take into account your modification.
- If everything is correct, you will switch back to the
Debug Perspective
window after reloading the new firmware.
10.2. Test[edit | edit source]
- Initialize the
ttyRPMSG0
andttyRPMSG1
configurations.
stty -onlcr -echo -F /dev/ttyRPMSG0
stty -onlcr -echo -F /dev/ttyRPMSG1
- Read constantly the
ttyRPMSG0
andttyRPMSG1
channels in the background.
cat /dev/ttyRPMSG0 &
cat /dev/ttyRPMSG1 &
- Send a message on one
ttyRPMSG0
channel and check the echo log.
echo "Hello Virtual UART0" > /dev/ttyRPMSG0
Channel RPMSG0: Hello Virtual UART0
- Send a message on one
ttyRPMSG1
channel and check the echo log.
echo "Hello Virtual UART1" > /dev/ttyRPMSG1
Channel RPMSG1: Hello Virtual UART1
![]() |
When the firmware is running, you can output log from the firmware by using the following command:
cat /sys/kernel/debug/remoteproc/remoteproc0/trace0 |
- Terminate the STM32CubeIDE debug session.