Some typical issues related to the management of a coprocessor are listed below. Solutions or debugging methods are proposed for these issues.
If your issue is not listed, try looking in the articles in the Coprocessor management Linux, Coprocessor management STM32Cube or troubleshooting grids categories.
1. Coprocessor firmware loading and control[edit | edit source]
Symptom | Resolution |
---|---|
The coprocessor traces are not available on Linux® side
cat /sys/kernel/debug/remoteproc/remoteproc0/trace0
No such file or directory
|
This may happen for two reasons:
readelf -l <elf file>
...
02 .data .resource_table .bss ._user_heap_stack
....
|
When starting the coprocessor from the bootloader (u-boot):
"unsupported fw ver: 0
Remote Processor 0 resource table Not found : 0x00000000-0x0 "
|
The firmware does not include any resource table. This is only a warning that does not prevent the firmware from starting properly. "rproc load_rsc" step can be bypassed. |
When Loading a signed firmware from OP-TEE:
"remoteproc remoteproc0: bad phdr da 0x80123db8 mem 0x7f36a8"
|
There is probably a mismatch between the firmware memory mapping and the memory regions declared in the Linux remoteproc device tree. Use the following command to verify it in the generated elf file:
readelf -l <elf file>
and compare the elf program header with the OPTEE device tree reserved-memory declaration. |
When Loading a signed firmware from OP-TEE: TA: remoteproc_load_segment:887 Fails to clear segment, res = 0xffff0001""E/ |
There is probably a mismatch between the firmware memory mapping and the memory regions declared in the OP-TEE remoteproc device tree. Use the following command to verify it in the generated elf file:
readelf -l <elf file>
and compare the elf program header with the OPTEE device tree reserved-memory declaration. |
When Loading a signed firmware from OP-TEE: TA: remoteproc_load_fw:1014 Can't Authenticate the firmware <res = 0xFFFF0000>""E/ |
This means the OP-TEE remoteproc framework detect something not valid in the the firmware format. The root cause can be:
cat sys/class/remoteproc/remoteproc0/fw_format
See Firmware_signature for details |
2. Inter processor communication[edit | edit source]
Symptom | Resolution |
---|---|
Frozen firmware as consequence of a deadlock in OpenAMP during IP communication with the the main processor. |
This Issue probably comes from rpmsg_virtio_rx_callback or rpmsg_virtio_send_offchannel_raw (rpmsg_virtio.c) functions that are called in interrupt context. These functions use a mutex lock in rpmsg_device struct when accessing the index of the virtio queue index. Rework your code so that these functions are not called in interrupt context. |
Linux kernel trace: TX_QUEUE_LENstm32-ipcc 4c001000.mailbox: Try increasing MBOX_ |
|
Linux kernel trace ( example with rpmsg_tty driver):
rpmsg_tty virtio0.rpmsg-tty-channel.-1.0: timeout waiting for a tx buffer
|
This message means that there is no more TX buffer available to transmit messages to the remote processor. This may happen for two reasons:
|
Linux kernel trace:
rpmsg_tty virtio0.rpmsg-tty-channel.-1.0: No memory for tty_prepare_flip_string
|
There is no more space in the TTY temporary buffer on reception. The root cause is probably that the Linux application did not read the tty device on time to treat the incoming TTY stream. Consider reworking the Linux application so that it takes less time to process messages or decreasing the message exchange rate. |
Linux kernel trace:
remoteproc remoteproc0: stm32_rproc_kick: failed (<mbx>, <error value>)
|
The Linux remoteproc driver cannot use the IPCC mailbox. This may happen for two reasons:
|
stm32Cube error:
VIRT_UART_Transmit() returns an error until a first message |
Before the Cortex-M can send any message, the RPMsg protocol requires that the Linux application has sent a first message (to provide its address to the Cortex-M). The Linux and/or the Cortex-M applications shall be reworked to follow this constraint. |