1. Article purpose[edit | edit source]
The purpose of this article is to:
- briefly introduce the SYSCFG peripheral and its main features,
- indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
- list the software frameworks and drivers managing the peripheral,
- explain how to configure the peripheral.
2. Peripheral overview[edit | edit source]
The SYSCFG peripheral is used to configure various system aspects like IOs compensation, Ethernet clocking path, …
Refer to the STM32 MPU reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.
3. Peripheral usage[edit | edit source]
This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.
3.1. Boot time assignment[edit | edit source]
3.1.1. On STM32MP1 series[edit | edit source]
The SYSCFG peripheral is configured by TF-A and U-Boot at boot time.
Click on to expand or collapse the legend...
Domain | Peripheral | Boot time allocation | Comment ![]() | |||
---|---|---|---|---|---|---|
Instance | Cortex-A7 secure (ROM code) |
Cortex-A7 secure (TF-A BL2) |
Cortex-A7 non-secure (U-Boot) | |||
Core | SYSCFG | SYSCFG | ✓ | ☑ | ☑ |
3.1.2. On STM32MP2 series[edit | edit source]
Click on to expand or collapse the legend...
Domain | Peripheral | Boot time allocation | Comment ![]() | |||
---|---|---|---|---|---|---|
Instance | Cortex-A35 secure (ROM code) |
Cortex-A35 secure (TF-A BL2) |
Cortex-A35 non-secure (U-Boot) | |||
Core | SYSCFG | SYSCFG | ✓ | ☑ | ☑ |
3.2. Runtime assignment[edit | edit source]
3.2.1. On STM32MP13x lines
[edit | edit source]
Click on to expand or collapse the legend...
Domain | Peripheral | Runtime allocation | Comment ![]() | ||
---|---|---|---|---|---|
Instance | Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) | |||
Core | SYSCFG | SYSCFG | ☑ | ☑ |
3.2.2. On STM32MP15x lines
[edit | edit source]
Click on to expand or collapse the legend...
Domain | Peripheral | Runtime allocation | Comment ![]() | |||
---|---|---|---|---|---|---|
Instance | Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) |
Cortex-M4 (STM32Cube) | |||
Core | SYSCFG | SYSCFG | ☑ | ☑ | ☑ |
3.2.3. On STM32MP25x lines
[edit | edit source]
Click on to expand or collapse the legend...
Domain | Peripheral | Runtime allocation | Comment ![]() | |||||
---|---|---|---|---|---|---|---|---|
Instance | Cortex-A35 secure (OP-TEE / TF-A BL31) |
Cortex-A35 non-secure (Linux) |
Cortex-M33 secure (TF-M) |
Cortex-M33 non-secure (STM32Cube) |
Cortex-M0+![]() (STM32Cube) | |||
Core | SYSCFG | SYSCFG | ☑ | ☑ | ☑ | ☑ |
4. Software frameworks and drivers[edit | edit source]
Below are listed the software frameworks and drivers managing the SYSCFG peripheral for the embedded software components listed in the above tables.
Linux and STM32Cube can directly change the SYSCFG at runtime from various drivers.
- Linux®: for example, Linux I2C driver uses the syscon framework[1] to enable the I2C fast mode plus (FM+) in the SYSCFG for the instances allocated to itself
- STM32Cube: for example, I2C HAL driver uses its SYSCFG HAL driver to do the same on the instances allocated to itself
5. How to assign and configure the peripheral[edit | edit source]
The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:
- partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
- HAL initialization code generation for the STM32CubeMPU Package.
The configuration is applied by the firmware running in the context in which the peripheral is assigned.
6. References[edit | edit source]