Template:ArticleMainWriter Template:ArticleApprovedVersion
1. Purpose[edit | edit source]
This article shows two ways to control a GPIO in userspace:
- using libgpiod
- by writing an application
2. GPIO control through libgpiod[edit | edit source]
libgpiod provides a C library and tools for interacting with the linux GPIO character device (gpiod stands for GPIO device). See the libgpiod repository[1] for further explanation.
- gpiodetect
- List all gpiochips present on the system
- Usage:
Template:Board$ gpiodetect gpiochip11 [GPIOZ] (16 lines)
...
gpiochip0 [GPIOA] (16 lines)
- gpioinfo
- list all lines of specified gpiochips, their names, consumers, and their settings
- Usage:
Template:Board$gpioinfo gpiochip11 - 16 lines: line 0: unnamed unused input active-high line 1: unnamed unused input active-high ...
or
Template:Highlight Template:Board$gpioinfo gpiochip0 Template:Highlight
- gpioget
- Read the values of the specified GPIO lines (not valid if the line is already requested)
Template:Highlight Template:Board$gpioget gpiochip0 5 Template:Highlight 0 Template:Highlight
- gpioset
- Set the values of the specified GPIO lines, potentially keeping the lines exported, and wait until timeout, user input or signal.
Template:Board$gpioset gpiochip3 8=1 Template:Highlight
Template:ReviewsComments Template:ReviewsComments Template:ReviewsComments
3. GPIO control through your own application[edit | edit source]
3.1. Purpose[edit | edit source]
This application toggles GPIO_A_14 (GPIO bank A, line 14). On STM32MP15_Evaluation_boards or STM32MP15_Discovery_kits GPIO_A_14 is connected to the green LED. Template:ReviewsComments This application must be cross compiled with same toolchain as the Kernel.
3.2. Code[edit | edit source]
GPIO bank A */ fd = open(chrdev_name, 0); if (fd == -1) { ret = -errno; fprintf(stderr, "Failed to open %s\n", chrdev_name); return ret; } /* request GPIO line: GPIO_A_14 */ req.lineoffsets[0] = 14; req.flags = GPIOHANDLE_REQUEST_OUTPUT; memcpy(req.default_values, &data, sizeof(req.default_values)); strcpy(req.consumer_label, "led_gpio_a_14"); req.lines = 1; ret = ioctl(fd, GPIO_GET_LINEHANDLE_IOCTL, &req); if (ret == -1) { ret = -errno; fprintf(stderr, "Failed to issue GET LINEHANDLE IOCTL (%d)\n", ret); } if (close(fd) == -1) perror("Failed to close GPIO character device file"); free(chrdev_name); /* Start led blinking */ while(1) { data.values[0] = !data.values[0]; ret = ioctl(req.fd, GPIOHANDLE_SET_LINE_VALUES_IOCTL, &data); if (ret == -1) { ret = -errno; fprintf(stderr, "Failed to issue %s (%d)\n", "GPIOHANDLE_SET_LINE_VALUES_IOCTL", ret); } sleep(1); } /* release line */ ret = close(req.fd); if (ret == -1) { perror("Failed to close GPIO LINEHANDLE device file"); ret = -errno; } return ret; }#include <errno.h> #include <fcntl.h> #include <stdio.h> #include <stdlib.h> #include <string.h> #include <sys/ioctl.h> #include <unistd.h> #include <linux/gpio.h> int main(int argc, char **argv) { struct gpiohandle_request req; struct gpiohandle_data data; char chrdev_name[20] = NULL; int fd, ret; strcpy(chrdev_name, "/dev/gpiochip0"); /* Open device: gpiochip0 for
3.3. Build application[edit | edit source]
See Adding_Linux_user_space_applications to build this application.