Last edited 7 months ago

I3C internal peripheral


1. Article purpose[edit | edit source]

The purpose of this article is to:

  • briefly introduce the I3C peripheral and its main features,
  • indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
  • list the software frameworks and drivers managing the peripheral,
  • explain how to configure the peripheral.

2. Peripheral overview[edit | edit source]

The I3C peripheral is used to handle communication between this device and others, such as sensors and host processors connected on an I3C bus.
An I3C bus is a two-wire, serial single-ended, multidrop bus, intended to improve a legacy I2C bus.
This I3C peripheral is SDR-only (single data rate) and implements all the features required by the MIPI® I3C specification v1.1.
It can control all I3C bus-specific sequencing, protocol, arbitration, and timing, and can act as controller (formerly known as master), or as target (formerly known as slave).
When acting as controller, the I3C peripheral improves the features on the I2C interface preserving some backward compatibility: it allows an I2C target to operate on an I3C bus in legacy I2C fast mode (Fm) or legacy I2C fast mode plus (Fm+), provided that the latter does not perform clock stretching.

For more information about I3C, refer to this link: MIPI® I3C Wikipedia page [1] or MIPI® I3C[2].

Here are the main features:

  • MIPI® I3C specification v1.1, as:
    • I3C SDR-only primary controller
    • I3C SDR-only secondary controller
    • I3C SDR-only target
  • I3C SCL bus clock frequency up to 12.5 MHz
  • Messages:
    • Legacy I2C read/write messages to legacy I2C targets in Fm/Fm+
    • I3C SDR read/write private messages
    • I3C SDR broadcast CCC messages
    • I3C SDR read/write direct CCC messages

Refer to the STM32 MPU reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.

3. Peripheral usage[edit | edit source]

This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor, and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.

3.1. Boot time assignment[edit | edit source]

3.1.1. On STM32MP2 series[edit | edit source]

Click on How to.png to expand or collapse the legend...

Domain Peripheral Boot time allocation Comment How to.png
Instance Cortex-A35
secure
(ROM code)
Cortex-A35
secure
(TF-A BL2)
Cortex-A35
non-secure
(U-Boot)
Low speed interface I3C I3C1
I3C2
I3C3
I3C4

3.2. Runtime assignment[edit | edit source]

3.2.1. On STM32MP25x lines More info.png[edit | edit source]

Click on How to.png to expand or collapse the legend...

Domain Peripheral Runtime allocation Comment How to.png
Instance Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
non-secure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
non-secure
(STM32Cube)
Cortex-M0+
Warning.png
(STM32Cube)
Low speed interface I3C I3C1 OP-TEE
TF-A BL31
I3C2 OP-TEE
TF-A BL31
I3C3 OP-TEE
TF-A BL31
I3C4 OP-TEE
TF-A BL31

4. Software frameworks and drivers[edit | edit source]

Below are listed the software frameworks and drivers managing the I3C peripheral for the embedded software components listed in the above tables.

  • Linux®: I3C SDR-only primary controller as defined in MIPI® I3C specification v1.1 in I3C driver

5. How to assign and configure the peripheral[edit | edit source]

The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral by generating:

  • partial device trees (pin control and clock tree) for the OpenSTLinux software components,
  • HAL initialization code for the STM32CubeMPU Package.

The configuration is applied by the firmware running in the context in which the peripheral is assigned.

6. References[edit | edit source]