1. Overview[edit | edit source]
This article explains how to stream camera content over network thanks to GStreamer application on top of V4L2 Linux® kernel framework.
This article focuses on camera sensors that does not output compressed image or video content but raw content such as YUV, RGB, or Raw-bayer images.
Remote sending of images with a decent framerate requires compression to respect a reasonable bandwidth on the network. This could be achieved by compressing to JPEG image format or video formats like VP8 or H264.
Find below some examples of command lines allowing to capture a continuous stream of raw images then compress to JPEG, VP8 or H264 stream while playing it using various multimedia players, either local or remote.
2. Local streaming[edit | edit source]
Here is an example of a local preview loopback using gst-launch to capture raw pictures then compress to JPEG then decode and display.
ExpandFor STM32MP255 line ![]() |
image/jpeg" ! decodebin ! autovideosinkgst-launch-1.0 v4l2src device=/dev/video3 ! video/x-raw, format=YUY2, width=640, height=480, framerate=30/1 ! encodebin profile="
3. UDP streaming[edit | edit source]
An internet connection is required, for example, by plugging an Ethernet cable on the:
STM32MP257x-EV1 Evaluation board ![]() |
CN17 Ethernet connector 1 |
ExpandFor STM32MP255 line ![]() |
Get the IP address aa.bb.cc.dd of the host PC using the ifconfig command:
aa.bb.cc.dd Bcast:10.201.23.255 Mask:255.255.252.0 inet addr:127.0.0.1 Mask:255.0.0.0ifconfig | grep "inet" inet addr:
Then fill the host= udpsink property with this IP address on the remote side to send UDP JPEG stream:
image/jpeg" ! rtpjpegpay ! udpsink host=aa.bb.cc.dd port=5000gst-launch-1.0 v4l2src device=/dev/video3 ! video/x-raw, format=YUY2, width=640, height=480, framerate=30/1 ! encodebin profile="
Then play the UDP JPEG stream on host PC:
JPEG ! rtpjpegdepay ! jpegparse ! decodebin ! videoconvert ! autovideosink sync=falsegst-launch-1.0 udpsrc port=5000 ! application/x-rtp, encoding-name=
A new window appears on the host PC displaying the camera content.
The same can be done with a lower bandwidth thanks to video compression. Here is an example with VP8:
video/x-vp8" ! rtpvp8pay ! udpsink host=aa.bb.cc.dd port=5000gst-launch-1.0 v4l2src device=/dev/video3 ! video/x-raw, format=YUY2, width=640, height=480, framerate=30/1 ! encodebin profile="
Then play the UDP VP8 stream on host PC:
VP8 ! rtpvp8depay ! decodebin ! videoconvert ! autovideosink sync=falsegst-launch-1.0 udpsrc port=5000 ! application/x-rtp, encoding-name=
Another example with H264:
video/x-h264" ! h264parse config-interval=1 ! rtph264pay ! udpsink host=aa.bb.cc.dd port=5000gst-launch-1.0 v4l2src device=/dev/video3 ! video/x-raw, format=YUY2, width=640, height=480, framerate=30/1 ! encodebin profile="
Then play the UDP H264 stream on host PC:
H264 ! rtph264depay ! decodebin ! videoconvert ! autovideosink sync=falsegst-launch-1.0 udpsrc port=5000 ! application/x-rtp, encoding-name=
Another H264 streaming example giving a 200 KB/s bitrate constraint to limit network bandwidth:
rate-control=1,bitrate=200000" ! h264parse config-interval=1 ! rtph264pay ! udpsink host=aa.bb.cc.dd port=5000gst-launch-1.0 v4l2src device=/dev/video3 ! video/x-raw, format=YUY2, width=640, height=480, framerate=30/1 ! encodebin profile="video/x-h264|element-properties,