This article lists all internal peripherals embedded in STM32MP15x lines and shows the assignment possibilities to the execution contexts for each one of them.
From this article, you can also access to individual peripheral articles in which information related to the overview and configuration can be found.
1. Internal peripherals overview[edit | edit source]
The figure below shows all peripherals embedded in STM32MP15x lines , grouped per functional domains that are reused in many places of this wiki to structure the articles.
Several execution contexts exist on STM32MP15x lines [1], corresponding to the different Arm cores and associated security modes:
- Arm dual core Cortex-A7 secure (Trustzone), running ROM code and TF-A BL2 at boot time, and running OP-TEE at runtime
- Arm dual core Cortex-A7 non secure , running U-Boot at boot time, and running Linux at runtime
- Arm Cortex-M4 non-secure , running STM32Cube
Some peripherals can be strictly assigned to one execution context: this is the case for most of the peripherals, like USART or I2C.
Other ones can be shared between several execution contexts: this is the case for system peripherals, like PWR or RCC.
The legend below shows how assigned and shared peripherals are identified in the assignment diagram that follows:
Both the diagram below and the following summary table (in Internal peripherals runtime assignment and Internal peripherals boot time assignment chapters below) are clickable in order to jump to each peripheral overview articles and get more detailed information (like software frameworks used to control them). They list STMicroelectronics recommendations. The STM32MP15 reference manual [2] may expose more possibilities than what is shown here.

2. Internal peripherals runtime assignment[edit | edit source]
Click on to expand or collapse the legend...
Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:
- ☐ means that the peripheral can be assigned to the given runtime context.
- ☑ means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
- ⬚ means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
- ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.
Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.
Domain | Peripheral | Runtime allocation | Comment ![]() | |||
---|---|---|---|---|---|---|
Instance | Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) |
Cortex-M4 (STM32Cube) | |||
Analog | ADC | ADC | ☐ | ☐ | Assignment (single choice) | |
Analog | DAC | DAC | ☐ | ☐ | Assignment (single choice) | |
Analog | DFSDM | DFSDM | ☐ | ☐ | Assignment (single choice) | |
Analog | VREFBUF | VREFBUF | ☐ | ☐ | Assignment (single choice) | |
Audio | SAI | SAI1 | ☐ | ☐ | Assignment (single choice) | |
SAI2 | ☐ | ☐ | Assignment (single choice) | |||
SAI3 | ☐ | ☐ | Assignment (single choice) | |||
SAI4 | ☐ | ☐ | Assignment (single choice) | |||
Audio | SPDIFRX | SPDIFRX | ☐ | ☐ | Assignment (single choice) | |
Coprocessor | IPCC | IPCC | ☑ | ☑ | Shared (none or both) | |
Coprocessor | HSEM | HSEM | ⬚ | ☑ | ☑ | |
Core | RTC | RTC | ☑ | ☐ | ☐ | RTC is mandatory to resynchronize STGEN after exiting low-power modes. |
Core | STGEN | STGEN | ✓ | |||
Core | SYSCFG | SYSCFG | ☑ | ☑ | ☑ | |
Core/DMA | DMA | DMA1 | ☐ | ☐ | Assignment (single choice) | |
DMA2 | ☐ | ☐ | Assignment (single choice) | |||
Core/DMA | DMAMUX | DMAMUX | ☐ | ☐ | Shareable (multiple choices supported) | |
Core/DMA | MDMA | MDMA | ⬚ | ☐ | Shareable (multiple choices supported) | |
Core/Interrupts | EXTI | EXTI | ☐ | ☐ | ☐ | Shared |
Core/Interrupts | GIC | GIC | ✓ | ✓ | ||
Core/Interrupts | NVIC | NVIC | ✓ | |||
Core/IOs | GPIO | GPIOA-K | ☐ (*) | ☐ | ☐ | The pins can individually be shared (*): despite they cannot be secured, the pins can be used by the secure context |
GPIOZ | ☐ | ☐ | ☐ | The pins can individually be secured or shared | ||
Core/RAM | BKPSRAM | BKPSRAM | ☑ | ⬚ | ⬚ | Assignment (single choice) |
Core/RAM | DDRCTRL | DDR | ☑ | ⬚ | ||
Core/RAM | MCU SRAM | SRAM1 | ☐ | ☐ | ☐ | Assignment (between A7 S and A7 NS / M4) Shareable (between A7 NS and M4) |
SRAM2 | ☐ | ☐ | ☐ | Assignment (between A7 S and A7 NS / M4) Shareable (between A7 NS and M4) | ||
SRAM3 | ☐ | ☐ | ☐ | Assignment (between A7 S and A7 NS / M4) Shareable (between A7 NS and M4) | ||
SRAM4 | ☐ | ☐ | ☐ | Assignment (between A7 S and A7 NS / M4) Shareable (between A7 NS and M4) | ||
Core/RAM | RETRAM | RETRAM | ⬚ | ⬚ | ☑ | Assignment to the Arm® Cortex®-M4 if used |
Core/RAM | SYSRAM | SYSRAM | ☑ | ☐ | ⬚ | Shareable (multiple choices supported)
Secure section required for low power entry and exit |
Core/Timers | LPTIM | LPTIMx (x = 1 to 5) | ☐ | ☐ | Assignment (single choice) | |
Core/Timers | TIM | TIM1 (APB2 group) | ☐ | ☐ | Assignment (single choice) | |
TIM2 (APB1 group) | ☐ | ☐ | Assignment (single choice) | |||
TIM3 (APB1 group) | ☐ | ☐ | Assignment (single choice) | |||
TIM4 (APB1 group) | ☐ | ☐ | Assignment (single choice) | |||
TIM5 (APB1 group) | ☐ | ☐ | Assignment (single choice) | |||
TIM6 (APB1 group) | ☐ | ☐ | Assignment (single choice) | |||
TIM7 (APB1 group) | ☐ | ☐ | Assignment (single choice) | |||
TIM8 (APB2 group) | ☐ | ☐ | Assignment (single choice) | |||
TIM12 (APB1 group) | ☐ | ☐ | ☐ | Assignment (single choice) TIM12 or TIM15 can be used for HSI/CSI calibration[3] | ||
TIM13 (APB1 group) | ☐ | ☐ | Assignment (single choice) | |||
TIM14 (APB1 group) | ☐ | ☐ | Assignment (single choice) | |||
TIM15 (APB2 group) | ☐ | ☐ | ☐ | Assignment (single choice) TIM12 or TIM15 can be used for HSI/CSI calibration[3] | ||
TIM16 (APB2 group) | ☐ | ☐ | Assignment (single choice) | |||
TIM17 (APB2 group) | ☐ | ☐ | Assignment (single choice) | |||
Core/Watchdog | IWDG | IWDG1 | ☐ | ☐ | ||
IWDG2 | ☐ | ☐ | Shared (none or both):
| |||
Core/Watchdog | WWDG | WWDG | ☐ | |||
High speed interface | OTG (USB OTG) | OTG (USB OTG) | ☐ | ⬚ | ||
High speed interface | USBH (USB Host) | USBH (USB Host) | ☐ | ⬚ | ||
High speed interface | USBPHYC (USB HS PHY controller) | USBPHYC (USB HS PHY controller) | ☐ | ⬚ | ||
Low speed interface | I2C | I2C1 | ☐ | ☐ | Assignment (single choice) | |
I2C2 | ☐ | ☐ | Assignment (single choice) | |||
I2C3 | ☐ | ☐ | Assignment (single choice) | |||
I2C4 | ☐ | ☐ | Assignment (single choice). Used for PMIC control on ST boards. | |||
I2C5 | ☐ | ☐ | Assignment (single choice) | |||
I2C6 | ☐ | ☐ | Assignment (single choice) | |||
Low speed interface or audio |
SPI | SPI2S1 | ☐ | ☐ | Assignment (single choice) | |
SPI2S2 | ☐ | ☐ | Assignment (single choice) | |||
SPI2S3 | ☐ | ☐ | Assignment (single choice) | |||
SPI4 | ☐ | ☐ | Assignment (single choice) | |||
SPI5 | ☐ | ☐ | Assignment (single choice) | |||
SPI6 | ⬚ | ☐ | Assignment (single choice) | |||
Low speed interface | USART | USART1 | ☐ | ☐ | Assignment (single choice) | |
USART2 | ☐ | ☐ | Assignment (single choice) | |||
USART3 | ☐ | ☐ | Assignment (single choice) | |||
UART4 | ☐ | ☐ | Assignment (single choice). Used for Linux® serial console on ST boards. | |||
UART5 | ☐ | ☐ | Assignment (single choice) | |||
USART6 | ☐ | ☐ | Assignment (single choice) | |||
UART7 | ☐ | ☐ | Assignment (single choice) | |||
UART8 | ☐ | ☐ | Assignment (single choice) | |||
Mass storage | FMC | FMC | ☐ | ☐ | Assignment (single choice) | |
Mass storage | QUADSPI | QUADSPI | ☐ | ☐ | Assignment (single choice) | |
Mass storage | SDMMC | SDMMC1 | ☐ | |||
SDMMC2 | ☐ | |||||
SDMMC3 | ☐ | ☐ | Assignment (single choice) | |||
Networking | ETH | ETH | ☐ | Assignment (single choice) | ||
Networking | FDCAN | FDCAN1 | ☐ | ☐ | Assignment (single choice) | |
FDCAN2 | ☐ | ☐ | Assignment (single choice) | |||
Power & Thermal | DTS | DTS | ☐ | |||
Power & Thermal | PWR | PWR | ✓ | ✓ | ✓ | |
Power & Thermal | RCC | RCC | ✓ | ✓ | ✓ | |
Security | BSEC | BSEC | ✓ | ☐ | ⬚ | Cortex-M4 can read BSEC shadow register (BSEC_OTP_DATAx) to read a lower OTP value |
Security | CRC | CRC1 | ☐ | ☐ | ||
CRC2 | ☐ | ☐ | ||||
Security | CRYP | CRYP1 | ☐ | ☐ | Assignment (single choice) | |
CRYP2 | ☐ | |||||
Security | ETZPC | ETZPC | ✓ | ✓ | ⬚ | |
Security | HASH | HASH1 | ☐ | ☐ | Assignment (single choice) | |
HASH2 | ☐ | |||||
Security | RNG | RNG1 | ☐ | ☐ | Assignment (single choice) | |
RNG2 | ☐ | |||||
Security | TZC | TZC | ✓ | |||
Security | TAMP | TAMP | ☐ | ☐ | ☐ | |
Trace & Debug | DBGMCU | DBGMCU | ⬚ | ⬚ | ⬚ | |
Trace & Debug | DDRPERFM | DDRPERFM | ☐ | |||
Trace & Debug | HDP | HDP | ☐ | |||
Visual | CEC | CEC | ☐ | ☐ | Assignment (single choice) | |
Visual | DCMI | DCMI | ☑ | ☐ | Assignment (single choice) | |
Visual | DSI | DSI | ☐ | |||
Visual | GPU | GPU | ☐ | |||
Visual | LTDC | LTDC | ☐ |
3. Internal peripherals boot time assignment[edit | edit source]
Click on to expand or collapse the legend...
Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:
- ☐ means that the peripheral can be assigned to the given boot time context.
- ☑ means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
- ⬚ means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
- ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32 MPU reference manuals.
Domain | Peripheral | Boot time allocation | Comment ![]() | |||
---|---|---|---|---|---|---|
Instance | Cortex-A7 secure (ROM code) |
Cortex-A7 secure (TF-A BL2) |
Cortex-A7 non-secure (U-Boot) | |||
Analog | ADC | ADC | ☐ | |||
Coprocessor | HSEM | HSEM | ☐ | |||
Core | RTC | RTC | ☐ | |||
Core | STGEN | STGEN | ✓ | ✓ | ||
Core | SYSCFG | SYSCFG | ✓ | ☑ | ☑ | |
Core/IOs | GPIO | GPIOA-K | ✓ | ☑ (*) | ☐ | The pins cannot be secured (*): despite they cannot be secured, the pins can be used by the secure context |
GPIOZ | ☐ | ☐ | The pins can individually be secured | |||
Core/RAM | BKPSRAM | BKPSRAM | ☑ | ⬚ | ||
Core/RAM | DDRCTRL | DDR | ☑ | ⬚ | ||
Core/RAM | MCU SRAM | Any instance | ✓ | ☑ | ☐ | |
Core/RAM | RETRAM | RETRAM | ☐ | |||
Core/RAM | SYSRAM | SYSRAM | ✓ | ✓ | ||
Core/Timers | LPTIM | LPTIMx (x = 1 to 5) | ⬚ | ⬚ | LPTIM are not used at boot time. | |
Core/Timers | TIM | TIMx (x = 2 to 7, 12, 13, 14. APB1 group) | ⬚ | |||
TIMx (x = 1, 8, 15, 16, 17. APB2 group) | ⬚ | |||||
Core/Watchdog | IWDG | Any instance | ✓ | ☐ | ☐ | |
High speed interface | OTG (USB OTG) | OTG (USB OTG) | ✓ | ☐ | ☐ | The OTG can be used by ROM code, FSBL and SSBL in DFU mode to support serial boot. It can be used also in U-boot with command line tools. |
High speed interface | USBH (USB Host) | USBH (USB Host) | ☐ | |||
High speed interface | USBPHYC (USB HS PHY controller) | USBPHYC (USB HS PHY controller) | ✓ | ☐ | ☐ | The USBPHYC can be used by ROM code, FSBL and SSBL in DFU mode to support serial boot. It can be used also in U-boot by OTG and USBH with command line tools. |
Low speed interface | I2C | Any instance | ☐ | ☐ | ||
Low speed interface | USART | Any instance | ✓ | ☐ | ☐ | |
Mass storage | FMC | FMC | ☐ | ☐ | ☐ | |
Mass storage | QUADSPI | QUADSPI | ✓ | ☐ | ☐ | |
Mass storage | SDMMC | SDMMC1 | ☐ | ☐ | ☐ | |
SDMMC2 | ☐ | ☐ | ☐ | |||
Networking | ETH | Any instance | ☐ | Assignment (single choice) | ||
Power & Thermal | PWR | PWR | ✓ | ✓ | ✓ | |
Power & Thermal | RCC | RCC | ✓ | ✓ | ✓ | |
Security | BSEC | BSEC | ✓ | ✓ | ☐ | |
Security | ETZPC | Any instance | ✓ | ✓ | ✓ | ETZPC configuration is set by OP-TEE |
Security | HASH | HASH1 | ✓ | ☑ | ||
HASH2 | not used at boot time. | |||||
Security | RNG | RNG1 | ☑ | ☐ | ||
Security | TZC | TZC | ☑ | |||
Security | TAMP | TAMP | ✓ | ✓ | ✓ | |
Trace & Debug | DBGMCU | DBGMCU | ⬚ | ⬚ | ⬚ | |
Visual | DSI | DSI | ☐ | |||
Visual | LTDC | LTDC | ☐ |
4. References[edit | edit source]