Last edited one year ago

CEC internal peripheral: Difference between revisions


Latest revision as of 15:08, 4 January 2024



1. Article purpose[edit | edit source]

The purpose of this article is to:

  • briefly introduce the CEC peripheral and its main features,
  • indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
  • list the software frameworks and drivers managing the peripheral,
  • explain how to configure the peripheral.

2. Peripheral overview[edit | edit source]

The CEC (consumer electronics control) or HDMI-CEC peripheral is used to receive/send messages from/to devices, such as TV or tuner, through a HDMI cable.

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.

Refer to the STM32 CEC presentation [1] for an overview of the CEC hardware block capabilities.

3. Peripheral usage[edit | edit source]

This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.

3.1. Boot time assignment[edit | edit source]

The CEC peripheral is not used at boot time.

3.2. Runtime assignment[edit | edit source]

3.2.1. On STM32MP15x lines More info.png[edit | edit source]

Click on How to.png to expand or collapse the legend...

Domain Peripheral Runtime allocation Comment How to.png
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Visual CEC CEC Assignment (single choice)

4. Software frameworks and drivers[edit | edit source]

Below are listed the software frameworks and drivers managing the CEC peripheral for the embedded software components listed in the above tables.

5. How to assign and configure the peripheral[edit | edit source]

The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:

  • partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
  • HAL initialization code generation for the STM32CubeMPU Package.

The configuration is applied by the firmware running in the context in which the peripheral is assigned.

See also additional information in the CEC device tree configuration article for Linux®.

6. How to go further[edit | edit source]

Refer to the STM32 CEC application note (AN4066) [2] for a detailed description of the CEC peripheral and applicable use-cases.

Even if this application note is related to STM32 microcontrollers, it also applies to STM32 MPUs.

7. References[edit | edit source]