Registered User mNo edit summary |
Registered User mNo edit summary |
||
(5 intermediate revisions by 2 users not shown) | |||
Line 1: | Line 1: | ||
<noinclude>{{ApplicableFor | <noinclude>{{ApplicableFor | ||
|MPUs list=STM32MP15x | |MPUs list=STM32MP15x | ||
|MPUs checklist=STM32MP13x, STM32MP15x | |MPUs checklist=STM32MP13x, STM32MP15x, STM32MP25x | ||
}}</noinclude> | }}</noinclude> | ||
==Article purpose== | ==Article purpose== | ||
The purpose of this article is to | The purpose of this article is to: | ||
* briefly introduce the DAC peripheral and its main features | * briefly introduce the DAC peripheral and its main features, | ||
* indicate the | * indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts), | ||
* list the software frameworks and drivers managing the peripheral, | |||
* explain how to configure the | * explain how to configure the peripheral. | ||
==Peripheral overview== | ==Peripheral overview== | ||
The '''DAC''' peripheral is a voltage output digital-to-analog converter | The '''DAC''' peripheral is a voltage output digital-to-analog converter: | ||
* It may be configured in '''8- or 12-bit mode''' (data could be left- or right-aligned) | * It may be configured in '''8- or 12-bit mode''' (data could be left- or right-aligned) | ||
* It has '''two output channels''', each with its '''own converter''' | * It has '''two output channels''', each with its '''own converter''' | ||
Line 25: | Line 22: | ||
* The '''common reference voltage''', can be provided by either VREFBUF<ref name="VREFBUF internal peripheral">[[VREFBUF internal peripheral]]</ref> or any other external regulator<ref name="Regulator overview">[[Regulator overview]]</ref> wired to VREF+ pin. | * The '''common reference voltage''', can be provided by either VREFBUF<ref name="VREFBUF internal peripheral">[[VREFBUF internal peripheral]]</ref> or any other external regulator<ref name="Regulator overview">[[Regulator overview]]</ref> wired to VREF+ pin. | ||
== | Refer to the [[STM32MP15 resources#Reference manuals|STM32MP15 reference manuals]] for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented. | ||
==Peripheral usage== | |||
This chapter is applicable in the scope of the '''OpenSTLinux BSP''' running on the Arm<sup>®</sup> Cortex<sup>®</sup>-A processor(s), and the '''STM32CubeMPU Package''' running on the Arm<sup>®</sup> Cortex<sup>®</sup>-M processor. | |||
===Boot time assignment=== | |||
===Boot time=== | The DAC peripheral is not used at boot time. | ||
The DAC is not used at boot time. | |||
===Runtime=== | ===Runtime assignment=== | ||
==== | ====On {{MicroprocessorDevice | device=15}}==== | ||
{{#lst:STM32MP1_internal_peripherals_assignment_table_template|stm32mp15_runtime}} | |||
<section begin=stm32mp15_runtime /> | |||
| rowspan="1" | Analog | |||
| rowspan="1" | [[DAC internal peripheral|DAC]] | |||
| DAC | |||
| | |||
| <span title="assignable peripheral" style="font-size:21px">☐</span> | |||
| <span title="assignable peripheral" style="font-size:21px">☐</span> | |||
| Assignment (single choice) | |||
|- | |||
<section end=stm32mp15_runtime /> | |||
|} | |||
==Software frameworks and drivers== | |||
Below are listed the software frameworks and drivers managing the DAC peripheral for the embedded software components listed in the above tables. | |||
* '''Linux<sup>®</sup>''': [[IIO overview|IIO framework]] | |||
* '''STM32Cube''': {{CodeSource | STM32CubeMP1 | Drivers/STM32MP1xx_HAL_Driver/Src/stm32mp1xx_hal_dac.c | HAL DAC driver}} | |||
| | |||
== | ==How to assign and configure the peripheral== | ||
The | The peripheral assignment can be done via the [[STM32CubeMX]] graphical tool (and manually completed if needed).<br /> | ||
This tool also helps to configure the peripheral: | |||
* partial device trees (pin control and clock tree) generation for the OpenSTLinux software components, | |||
* HAL initialization code generation for the STM32CubeMPU Package. | |||
The configuration is applied by the firmware running in the context in which the peripheral is assigned. | |||
For the Linux kernel configuration, please refer to [[DAC device tree configuration]] and [[DAC Linux driver]] articles. | For the Linux kernel configuration, please refer to [[DAC device tree configuration]] and [[DAC Linux driver]] articles. | ||
==References== | ==References== | ||
Line 75: | Line 64: | ||
<noinclude> | <noinclude> | ||
[[Category:Analog peripherals]] | |||
{{ArticleBasedOnModel| Internal peripheral article model}} | {{ArticleBasedOnModel| Internal peripheral article model}} | ||
{{PublicationRequestId | 8310 | 2019-08-07 | AlainF}} | {{PublicationRequestId | 8310 | 2019-08-07 | AlainF}} | ||
</noinclude> | </noinclude> |
Latest revision as of 15:10, 20 July 2023
1. Article purpose[edit | edit source]
The purpose of this article is to:
- briefly introduce the DAC peripheral and its main features,
- indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
- list the software frameworks and drivers managing the peripheral,
- explain how to configure the peripheral.
2. Peripheral overview[edit | edit source]
The DAC peripheral is a voltage output digital-to-analog converter:
- It may be configured in 8- or 12-bit mode (data could be left- or right-aligned)
- It has two output channels, each with its own converter
- The dual DAC channel mode could be done independently or simultaneously
- It has built-in noise and triangle waveform generator and supports triggers for conversions, using: TIM[1], LPTIM[2] or EXTI[3]
- The DAC output buffer allows a high drive output current
- It can operate under Normal mode or low-power Sample and Hold mode (uses LSI clock, from RCC[4]).
- It may be used in conjunction with the DMA[5] controller (with underrun error detection)
- The common reference voltage, can be provided by either VREFBUF[6] or any other external regulator[7] wired to VREF+ pin.
Refer to the STM32MP15 reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.
3. Peripheral usage[edit | edit source]
This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.
3.1. Boot time assignment[edit | edit source]
The DAC peripheral is not used at boot time.
3.2. Runtime assignment[edit | edit source]
3.2.1. On STM32MP15x lines
[edit | edit source]
Click on to expand or collapse the legend...
Domain | Peripheral | Runtime allocation | Comment ![]() | |||
---|---|---|---|---|---|---|
Instance | Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) |
Cortex-M4 (STM32Cube) | |||
Analog | DAC | DAC | ☐ | ☐ | Assignment (single choice) |
4. Software frameworks and drivers[edit | edit source]
Below are listed the software frameworks and drivers managing the DAC peripheral for the embedded software components listed in the above tables.
- Linux®: IIO framework
- STM32Cube: HAL DAC driver
5. How to assign and configure the peripheral[edit | edit source]
The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:
- partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
- HAL initialization code generation for the STM32CubeMPU Package.
The configuration is applied by the firmware running in the context in which the peripheral is assigned.
For the Linux kernel configuration, please refer to DAC device tree configuration and DAC Linux driver articles.
6. References[edit | edit source]