Registered User |
Registered User mNo edit summary |
||
(2 intermediate revisions by the same user not shown) | |||
Line 1: | Line 1: | ||
==Modifying target password== | <noinclude>{{ApplicableFor | ||
|MPUs list=STM32MP13x, STM32MP15x | |||
|MPUs checklist=STM32MP13x, STM32MP15x | |||
}}</noinclude> | |||
==Modifying the target password== | |||
When debugging Cortex-M in "production mode", | When debugging the Cortex<sup>®</sup>-M in "production mode", a typo entering the target password implies to modify the target password registered by the STM32CubeIDE. Indeed, this prevents the user from debugging in "production mode". | ||
This password | This password can be updated with ''Remote Connections'' preferences menu: ''Window > Preferences > Remote Development''. | ||
[[File: | [[File:MPU Password Setup.png|700px|center|thumb|Linux device password setup]] | ||
Note that if "MPU SSH" is opened, it must be closed first to enable edit. | |||
Note that if "MPU SSH" is | |||
<noinclude> | <noinclude> | ||
[[Category:STM32CubeIDE|4]] | [[Category:STM32CubeIDE|4]] | ||
{{PublicationRequestId | 19684 (LudovicB) |2021-04-20 }} | |||
</noinclude> | </noinclude> |
Latest revision as of 11:00, 31 January 2023
1. Modifying the target password[edit | edit source]
When debugging the Cortex®-M in "production mode", a typo entering the target password implies to modify the target password registered by the STM32CubeIDE. Indeed, this prevents the user from debugging in "production mode".
This password can be updated with Remote Connections preferences menu: Window > Preferences > Remote Development.
Note that if "MPU SSH" is opened, it must be closed first to enable edit.