Registered User mNo edit summary |
Registered User Tag: 2017 source edit |
||
(5 intermediate revisions by 2 users not shown) | |||
Line 1: | Line 1: | ||
{{ApplicableFor | |||
|MPUs list=STM32MP15x | |MPUs list=STM32MP15x, STM32MP25x | ||
|MPUs checklist=STM32MP13x, STM32MP15x | |MPUs checklist=STM32MP13x, STM32MP15x, STM32MP25x | ||
}}</noinclude> | }} | ||
<noinclude></noinclude> | |||
== Introduction == | == Introduction == | ||
'' '''glmark2''' is an OpenGL 2.0 and ES 2.0 benchmark, developed by Alexandros Frantzis and Jesse Barker. It is based on the original glmark benchmark by Ben Smith. {{grey|extracted from '''The glmark2 official web site''' <ref> https://github.com/glmark2/glmark2 </ref>}}'' | '' '''glmark2''' is an OpenGL 2.0 and ES 2.0 benchmark, developed by Alexandros Frantzis and Jesse Barker. It is based on the original glmark benchmark by Ben Smith. {{grey|extracted from '''The glmark2 official web site''' <ref> https://github.com/glmark2/glmark2 </ref>}}'' | ||
Line 12: | Line 13: | ||
=== glmark2-es2-wayland === | === glmark2-es2-wayland === | ||
* Start Weston (if not already started) | * Start Weston (if not already started)<ref name="weston_start">[[How to stop and start Weston]]</ref> | ||
{{Board$}} systemctl start weston | {{Board$}} systemctl start weston-graphical-session | ||
* Launch glmark2 | * Launch glmark2 | ||
{{Board$}} glmark2-es2-wayland | {{Board$}} glmark2-es2-wayland | ||
{{WestonLaunch|glmark2-es2-wayland}} | |||
=== glmark2-es2-drm === | === glmark2-es2-drm === | ||
* Stop Weston | * Stop Weston<ref name="weston_start"/> | ||
{{Board$}} systemctl stop weston | {{Board$}} systemctl stop weston-graphical-session | ||
* The DRM display mode may need to be set and the DRM master token released so that glmark2 can use the DRM interfaces. This depends on the glmark2 version. For instance: | * The DRM display mode may need to be set and the DRM master token released so that glmark2 can use the DRM interfaces. This depends on the glmark2 version. For instance: | ||
{{Board$}} modetest -s 27:720x1280 -d & | {{Board$}} modetest -s 27:720x1280 -d & | ||
Line 30: | Line 33: | ||
== To go further == | == To go further == | ||
You can find the full documentation of glmark2 in the related | You can find the full documentation of glmark2 in the related <ref>[http://manpages.ubuntu.com/manpages/lastest/man1/glmark2.1.html Ubuntu glmark2 man page]</ref>. | ||
==References== | ==References== |
Latest revision as of 14:32, 21 June 2024
1. Introduction[edit | edit source]
glmark2 is an OpenGL 2.0 and ES 2.0 benchmark, developed by Alexandros Frantzis and Jesse Barker. It is based on the original glmark benchmark by Ben Smith. extracted from The glmark2 official web site [1]
2. Using glmark2[edit | edit source]
Building glmark2 generates 2 binaries:
- glmark2-es2-wayland, to launch glmark2 benchmark as a wayland client.
- glmark2-es2-drm, to launch glmark2 benchmark as a native DRM/GBM openGLES application.
2.1. glmark2-es2-wayland[edit | edit source]
- Start Weston (if not already started)[2]
Board $> systemctl start weston-graphical-session
- Launch glmark2
Board $> glmark2-es2-wayland
2.2. glmark2-es2-drm[edit | edit source]
- Stop Weston[2]
Board $> systemctl stop weston-graphical-session
- The DRM display mode may need to be set and the DRM master token released so that glmark2 can use the DRM interfaces. This depends on the glmark2 version. For instance:
Board $> modetest -s 27:720x1280 -d &
Note: The connector and the mode are given as an example.
- Launch glmark2
Board $> glmark2-es2-drm
3. Source code location[edit | edit source]
- Official source code: https://github.com/glmark2/glmark2
4. To go further[edit | edit source]
You can find the full documentation of glmark2 in the related [3].
5. References[edit | edit source]