Registered User mNo edit summary |
Registered User mNo edit summary Tag: 2017 source edit |
||
(4 intermediate revisions by 2 users not shown) | |||
Line 15: | Line 15: | ||
The LPTIM peripheral is available in different configurations. Depending on the selected instance, it can act as PWM, quadrature encoder<ref name="quadrature_encoder">[https://en.wikipedia.org/wiki/Rotary_encoder#Incremental_rotary_encoder Quadrature encoder]</ref>, | The LPTIM peripheral is available in different configurations. Depending on the selected instance, it can act as PWM, quadrature encoder<ref name="quadrature_encoder">[https://en.wikipedia.org/wiki/Rotary_encoder#Incremental_rotary_encoder Quadrature encoder]</ref>, | ||
external event counter or trigger source for other internal peripherals, like | external event counter or trigger source for other internal peripherals, like [[ADC internal peripheral|ADC]], [[DAC internal peripheral|DAC]] and [[DFSDM internal peripheral|DFSDM]] (on {{MicroprocessorDevice | device=1}}) or [[MDF internal peripheral|MDF]] (on {{MicroprocessorDevice | device=2}}). | ||
* LPTIM on {{MicroprocessorDevice | device=1}} | |||
{| class="st-table" style="width: 100%;" | {| class="st-table" style="width: 100%;" | ||
Line 38: | Line 40: | ||
| | | | ||
| | | | ||
|- | |||
|} | |||
* LPTIM on {{MicroprocessorDevice | device=2}} | |||
{| class="st-table" style="width: 100%;" | |||
|- style="background: {{STLightGrey}};" | |||
! style="width:40%; | LPTIM features | |||
! style="width:20%; | PWM | |||
! style="width:20%;" | External event counter <br/>Trigger source | |||
! style="width:20%;" | Quadrature encoder | |||
|- | |||
| LPTIM1, LPTIM2 | |||
| {{Y}} | |||
| {{Y}} | |||
| {{Y}} | |||
|- | |||
| LPTIM3, LPTIM4, LPTIM5 | |||
| {{Y}} | |||
| {{Y}} | |||
| | |||
|- | |- | ||
|} | |} |
Latest revision as of 18:00, 13 May 2024
1. Article purpose[edit | edit source]
The purpose of this article is to:
- briefly introduce the LPTIM peripheral and its main features,
- indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
- list the software frameworks and drivers managing the peripheral,
- explain how to configure the peripheral.
2. Peripheral overview[edit | edit source]
The LPTIM peripheral is a single channel low-power timer unit, that can continue to run even during low power modes when it selects a clock source that remains active in RCC.
The LPTIM peripheral is available in different configurations. Depending on the selected instance, it can act as PWM, quadrature encoder[1], external event counter or trigger source for other internal peripherals, like ADC, DAC and DFSDM (on STM32MP1 series) or MDF (on STM32MP2 series).
- LPTIM on STM32MP1 series
LPTIM features | PWM | External event counter Trigger source |
Quadrature encoder |
---|---|---|---|
LPTIM1, LPTIM2 | ![]() |
![]() |
![]() |
LPTIM3 | ![]() |
![]() |
|
LPTIM4, LPTIM5 | ![]() |
- LPTIM on STM32MP2 series
LPTIM features | PWM | External event counter Trigger source |
Quadrature encoder |
---|---|---|---|
LPTIM1, LPTIM2 | ![]() |
![]() |
![]() |
LPTIM3, LPTIM4, LPTIM5 | ![]() |
![]() |
- On STM32MP13x lines
, LPTIM3 can be used for RCC HSE clock source monitoring
- On STM32MP25x lines
, LPTIM can have up to 2 independent channels. It also supports input capture. LPTIM1 can be used for RCC HSE monitoring.
Refer to the STM32 MPU reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.
3. Peripheral usage[edit | edit source]
This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.
3.1. Boot time assignment[edit | edit source]
3.1.1. On STM32MP13x lines
[edit | edit source]
Click on to expand or collapse the legend...
Domain | Peripheral | Boot time allocation | Comment ![]() | |||
---|---|---|---|---|---|---|
Instance | Cortex-A7 secure (ROM code) |
Cortex-A7 secure (TF-A BL2) |
Cortex-A7 non-secure (U-Boot) | |||
Core/Timers | LPTIM | LPTIM1 | ⬚ | |||
LPTIM2 | ⬚ | ⬚ | ||||
LPTIM3 | ⬚ | ⬚ | ||||
LPTIM4 | ⬚ | |||||
LPTIM5 | ⬚ |
3.1.2. On STM32MP15x lines
[edit | edit source]
Click on to expand or collapse the legend...
Domain | Peripheral | Boot time allocation | Comment ![]() | |||
---|---|---|---|---|---|---|
Instance | Cortex-A7 secure (ROM code) |
Cortex-A7 secure (TF-A BL2) |
Cortex-A7 non-secure (U-Boot) | |||
Core/Timers | LPTIM | LPTIMx (x = 1 to 5) | ⬚ | ⬚ | LPTIM are not used at boot time. |
3.1.3. On STM32MP25x lines
[edit | edit source]
STM32MP2 internal peripherals assignment table template
| rowspan="1" | Core/Timers | rowspan="1" | LPTIM | LPTIMx (x = 1 to 5) | | ⬚ | ⬚ | LPTIM are not used at boot time. |-
|}
3.2. Runtime assignment[edit | edit source]
3.2.1. On STM32MP13x lines
[edit | edit source]
Click on to expand or collapse the legend...
Domain | Peripheral | Runtime allocation | Comment ![]() | ||
---|---|---|---|---|---|
Instance | Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) | |||
Core/Timers | LPTIM | LPTIM1 | ☐ | ||
LPTIM2 | ☐ | ☐ | Assignment (single choice) | ||
LPTIM3 | ☐ | ☐ | Assignment (single choice) LPTIM3 can be used for HSE monitoring | ||
LPTIM4 | ☐ | ||||
LPTIM5 | ☐ |
3.2.2. On STM32MP15x lines
[edit | edit source]
Click on to expand or collapse the legend...
Domain | Peripheral | Runtime allocation | Comment ![]() | |||
---|---|---|---|---|---|---|
Instance | Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) |
Cortex-M4 (STM32Cube) | |||
Core/Timers | LPTIM | LPTIMx (x = 1 to 5) | ☐ | ☐ | Assignment (single choice) |
3.2.3. On STM32MP25x lines
[edit | edit source]
STM32MP2 internal peripherals assignment table template
| rowspan="5" | Core/Timers | rowspan="5" | LPTIM | LPTIM1 | ☐OP-TEE | ☐ | ⬚ | ☐ | | LPTIM1 can be used for HSE monitoring. |- | LPTIM2 | ☐OP-TEE | ☐ | ⬚ | ☐ | | |- | LPTIM3 | ☐OP-TEE | ☐ | ⬚ | ☐ | ☐ | |- | LPTIM4 | ☐OP-TEE | ☐ | ⬚ | ☐ | ☐ | |- | LPTIM5 | ☐OP-TEE | ☐ | ⬚ | ☐ | ☐ | |-
|}
4. Software frameworks and drivers[edit | edit source]
Below are listed the software frameworks and drivers managing the LPTIM peripheral for the embedded software components listed in the above tables.
- Linux®: PWM framework, IIO framework, Counter framework, and Clock events framework
- OP-TEE: OP-TEE LPTIM driver
- STM32Cube: HAL LPTIM driver
5. How to assign and configure the peripheral[edit | edit source]
The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:
- partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
- HAL initialization code generation for the STM32CubeMPU Package.
The configuration is applied by the firmware running in the context in which the peripheral is assigned.
For Linux kernel configuration, please refer to LPTIM device tree configuration and STM32 LPTIM Linux driver articles.
6. References[edit | edit source]