Registered User mNo edit summary |
Registered User No edit summary |
||
(3 intermediate revisions by one other user not shown) | |||
Line 1: | Line 1: | ||
{{ApplicableFor | {{ApplicableFor | ||
|MPUs list=STM32MP15x | |MPUs list=STM32MP15x | ||
|MPUs checklist=STM32MP13x, STM32MP15x | |MPUs checklist=STM32MP13x, STM32MP15x, STM32MP25x | ||
}} | }} | ||
==Article purpose== | ==Article purpose== | ||
The purpose of this article is to: | The purpose of this article is to: | ||
Line 32: | Line 31: | ||
| | | | ||
| | | | ||
| <span title=" | | <span title="assignable peripheral" style="font-size:21px">☐</span> | ||
| | | | ||
|- | |- | ||
Line 50: | Line 49: | ||
| rowspan="1" | [[HSEM internal peripheral|HSEM]] | | rowspan="1" | [[HSEM internal peripheral|HSEM]] | ||
| HSEM | | HSEM | ||
| <span title=" | | <span title="assignable peripheral but not supported" style="font-size:21px">⬚</span> | ||
| <span title=" | | <span title="assigned peripheral" style="font-size:21px">☑</span> | ||
| <span title=" | | <span title="assigned peripheral" style="font-size:21px">☑</span> | ||
| | | | ||
|- | |- | ||
Line 62: | Line 61: | ||
* '''Linux<sup>®</sup>''': [[Hardware spinlock overview|hardware spinlock framework]] | * '''Linux<sup>®</sup>''': [[Hardware spinlock overview|hardware spinlock framework]] | ||
* '''STM32Cube''': [[ | * '''STM32Cube''': [[STM32CubeMP15 Package architecture|HSEM HAL driver]] and {{CodeSource | STM32CubeMP1 | Drivers/STM32MP1xx_HAL_Driver/Inc/stm32mp1xx_hal_hsem.h | header file of HSEM HAL module}} | ||
==How to assign and configure the peripheral== | ==How to assign and configure the peripheral== |
Latest revision as of 11:50, 8 February 2024
1. Article purpose[edit | edit source]
The purpose of this article is to:
- briefly introduce the HSEM peripheral and its main features,
- indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
- list the software frameworks and drivers managing the peripheral,
- explain how to configure the peripheral.
2. Peripheral overview[edit | edit source]
The HSEM (hardware spinlock) peripheral is used to provide synchronization and mutual exclusion between heterogeneous processors.
- 32 hardware semaphores are available on the platform.
- semaphores could be accessed by the Arm® Cortex®-A7 core and the Arm® Cortex®-M4
Refer to the STM32MP15 reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.
3. Peripheral usage[edit | edit source]
This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.
3.1. Boot time assignment[edit | edit source]
3.1.1. On STM32MP15x lines
[edit | edit source]
The hardware semaphore is used at boot time for GPIO access protection between the Arm® Cortex®-A7 and Cortex®-M4 cores. See Protecting GPIO and EXTI system resources by hardware semaphores for details.
Click on the right to expand the legend...
Domain | Peripheral | Boot time allocation | Comment | |||
---|---|---|---|---|---|---|
Instance | Cortex-A7 secure (ROM code) |
Cortex-A7 secure (TF-A BL2) |
Cortex-A7 non-secure (U-Boot) | |||
Coprocessor | HSEM | HSEM | ☐ |
3.2. Runtime assignment[edit | edit source]
3.2.1. On STM32MP15x lines
[edit | edit source]
It does not make sense to allocate HSEM to a single runtime execution context, that is why it is enabled by default for both cores in the STM32CubeMX.
The hardware semaphore is used at runtime for GPIO and EXTI access protection between the Arm® Cortex®-A7 and Cortex®-M4 cores. See Protecting GPIO and EXTI system resources by hardware semaphores for details.
Click on the right to expand the legend...
Domain | Peripheral | Runtime allocation | Comment | |||
---|---|---|---|---|---|---|
Instance | Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) |
Cortex-M4 (STM32Cube) | |||
Coprocessor | HSEM | HSEM | ⬚ | ☑ | ☑ |
4. Software frameworks and drivers[edit | edit source]
Below are listed the software frameworks and drivers managing the HSEM peripheral for the embedded software components listed in the above tables.
- Linux®: hardware spinlock framework
- STM32Cube: HSEM HAL driver and header file of HSEM HAL module
5. How to assign and configure the peripheral[edit | edit source]
The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:
- partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
- HAL initialization code generation for the STM32CubeMPU Package.
The configuration is applied by the firmware running in the context in which the peripheral is assigned.
The HSEM peripheral is shared between the Cortex-A and Cortex-M contexts, so a particular attention must be paid to have a complementary configuration on both contexts.