Registered User mNo edit summary |
Registered User mNo edit summary |
||
(17 intermediate revisions by 4 users not shown) | |||
Line 1: | Line 1: | ||
<noinclude>{{ApplicableFor | <noinclude>{{ApplicableFor | ||
|MPUs list=STM32MP13x, STM32MP15x | |MPUs list=STM32MP13x, STM32MP15x, STM32MP25x | ||
|MPUs checklist=STM32MP13x, STM32MP15x | |MPUs checklist=STM32MP13x, STM32MP15x, STM32MP25x | ||
}}</noinclude> | }}</noinclude> | ||
==Article purpose== | |||
The purpose of this article is to: | |||
{| | * briefly introduce the SYSCFG peripheral and its main features, | ||
* indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts), | |||
* list the software frameworks and drivers managing the peripheral, | |||
* explain how to configure the peripheral. | |||
==Peripheral overview== | |||
The '''SYSCFG''' peripheral is used to configure various system aspects like IOs compensation, Ethernet clocking path, … | |||
Refer to the [[STM32 MPU resources#Reference manuals|STM32 MPU reference manuals]] for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented. | |||
==Peripheral usage== | |||
This chapter is applicable in the scope of the '''OpenSTLinux BSP''' running on the Arm<sup>®</sup> Cortex<sup>®</sup>-A processor(s), and the '''STM32CubeMPU Package''' running on the Arm<sup>®</sup> Cortex<sup>®</sup>-M processor. | |||
===Boot time assignment=== | |||
====On {{MicroprocessorDevice | device=1}}==== | |||
The SYSCFG peripheral is configured by [[TF-A overview|TF-A]] and [[U-Boot overview|U-Boot]] at boot time. | |||
{{#lst:STM32MP1_internal_peripherals_assignment_table_template|stm32mp1_boottime}} | |||
<section begin=stm32mp13_boottime /><section begin=stm32mp15_boottime /> | |||
| rowspan="1" | Core | |||
| rowspan="1" | [[SYSCFG internal peripheral|SYSCFG]] | |||
| SYSCFG | |||
| <span title="system peripheral" style="font-size:21px">✓</span> | |||
| <span title="assigned peripheral" style="font-size:21px">☑</span> | |||
| <span title="assigned peripheral" style="font-size:21px">☑</span> | |||
| | |||
|- | |- | ||
<section end=stm32mp13_boottime /><section end=stm32mp15_boottime /> | |||
|} | |||
====On {{MicroprocessorDevice | device=2}}==== | |||
{{#lst:STM32MP2_internal_peripherals_assignment_table_template|stm32mp2_a35_boottime}} | |||
<section begin=stm32mp25_a35_boottime /> | |||
| rowspan="1" | Core | |||
| rowspan="1" | [[SYSCFG internal peripheral|SYSCFG]] | |||
| SYSCFG | |||
| <span title="system peripheral" style="font-size:21px">✓</span> | |||
| <span title="assigned peripheral" style="font-size:21px">☑</span> | |||
| <span title="assigned peripheral" style="font-size:21px">☑</span> | |||
| | |||
|- | |- | ||
| | <section end=stm32mp25_a35_boottime /> | ||
|} | |||
===Runtime assignment=== | |||
====On {{MicroprocessorDevice | device=13}}==== | |||
{{#lst:STM32MP1_internal_peripherals_assignment_table_template|stm32mp13_runtime}} | |||
<section begin=stm32mp13_runtime /> | |||
| rowspan="1" | Core | |||
| rowspan="1" | [[SYSCFG_internal_peripheral|SYSCFG]] | |||
| SYSCFG | |||
| <span title="assigned peripheral" style="font-size:21px">☑</span> | |||
| <span title="assigned peripheral" style="font-size:21px">☑</span> | |||
| | |||
|- | |- | ||
<section end=stm32mp13_runtime /> | |||
|} | |} | ||
====On {{MicroprocessorDevice | device=15}}==== | |||
{{#lst:STM32MP1_internal_peripherals_assignment_table_template|stm32mp15_runtime}} | |||
<section begin=stm32mp15_runtime /> | |||
| rowspan="1" | Core | |||
| rowspan="1" | [[SYSCFG internal peripheral|SYSCFG]] | |||
| SYSCFG | |||
| <span title="assigned peripheral" style="font-size:21px">☑</span> | |||
| <span title="assigned peripheral" style="font-size:21px">☑</span> | |||
| <span title="assigned peripheral" style="font-size:21px">☑</span> | |||
| | |||
|- | |||
<section end=stm32mp15_runtime /> | |||
|} | |||
====On {{MicroprocessorDevice | device=25}}==== | |||
{{#lst:STM32MP2_internal_peripherals_assignment_table_template|stm32mp25_runtime}} | |||
<section begin=stm32mp25_a35_runtime /> | |||
| rowspan="1" | Core | |||
| rowspan="1" | [[SYSCFG internal peripheral|SYSCFG]] | |||
| SYSCFG | |||
| <span title="assigned peripheral" style="font-size:21px">☑</span> | |||
| <span title="assigned peripheral" style="font-size:21px">☑</span> | |||
| <span title="assigned peripheral" style="font-size:21px">☑</span> | |||
| <span title="assigned peripheral" style="font-size:21px">☑</span> | |||
| | |||
| | |||
|- | |||
<section end=stm32mp25_a35_runtime /> | |||
|} | |||
==Software frameworks and drivers== | |||
Below are listed the software frameworks and drivers managing the SYSCFG peripheral for the embedded software components listed in the above tables. | |||
[[STM32 MPU Linux kernel overview|Linux]] and [[STM32CubeMP15 Package architecture|STM32CubeMP15 Package]] or [[STM32CubeMP2 Package architecture|STM32MP2 Package]] can directly change the SYSCFG at runtime from various drivers. | |||
* '''Linux<sup>®</sup>''': for example, [[I2C overview|Linux I2C driver]] uses the syscon framework<ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/mfd/syscon.yaml}}</ref> to enable the I2C fast mode plus (FM+) in the SYSCFG for the instances allocated to itself | |||
* '''STM32Cube''': for example, [[STM32CubeMP15 Package architecture|I2C HAL driver]] uses its [[STM32CubeMP15 Package architecture|SYSCFG HAL driver]] to do the same on the instances allocated to itself | |||
==How to assign and configure the peripheral== | |||
The peripheral assignment can be done via the [[STM32CubeMX]] graphical tool (and manually completed if needed).<br /> | |||
This tool also helps to configure the peripheral: | |||
* partial device trees (pin control and clock tree) generation for the OpenSTLinux software components, | |||
* HAL initialization code generation for the STM32CubeMPU Package. | |||
The configuration is applied by the firmware running in the context in which the peripheral is assigned. | |||
==References== | |||
<references/> | |||
<noinclude> | <noinclude> | ||
[[Category:Core peripherals]] | [[Category:Core peripherals]] | ||
{{ArticleBasedOnModel | Internal peripheral article model}} | |||
{{PublicationRequestId | 9289 | 2018-10-17 | AlainF}} | |||
</noinclude> | </noinclude> |
Latest revision as of 15:18, 4 January 2024
1. Article purpose[edit | edit source]
The purpose of this article is to:
- briefly introduce the SYSCFG peripheral and its main features,
- indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
- list the software frameworks and drivers managing the peripheral,
- explain how to configure the peripheral.
2. Peripheral overview[edit | edit source]
The SYSCFG peripheral is used to configure various system aspects like IOs compensation, Ethernet clocking path, …
Refer to the STM32 MPU reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.
3. Peripheral usage[edit | edit source]
This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.
3.1. Boot time assignment[edit | edit source]
3.1.1. On STM32MP1 series[edit | edit source]
The SYSCFG peripheral is configured by TF-A and U-Boot at boot time.
Click on to expand or collapse the legend...
Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:
- ⬚ means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
- ☐ means that the peripheral can be assigned to the given boot time context.
- ☑ means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
- ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32 MPU reference manuals.
Domain | Peripheral | Boot time allocation | Comment ![]() | |||
---|---|---|---|---|---|---|
Instance | Cortex-A7 secure (ROM code) |
Cortex-A7 secure (TF-A BL2) |
Cortex-A7 non-secure (U-Boot) | |||
Core | SYSCFG | SYSCFG | ✓ | ☑ | ☑ |
3.1.2. On STM32MP2 series[edit | edit source]
Click on to expand or collapse the legend...
- ⬚ means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
- ☐ means that the peripheral can be assigned to the given boot time context.
- ☑ means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
- ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.
Domain | Peripheral | Boot time allocation | Comment ![]() | |||
---|---|---|---|---|---|---|
Instance | Cortex-A35 secure (ROM code) |
Cortex-A35 secure (TF-A BL2) |
Cortex-A35 non-secure (U-Boot) | |||
Core | SYSCFG | SYSCFG | ✓ | ☑ | ☑ |
3.2. Runtime assignment[edit | edit source]
3.2.1. On STM32MP13x lines
[edit | edit source]
Click on to expand or collapse the legend...
Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:
- ⬚ means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
- ☐ means that the peripheral can be assigned to the given runtime context.
- ☑ means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
- ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.
Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP13 reference manuals.
Domain | Peripheral | Runtime allocation | Comment ![]() | ||
---|---|---|---|---|---|
Instance | Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) | |||
Core | SYSCFG | SYSCFG | ☑ | ☑ |
3.2.2. On STM32MP15x lines
[edit | edit source]
Click on to expand or collapse the legend...
Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:
- ⬚ means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
- ☐ means that the peripheral can be assigned to the given runtime context.
- ☑ means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
- ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.
Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.
Domain | Peripheral | Runtime allocation | Comment ![]() | |||
---|---|---|---|---|---|---|
Instance | Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) |
Cortex-M4 (STM32Cube) | |||
Core | SYSCFG | SYSCFG | ☑ | ☑ | ☑ |
3.2.3. On STM32MP25x lines
[edit | edit source]
Click on to expand or collapse the legend...
Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:
- ⬚ means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
- ☐ means that the peripheral can be assigned to the given runtime context.
- ☑ means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
- ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.
Domain | Peripheral | Runtime allocation | Comment ![]() | |||||
---|---|---|---|---|---|---|---|---|
Instance | Cortex-A35 secure (OP-TEE / TF-A BL31) |
Cortex-A35 non-secure (Linux) |
Cortex-M33 secure (TF-M) |
Cortex-M33 non-secure (STM32Cube) |
Cortex-M0+![]() (STM32Cube) | |||
Core | SYSCFG | SYSCFG | ☑ | ☑ | ☑ | ☑ |
4. Software frameworks and drivers[edit | edit source]
Below are listed the software frameworks and drivers managing the SYSCFG peripheral for the embedded software components listed in the above tables.
Linux and STM32CubeMP15 Package or STM32MP2 Package can directly change the SYSCFG at runtime from various drivers.
- Linux®: for example, Linux I2C driver uses the syscon framework[1] to enable the I2C fast mode plus (FM+) in the SYSCFG for the instances allocated to itself
- STM32Cube: for example, I2C HAL driver uses its SYSCFG HAL driver to do the same on the instances allocated to itself
5. How to assign and configure the peripheral[edit | edit source]
The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:
- partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
- HAL initialization code generation for the STM32CubeMPU Package.
The configuration is applied by the firmware running in the context in which the peripheral is assigned.
6. References[edit | edit source]