This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.The following pages link to Template:=:
Displayed 100 items.
- Debugging the Linux kernel using the GDB (transclusion) (← links)
- Hardware random overview (transclusion) (← links)
- GStreamer troubleshooting grid (transclusion) (← links)
- Wayland Weston troubleshooting grid (transclusion) (← links)
- How to add a customer application (transclusion) (← links)
- How to customize the Linux kernel (transclusion) (← links)
- DFSDM Linux driver (transclusion) (← links)
- Ethernet device tree configuration (transclusion) (← links)
- NVMEM overview (transclusion) (← links)
- How to configure the Weston keyboard layout (transclusion) (← links)
- How to integrate an external software package (transclusion) (← links)
- How to boot the kernel via TFTP from U-Boot (transclusion) (← links)
- How to manually update bootloaders (transclusion) (← links)
- How to stop and start Weston (transclusion) (← links)
- How to stream camera over network (transclusion) (← links)
- Trace and debug scenario - UART issue (transclusion) (← links)
- How to set up a SocketCAN interface (transclusion) (← links)
- How to send or receive CAN data (transclusion) (← links)
- How to support UBIFS through MTD (transclusion) (← links)
- How to support EXT4 through MMC (transclusion) (← links)
- How to configure ethernet interface (transclusion) (← links)
- How to perform ssh connection (transclusion) (← links)
- How to perform ping test (transclusion) (← links)
- Configfs (transclusion) (← links)
- How to configure a WLAN interface on hotspot mode (transclusion) (← links)
- WLAN and Bluetooth hardware component (transclusion) (← links)
- Visual troubleshooting grid (transclusion) (← links)
- How to set up a Bluetooth connection (transclusion) (← links)
- How to scan Bluetooth devices (transclusion) (← links)
- How to scan BLE devices (transclusion) (← links)
- How to profile video framerate (transclusion) (← links)
- How to monitor the display framerate (transclusion) (← links)
- STM32MP15 resources (transclusion) (← links)
- Top Linux command line (transclusion) (← links)
- How to control a RNG in userspace (transclusion) (← links)
- How to retrieve Cortex-M4 logs after crash (transclusion) (← links)
- How to monitor the GCNANO GPU load (transclusion) (← links)
- DRM KMS troubleshooting grid (transclusion) (← links)
- How to play audio (transclusion) (← links)
- Reading tips (transclusion) (← links)
- How to assign an internal peripheral to an execution context (transclusion) (← links)
- Debugfs (transclusion) (← links)
- USB overview (transclusion) (← links)
- SPI overview (transclusion) (← links)
- How to cross-compile with the Distribution Package (transclusion) (← links)
- HDP Linux driver (transclusion) (← links)
- DRM KMS overview (transclusion) (← links)
- CMSIS-SVD environment and scripts (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP157x-DK2/Let's start/Populate the target and boot the image (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP157x-DK2/Let's start/Execute basic commands (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP157x-DK2/Develop on Arm® Cortex®-A7/Create a simple hello-world application (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP157x-DK2/Develop on Arm® Cortex®-M4/Modify, rebuild and reload a firmware (transclusion) (← links)
- How to start the coprocessor from the bootloader (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP157x-EV1/Let's start/Populate the target and boot the image (transclusion) (← links)
- Sysdig (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP157x-EV1/Let's start/Execute basic commands (transclusion) (← links)
- Systemtap (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP157x-EV1/Develop on Arm® Cortex®-A7/Create a simple hello-world application (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP157x-EV1/Develop on Arm® Cortex®-M4/Modify, rebuild and reload a firmware (transclusion) (← links)
- Create a simple hello-world application (transclusion) (← links)
- Populate the target and boot the image (transclusion) (← links)
- How to accelerate JPEG compression and decompression (transclusion) (← links)
- How to calibrate the touchscreen (transclusion) (← links)
- How to compile the device tree with the Developer Package (transclusion) (← links)
- How to configure system resources (transclusion) (← links)
- How to get name and current status of a DRM connector (transclusion) (← links)
- How to install JAVA JDK (transclusion) (← links)
- How to modify the panel backlight (transclusion) (← links)
- How to optimize the boot time (transclusion) (← links)
- How to record audio (transclusion) (← links)
- STM32CubeMP15 Package release note (transclusion) (← links)
- STM32CubeProgrammer OTP management (transclusion) (← links)
- How to configure OP-TEE (transclusion) (← links)
- Modify, rebuild and reload a firmware (transclusion) (← links)
- How to build Linux kernel user space tools (transclusion) (← links)
- IKS01Ax MEMS expansion board (transclusion) (← links)
- How to protect the coprocessor firmware (transclusion) (← links)
- How to use SPI from Linux userland with spidev (transclusion) (← links)
- How to use the RTC (transclusion) (← links)
- Coprocessor management troubleshooting grid (transclusion) (← links)
- Package repository for OpenSTLinux distribution (transclusion) (← links)
- Wrapper for FSBL images (transclusion) (← links)
- How to update OTP with U-Boot (transclusion) (← links)
- How to configure U-Boot for your board (transclusion) (← links)
- STPM4RasPI expansion board (transclusion) (← links)
- How to read or write peripheral registers (transclusion) (← links)
- How to build and use an SDK for QT (transclusion) (← links)
- How to install Node-RED (transclusion) (← links)
- How to install a simple web browser (transclusion) (← links)
- How to load U-Boot with STM32CubeProgrammer (transclusion) (← links)
- How to configure TF-A FIP (transclusion) (← links)
- How to configure TF-A FW CONFIG (transclusion) (← links)
- IKS01A3 MEMS expansion board (transclusion) (← links)
- IKS01A2 MEMS expansion board (transclusion) (← links)
- STM32MP13 U-Boot (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP135x-DK/Let's start/Populate the target and boot the image (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP135x-DK/Let's start/Execute basic commands (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP135x-DK/Develop on Arm® Cortex®-A7/Create a simple hello-world application (transclusion) (← links)
- How to load U-Boot with dfu-util (transclusion) (← links)
- How to measure the DDR throughput (transclusion) (← links)