Unpack the STM32MP135x-DK board

< Getting started‎ | STM32MP1 boards‎ | STM32MP135x-DK‎ | Let's start
Revision as of 15:29, 7 March 2023 by Registered User (Connection)
(diff) ← Older revision | Latest revision (diff) | Newer revision → (diff)

Applicable for STM32MP13x lines

STM32MP135x-DK.png
Let's start Develop on Arm® Cortex®-A7
Step category in.png Unpack the board Step.png Populate the target and boot the image Step.png Execute basic commands Step.png Use the demo launcher Step category out.png


1 Overview

This first step explains how to unpack the STM32MP135x-DK Discovery kit More info green.png and the additional equipment you need.
The following block diagram provides high-level information on how to connect them together.

STM32MP1 connection block diagram

2 Out-of-the-box kit

STM32MP135x-DK top view
STM32MP135x-DK bottom view

3 Required equipment

The following table lists the equipment required to start playing with your STM32MP135x-DK More info green.png board.
Some of them are delivered within the STM32MP135x-DK Discovery kit More info green.png. The others need to be purchased separately.

STM32MP135x-DK Discovery kit More info green.png Flexible development platform for STM32MP13 microprocessor devices Delivered
MicroSD card To be populated with the OpenSTLinux Distribution (Linux software),
and providing extra storage capacity.
A 2-Gbyte minimum microSD card is required.
Delivered
USB Type-C™ to USB Type-C™ cable Used to connect the STM32MP135x-DK Discovery kit More info green.png to the power supply Delivered
Micro USB Type-B to USB Type-A cable Used to connect the STM32MP135x-DK Discovery kit More info green.png to the PC
through the USB micro-B (ST-LINK/V3E)
Not delivered
USB Type-C™ to USB Type-A cable Used to connect the STM32MP135x-DK Discovery kit More info green.png to a USB OTG device. Not delivered
5V/3A power supply The power supply should be able to output 5V / 3A (15W) Not delivered
Laptop A Linux PC running Ubuntu 16.04 is required. Not delivered
Ethernet cable (optional) Used to connect the STM32MP135x-DK Discovery kit More info green.png through ssh Not delivered

4 Connection

  • Connect your laptop to the board ST-LINK/V3E port through the micro USB Type-B to USB Type-A cable.
  • Connect the USB Type-C™ to USB Type-C™ cable to the 5V/3A power supply.
  • Connect your laptop to the board USB Type-C™ OTG port through the USB Type-C™ to USB Type-A cable.
  • Optionally connect your Ethernet network to the board Ethernet port through the Ethernet cable.
STM32MP135x-DK Discovery kit connection



Back button.png Overview button.png Next button.png