1. Overview[edit source]
This first step explains how to unpack the STM32MP135x-DK Discovery kit and the additional equipment you need.
The following block diagram provides high-level information on how to connect them together.
![](/stm32mpu/nsfr_img_auth.php/e/e1/STM32MP1_connection_block_diagram.png)
STM32MP1 connection block diagram
2. Out-of-the-box kit[edit source]
File:STM32MP135F-DK angle2.jpg
STM32MP135x-DK back view
File:STM32MP135F-DK verso.jpg
STM32MP135x-DK front view
3. Required equipment[edit source]
The following table lists the equipment required to start playing with your STM32MP135x-DK board.
Some of them are delivered within the STM32MP135x-DK Discovery kit . The others need to be purchased separately.
4. Connection[edit source]
- Connect your laptop to the board ST-LINK/V3E port through the micro USB Type-B to USB Type-A cable.
- Connect the USB Type-C™ to USB Type-C™ cable to the 5V/3A power supply.
- Connect your laptop to the board USB Type-C™ OTG port through the USB Type-C™ to USB Type-A cable.
- Optionally connect your Ethernet network to the board Ethernet port through the Ethernet cable.