This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. STM32CubeProgrammer errata 2.23.x
2. Main fixed issues for 2.23.0
| ID | Summary |
|---|---|
| 8985 | Incorrect STM32_PRG_PATH using macOS ARM installer |
| 8844 | Need latest STM32WB_FUS_Operator V3.1.1 in CubeProg |
| 86 | Programming error, timeout modification seems not working. DFU timeout |
| 9269 | [DATABASE]STM32CubeProgrammer 2.22 GUI option byte page can't display for STM32F767BG |
| 8910 | [G0] Unable to change NRST_MODE on stm32g031j6m6 |
| 8967 | [L4] OTP programming wrong granularity |
| 8896 | [Multi Language] Memory leak in Chinese and Japanese languages causing a crash |
| 101 | [N6]Wrong OTP19 BOOTROM_CONFIG_10 bitfield visualization |
| 9022 | [OB Factory reset]STM32U585 bricked after using factory reset operation if BOOT_LOCK 1 |
| 8746 | [STM32CubeProgrammer] Fails to Execute --power off/on in STM32_Programmer_CLI |
| 8874 | [Signing Tool] Header Version not Accepted with PKCS#11 API |
| 8979 | [TPC] Unable to load HSM_P11_Lib.dll |
| 90 | unable to connect to G5 device with an stlinkV2 |
3. Known problems and limitations
- Integrity check:
- STM32H7 microcontrollers: support integrity check for SFI:
- Only the devices with a bootloader version higher than 0x91 are supported.
- STM32CubeProgrammer does not support the devices with older bootloader versions. Users must use STM32CubeProgrammer v2.9.0 to use devices with old bootloader versions.
- STM32H73xxx microcontrollers: support integrity check for SFI/SFIx:
- Only the devices with a bootloader version higher than 0x93 are supported.
- STM32CubeProgrammer does not support the devices with older bootloader versions. Users must use STM32CubeProgrammer v2.9.0 to use devices with old bootloader versions.
- STM32H7Bxxx microcontrollers: support integrity check for SFI/SFIx:
- Only the devices with a bootloader version equal to or higher than 0x92 are supported.
- STM32CubeProgrammer does not support the devices with older bootloader versions. Users must use STM32CubeProgrammer v2.9.0 to use devices with old bootloader versions.
- STM32H7 microcontrollers: support integrity check for SFI:
- SFIx fails when programming:
- Large flash memory content on Linux® via the UART interface.
- Small flash memory content on supported bootloader interfaces with all platforms.
- USB interoperability issue on macOS® due to ST-LINK limitation.
- STM32H7 microcontrollers:
- STM32CubeProgrammer does not support SFI.
- STM32H7Axxx/Bxxx microcontrollers: Download verification issue with OTP.
- STM32H7Rx/7Sx microcontrollers:
- Erasing the external flash memory is not supported using IWDG.
- GUI: the external memory edition is not supported via USB and UART while connected to the OpenBootloader.
- Option bytes are not supported via OpenBootloader interfaces.
- STM32L0 microcontrollers:
- Register access mode incorrectly displayed for register viewer.
- STM32L4R5xx microcontrollers:
- Issues occur when erasing sectors in bank 2 memory with the UART interface.
- STM32U3 microcontrollers:
- Limited support via JTAG (functional only with mode = normal and reset = HWrst).
- STM32U3C5/STM32U3B5: Unable to program binary or change OB when IWDG_SW=0
- STM32U335/STM32U345: The programming operation fails when Swap_Bank is enabled.
- STM32U5 microcontrollers:
- Unable to read the chip ID via J-Link when RDP is set to Level 2.
- OTP memory programming failure with CLI when TZEN is enabled.
- STM32U535/545 microcontrollers: SFIx is not supported.
- STM32U59xxx microcontrollers: SFIx only supports the area E installation with OTFDEC region 1 (region 0 on TPC).
- STM32U5Fxxx and STM32U5Gxxx microcontrollers: Unable to program SFIx via SPI/I2C on GUI.
- STM32U575/STM32U585 microcontrollers: For CPNs with flash Size 1M, failed to erase using Erase selected sectors when SWAP_BANK is enabled.
- STM32U535/STM32U545 microcontrollers: for flash Size 256K For CPNs with flash size 2M, failed to erase using Erase selected sectors when SWAP_BANK is enabled with the UART interface.
- STM32L43 and STM32L45 microcontrollers:
- Failed to erase a part of the last sector using the GUI with the SWD interface.
- STM32WBA microcontrollers:
- OpenBootloader via SPI: cannot connect to STM32CubeProgrammer when the baud rate is below 3000 Bd.
- “Connect Under Reset” is not working when called by STM32CubeIDE.
- STM32WBA2 microcontrollers:
- Erase operation failed when the External loader is selected. Note: Deselect the external flash to be able to perform the erase operation
- USB interoperability issue on macOS due to STLINK limitation
- Unable to read the Chip ID of the STM32U5 via JLINK when RDP is set to Level 2.
- STM32H74x/5x/7x: When connecting the target via JLINK, the BCM4 option byte is removed from STM32CubeProgrammer if it has been disabled.
- STM32WL33 microcontrollers:
- Failed to connect with Hotplug mode on CLI.
- STM32CubeProgrammer fails to program RDP=0xABACABAD on WL33.
- STM32L5 microcontrollers:
- Unable to read, write, or erase the external flash memory when TZEN is enabled.
- SFI programming failed via UART on Linux.
- STM3V8 microcontroller:
- Erase NVM High Cycle data not working, a workaround is to write 0xFFFFFFFF in the register.
- Incremental programming:
- Is not supported when TrustZone is enabled, the tool switches automatically to normal programming procedure.
- Is an experimental feature with limited test coverage:
- For Internal Flash programming, tested devices are: STM32C03x, STM32C05x, STM32C09x, STM32F101/F102/F103, STM32F37xx, STM32F411xC/E, STM32F72x/STM32F73x, STM32F76x/STM32F77x, STM32G03x/STM32G04x, STM32G0B0xx/B1xx/C1xx, STM32G491xx, STM32H50x, STM32H533/523, STM32H56x/573, STM32H72x/STM32H73x, STM32H7R/Sxx, STM32L05x/L06x/L010, STM32L4Pxxx/STM32L4Qxxx, STM32L4x1/STM32L475xx/STM32L476xx/STM32L486xx, STM32L5xx, STM32U0xx, STM32U3xx, STM32U535/STM32U545, STM32U575/STM32U585, STM32U59x/5Ax, STM32WB5x/35xx, STM32WBA52/54/55, STM32WBA6x, STM32WLxx
- For external flash programming, tested boards are: STM32H735G-DK, STM32H7S78-DK, STM32H573I-DK, STM32U575I-EV, STM32WBA65I-DK1.
- The automatic mode doesn't work with UART interface when using an STLink with Dual VCP, the STLink configuration must be changed to single VCP.
- In windows 10 32 bits: STM32TrustedPackageCreator display can be cut when maximizing the window.
- OBkey provisioning with JLINK is not supported, currently the CLI says it clearly, but the GUI message doesn't.
- SWD multidrop:
- Connection fails on U0 and WL dual core.
- The user must set targetsel to 0xxxxxxx instead of 0x0xxxxxx.
- There is an instability when programming in “under_reset” mode, it's recommended to use "Normal" mode.
- SFI not working.
- Memory map export supports a maximum of 9 segments.
- SWV feature is provided as a beta functionality for devices V8 and C5. It is not fully validated.
- MCU factory reset is supported only via ST-Link.
- RDP regression with password is supported only via ST-Link.
- SFI feature:
- For the full list of supported devices, please refer to AN4992.
- Parallel SFI Programming with Shared HSM is not supported.
- Starting from STM32CubeProgrammer v2.21.0 "-align" option using STM32_SigningTool_CLI is mandatory with STM32N6.
- Write and erase operations using an external flash with a start address @0x00000000 is not supported.
- Flash high cycle:
- Programming is not supported at secure addresses.
- A mass erase is required before programming the full flash high cycle area (bank1 + bank2)”,.
- The OTP memory programming is not supported when TZEN is enabled for CM33 SoCs.
- Display issues occur on Fedora when the system display scale is set to 125%; the recommended scale is 100%.
- Any file path provided as an input argument to the STM32CubeProgrammer CLI that contains spaces must be enclosed in quotation marks.