This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Main fixed issues for 2.19.0
| ID | Summary |
|---|---|
| 196145 | STM32U5: Issue encountered while programming a quad word in OTP memory. |
| 185269 | STM32H5: Provisioning failed on Virgin device. |
| 193258 | STM32U0: Wrong bootloader version display. |
| 198269 | STM32H5: Nonsecure area display issue after erasing secure watermark sector. |
| 198280 | STM32U5: Device authentication ID reading issue. |
| 185103 | Display issue when attempting to run the STM32TrustedPackageCreator_CLI within a Docker container. |
| 199305 | STM32L5: Memory programming failure when TZEN is enabled. |
| 199379 | Cannot write to MPU OTPs using CLI. |
| 194583 | STM32MP135: Large image programming issue. |
| 199332 | STM32N6: External memory sectors display issue. |
| 192569 | HSM_P11_Lib.dll cannot be loaded on Windows® 32 bits. |
| 193440 | List command does not display UART ports unless an ST-LINK is connected. |
| 161165 | STM32U5Axxx/Fxxx/Gxxx: Wrong size sector when DBANK=0. |
| 188164 | Libusb warnings when using serial number parameter on Linux®. |
2. Known problems and limitations
- Integrity check:
- STM32H7 microcontrollers: support integrity check for SFI:
- Only the devices with a bootloader version higher than 0x91 are supported.
- STM32CubeProgrammer does not support the devices with older bootloader versions. Users must use STM32CubeProgrammer v2.9.0 to use devices with old bootloader versions.
- STM32H73xxx microcontrollers: support integrity check for SFI/SFIx:
- Only the devices with a bootloader version higher than 0x93 are supported.
- STM32CubeProgrammer does not support the devices with older bootloader versions. Users must use STM32CubeProgrammer v2.9.0 to use devices with old bootloader versions.
- STM32H7Bxxx microcontrollers: support integrity check for SFI/SFIx:
- Only the devices with a bootloader version equal to or higher than 0x92 are supported.
- STM32CubeProgrammer does not support the devices with older bootloader versions. Users must use STM32CubeProgrammer v2.9.0 to use devices with old bootloader versions.
- STM32H7 microcontrollers: support integrity check for SFI:
- Debug authentication is not supported on Windows® 32 bits.
- SFIx fails for large flash memory content on Linux® via the UART interface.
- USB interoperability issue on macOS® due to ST-LINK limitation.
- STM32H7 microcontrollers:
- STM32CubeProgrammer does not support SFI.
- STM32H7Axxx/Bxxx microcontrollers: Download verification issue with OTP.
- STM32H7Rx/7Sx microcontrollers:
- Erasing the external flash memory is not supported using IWDG.
- GUI: the external memory edition is not supported via USB and UART while connected to the OpenBootloader.
- Option bytes are not supported via OpenBootloader interfaces.
- STM32L0 microcontrollers:
- Register access mode incorrectly displayed for register viewer.
- STM32L4R5xx microcontrollers:
- Issues occur when erasing sectors in bank 2 memory with the UART interface.
- STM32L5 and STM32U5 microcontrollers:
- Unable to read, write, or erase the external flash memory when TZEN is enabled.
- STM32U3 microcontrollers:
- Limited support via JTAG (functional only with mode = normal and reset = HWrst).
- STM32U5 microcontrollers:
- Unable to read the chip ID via J-Link when RDP is set to Level 2.
- OTP memory programming failure with CLI when TZEN is enabled.
- STM32U535/545 microcontrollers: SFIx is not supported.
- STM32U59xxx microcontrollers: SFIx only supports the area E installation with OTFDEC region 1 (region 0 on TPC).
- STM32U5Fxxx and STM32U5Gxxx microcontrollers: Unable to program SFIx via SPI/I2C on GUI.
- STM32WBA microcontrollers:
- OpenBootloader via SPI: cannot connect to STM32CubeProgrammer when the baud rate is below 3000 Bd.
- “Connect Under Reset” is not working when called by STM32CubeIDE.
- STM32WBA6xxx microcontrollers with 2 Mbytes of flash memory: Programming and OB configuration is not supported with mode hotplug when TZEN=1.
- Wrong maximum value for DTR/RTS pulse delay on GUI.
- Updater: Unable to perform the upgrade using the second option "Use System Proxy Parameters".