How to write a variable from flow

It is possible to write a variable value directly from a flow or dashboard, without entering the value in the "write panel" node. Here is a solution using standard nodes: A slider is used to set the value (but can be done by any node) then the “template” node formats the payload and the change node sets the topic.

1. Example :

1.1. Reference flow :

1.2. The template node:

 

The variable address and variable type must be filled here. For the type and address, the easiest way is to try first with a writing panel and a debug node, and see the values. The Payload value from the input will be inserted in the template. (the value to write)

The next node is a “change” node to set the topic to “write”



1.3. The result :

When the slider is moved, the new value is written to g_constDouble

2. Type definition :

The type number is representing the variable type :

  • 1: Unsigned 8-bit
  • 2: Signed 8-bit
  • 3: Unsigned 16-bit
  • 4: Signed 16-bit
  • 5: Unsigned 32-bit
  • 6: Signed 32-bit
  • 9: Float
  • 10: Double