Revision as of 07:53, 28 February 2020 by Registered User
(diff) ← Older revision | Latest revision (diff) | Newer revision → (diff)

A new category, STMicroElectronics, has been added in the palette manager. These specific nodes designed for STM32 devices are described below.

1. Design nodes

These nodes are used to create flows from target to variable, rendered in dashboard view. Design nodes are not visible on the dashboard.

1.1. Acquisition out

Acquisition out

This allows the user to define and/or select a probe configuration (probe name, protocol and frequency). This node opens and closes the connection, and send commands to the selected probe.

See STM32CubeMonitor:How to select the target for further details.

1.2. Acquisition in

Acquisition in

This allows user to define and/or select a probe configuration (probe name, protocol and frequency). This node receives data from the selected probe.

The acquisition in node is typically designed to be back-linked with one, or several, processing nodes.

See STM32CubeMonitor:How to select the target for further details.

1.3. Variables

Variables

This allows a variables group to be configured to hold a set of variables and few additional parameters that are useful for communication with the target.

See How to add a variable to monitor.

See How to extract address from ELF files.

See How to modify frequency of acquisition.

1.4. Processing

Processing

This transforms each input message representing one measurement of a group of variables into one message every 50 ms per variable. The message contains one, or several, duplets (x and y). It is also possible to define expressions and statistics based on the individual measurements and log options. This node allows filtering of probe data, per variables group.

See How to record and replay data

See How to perform additional calculations on measurements

2. Dashboard nodes

These nodes are visible in dashboard mode; they allow the user to visualize or modify variables used on the target.

2.1. Chart

Chart

This node allows input values to be plotted on a chart. This can be a line chart or a bar chart.

See STM32CubeMonitor:How to configure the chart for further details.

2.2. Write panel

Write panel

This adds a "write" widget to the dashboard. See STM32CubeMonitor:How to write variables for further details.

---> How to use basic flow