Registered User m (→Fixed issues) |
Registered User m (→General issues) |
||
| (12 intermediate revisions by 2 users not shown) | |||
| Line 1: | Line 1: | ||
==Warning== | ==Warning== | ||
STM32CubeIDE uses gdbserver to connect to the target. Be aware that gdbserver does not have any built-in security. Do not run gdbserver connected to any public network. A GDB connection to gdbserver provides access to the target system with the same privileges as the user running gdbserver. | STM32CubeIDE uses gdbserver to connect to the target. Be aware that gdbserver does not have any built-in security. Do not run gdbserver connected to any public network. A GDB connection to gdbserver provides access to the target system with the same privileges as the user running gdbserver. | ||
==Delta between 2.1.0 and 2.1.1== | |||
{| | |||
|- style="background: DeepSkyBlue; width:100px; text-align:left;" | |||
! style="width:100px;" |ID!! style="width:1020px;" |Summary | |||
|- style="height:100px;" | |||
|- | |||
|TIDEC1-6864|| CMake update to 3.30.8 to support "QUOTE" expression. | |||
|- | |||
|TIDEC1-6865 | |||
|JLink update to 9.24 to fix issues in the live expression view during the debug session. | |||
|} | |||
==Limitations== | ==Limitations== | ||
{| | {| | ||
| Line 99: | Line 111: | ||
221817/221820 | 221817/221820 | ||
|If GCC14 is used as the toolchain within STM32CubeIDE, some examples might have errors and warnings in compilation for the following families: STM32G0, STM32H5, STM32H7/H7RS, STM32N6, STM32WB/WB0, STM32WBA, STM32WL/WL3. | |||
228025 | |||
|If GCC14 is used as the toolchain within STM32CubeIDE, some examples might have errors and warnings in compilation for the following families: STM32G0, STM32H5, STM32H7/H7RS, STM32N6, STM32WB/WB0, STM32WBA, STM32WL/WL3. To work around these errors GCC13 should be set as a default toolchain: | |||
- Go to Window > preferences > STM32Cube > Toolchain manager- Once all GCC are listed, select GCC13.3.rel1 then click on install button the follow the update site installation steps | |||
|- | |- | ||
|221438 | |221438 | ||
| Line 293: | Line 308: | ||
Disable the automatic selection of a lesser printf variant by adding `-Wl,--no-auto-printf-variant-selection` to the linker flags in cmake/starm-clang.cmake. | Disable the automatic selection of a lesser printf variant by adding `-Wl,--no-auto-printf-variant-selection` to the linker flags in cmake/starm-clang.cmake. | ||
|- | |||
|TIDEC1-6907 | |||
|When a debug session is firstly started in STM32CubeIDE 2.1.1 after a fresh installation on macOS 15 or a later version, a pop-up window may appear with this message "stlink-server" is an app downloaded from internet, do you want to Open it ?", it is advised to click on "Open" button to allow debug operation to work as expected. | |||
|- | |||
|TIDEC1-6909 | |||
|When CubeIDE 2.1.1 is firstly launched after a fresh installation on macOS 15 or a later version, a pop-up window may appear asking to allow STM32CubeIDE to scan for devices on local networks.Click the ‘Allow’ button when this dialogue box appears, as STM32CubeIDE needs to establish a TCP connection and will interact with connected boards during debugging operations. | |||
|} | |} | ||
| Line 381: | Line 402: | ||
Workaround: | Workaround: | ||
* | * Use the default compiler (GCC14) or install GCC13 available through update site mechanism. | ||
* Compile without MVE extension, which can be done by passing argument "-mcpu=cortex-m55+nomve", in Settings > GCC compiler > Miscellaneous. | * Compile without MVE extension, which can be done by passing argument "-mcpu=cortex-m55+nomve", in Settings > GCC compiler > Miscellaneous. | ||
|- | |- | ||
| Line 453: | Line 474: | ||
|- | |- | ||
|CMake | |CMake | ||
|3. | |3.30.8 | ||
|- | |- | ||
|Ninja | |Ninja | ||
| Line 465: | Line 486: | ||
|- | |- | ||
| SEGGER J-Link | | SEGGER J-Link | ||
|9. | |9.24 | ||
|- | |- | ||
|STARM-Clang | |STARM-Clang | ||
Latest revision as of 09:25, 16 March 2026
1. Warning
STM32CubeIDE uses gdbserver to connect to the target. Be aware that gdbserver does not have any built-in security. Do not run gdbserver connected to any public network. A GDB connection to gdbserver provides access to the target system with the same privileges as the user running gdbserver.
2. Delta between 2.1.0 and 2.1.1
| ID | Summary |
|---|---|
| TIDEC1-6864 | CMake update to 3.30.8 to support "QUOTE" expression. |
| TIDEC1-6865 | JLink update to 9.24 to fix issues in the live expression view during the debug session. |
3. Limitations
| ID | Summary |
|---|---|
| 133183 | Unable to debug using FreeRTOS aware with a J-LINK Ultra+ in STM32CubeIDE 1.10.1. |
| 138771 | To start debugging in the NS zone when the product status is TZ-Closed for the STM32H5 using ST-Link GDBServer, add the following script to "Run Commands" in the debugging configuration.
For the "Reset & Restart" button to work:
|
| 143485 | Post-build commands are restored by using one of the following two options:
|
| 146043 | On STM32H745 Cortex-M4 dual-core projects, the predefined breakpoint is maintained but not caught upon run. |
| 152549 | From GCC11, the build can be in error with some functions:
_close, fstat, _getpid, _isatty, _kill, _lseek, _open, _read, _write, _gettimeofday This is due to the state definition using the system information. In main.c, add the following to address the issue: __attribute__((weak)) void _close(void) {} __attribute__((weak)) void _lseek(void) {} __attribute__((weak)) void _read(void) {} __attribute__((weak)) void _write(void) {} |
| 166245 | When using the STM32CubeMP13 bare-metal firmware and activating Azure® RTOS ThreadX, the STM32CubeIDE linker file must contain the following section to avoid compilation issues:
|
| 171852 | The implemented toolchain allocates to an enum type only as many bytes as needed for the declared range of possible values. |
| 174727 | STM32CubeIDE cannot build the project automatically after changing the IP configuration. It cannot automatically control this configuration. The user must increase flash memory size manually when needed, depending on the configuration. |
| 189888
213181 |
The "connect under reset" connection mode is not supported on STM32WB05, STM32WB09, STM32WL30, STM32WL31, and STM32WL33 microcontrollers. A hardware reset pulse is applied to connect and debug. |
| 192219 | For Cortex-M55 (like STM32N6), GCC12 and earlier versions detect warnings using when OFast and O3 optimizations level.
Workaround:
|
| 207895 | When importing a project from STM32CubeMX to STM32CubeIDE while using macOS or Ubuntu, a pop-up message or failure can appear. |
| 213261 | For STM32WBA65I-DK, incremental flashing is not supported for external flash. Flashing is performed according to the legacy mode. |
| 221619 | While debugging STM32H7S78-DK and NUCLEO-H7S3L8 using OpenOCD, a failure can occur when reading memory. This does not block debugging. |
| 221790/221794
221795/221798 221799/221803 221805/221816 221817/221820 228025 |
If GCC14 is used as the toolchain within STM32CubeIDE, some examples might have errors and warnings in compilation for the following families: STM32G0, STM32H5, STM32H7/H7RS, STM32N6, STM32WB/WB0, STM32WBA, STM32WL/WL3. To work around these errors GCC13 should be set as a default toolchain:
- Go to Window > preferences > STM32Cube > Toolchain manager- Once all GCC are listed, select GCC13.3.rel1 then click on install button the follow the update site installation steps |
| 221438 | Cmake projects are not supported for MPx product. |
| 226196 | After installing STM32CubeIDE on Fedora 43 using .rpm_bunle.sh installer, STM32CubeIDE must be started from its installation folder (/opt/st) in command line with sudo mode. This is mandatory to ensure that all build and debug operations are working as expected. |
| 227546 | For Cortex-M0, M0+, M33, and M55, core reset mode is not supported in STM32CubeIDE debug configuration. |
| 227652 | While debugging an RTOS project with rtos-proxy 0.18.0, the call stack displays only the active thread instead of all started threads. |
4. Fixed issues
| ID | Summary |
|---|---|
| 215781 | The PXN field is missing when inspecting the MPU_RLAR_* registers in the system/peripheral register view in STM32CubeIDE for STM32N657X0HxQ. |
| 215689 | When changing variables from live expression and other areas during debugging, the error message "Failed to read all registers from target" appears. |
| 215788 | For Cortex-M55, the system/peripheral register view displays only the nonsecure MPU registers, such as MPU_TYPE_NS, which are defined with a 0x20000 offset and the _NS suffix in the SVD file.
When debugging in the secure context, these nonsecure MPU registers always display a value of 0 in STM32CubeIDE, making them unusable for secure debugging. |
| 220120 | If a disruption occurs during debugging, the user can modify the optimization level in the starm-clang.cmake toolchain file, which is located under ImportedCmakeProjectName/cmake/starm-clang.cmake.
Set the following flags:
|
| 222685 | After importing a project, the interface might remain on the information center. This issue is observed in all types of projects except empty projects. |
| 223135 | When adding a linker folder to a project in STM32CubeIDE, avoid using path variables in the linked folder location, especially WORKSPACE_LOC and ECLIPSE_HOME. Otherwise, the linked folder is deleted after updating the project in STM32CubeMX by performing a new generate code operation on the same project.
Edit the linked folder location in STM32CubeIDE by using the absolute path of the linked folder instead of path variables before starting a new generate code operation in STM32CubeMX on the same project. To do this, follow these steps:
|
5. Known issues
The known issues are split into general, STM32CubeCLT, OS-specific, and target-specific issues.
5.1. General issues
| ID | Summary |
|---|---|
| 59435 | Having a space or a non-ASCII character in the project or workspace path, or installation path, is not fully supported |
| 68184 | Hierarchical projects cannot be imported with the option Copy into workspace. |
| 68440 | Hierarchical projects cannot be renamed. |
| 72498 | To debug an STM32CubeIDE Make file Project, modify the build settings: right click on the imported project >properties >C/C++ Build > MCU settings > select the requested MCU and apply. |
| 89454 | Restart configuration works only for flash memory projects, not for RAM projects. The program counter register is not set correctly. Manual workaround: In Restart configuration, manually set the program counter to the ResetHandler() in RAM: set $pc = 0x20000xxx. |
| 115928 | Editing live expressions while target is running does not work with SEGGER J-Link. |
| 124062 152549 | GCC-10 is stricter regarding the declaration of global variables in header files. Read the GCC-10 porting guide; many warnings and errors result. |
| 133183 | STM32CubeIDE cannot debug using FreeRTOS-aware debugging with J-LINK.
Work-arounds, if: Reset strategy == Connect under reset, requires Initialization commands:
Work-arounds, if: Reset strategy == None (attach mode), requires Initialization commands:
|
| 156812 | Missing string table in Build Analyzer when displaying the byte size of the .rodata section. |
| 159507 | Issues detected when updating STM32CubeIDE version from 1.9.0 to 1.13.1.
It is recommended to reinstall from scratch use the 1.13.1 version and use the old workspace. |
| 162500 | After programming a device in Run mode, STM32CubeIDE opens a new tab with the startup file and gives focus to that tab every time. |
| 170279 | Failure to compile embOS due to missing stack variable. A new section defining _stack_start__ and __stack_end__ must be added to the linker file when required by ThreadX. |
| 183033 | The restore default build configuration feature removes the build commands. |
| 190493 | When exporting a project, already imported, built and exported as Zip file, into different workspace, an error will occur while building it. The following workaround can be applied:
|
| 191504 | The Reset chip and restart debug session button does not work as expected when debugging with STM32CubeIDE the Nucleo-N657X0-Q board. It should reset the debug stack to the main function. Issue can be avoided by adding the "load" command in "Additional commands" in Restart configurations. |
| 199067 | In STM32CubeIDE 1.17.0, Hex files are not generated, setting a post build command:
arm-none-eabi-objcopy -O ihex "project_name.elf" "project_name.hex" is required. |
| 200233 | Compilation error when using toolchain GCC 12.3 with STM32CubeIDE 1.14.1.
As Workaround, GCC12 can be downloaded and load it from local by setting the toolchain
|
| 209826 | if GCC’s fallthrough attribute are used they will be flagged as error. |
| 213509 | If a file is added by the user named main.c it would generate a build fail in the project. Such file naming should be avoided and replaced with mainUser.c for example. |
| 220043 | To be able to display data in “Static Stack Analyser” view for Cmake projects (with GCC or starm-clang), the user needs to add the compilation flags “-fstack-usage” in the toolchain file located under:
Example: set(CMAKE_C_FLAGS "${CMAKE_C_FLAGS} -Wall -fdata-sections -fstack-usage -ffunction-sections") To be able to display data in “Cyclomatic Complexity” view for Cmake projects with GCC toolchain, the user needs to add the compilation flags “-fcyclomatic-complexity”in the toolchain file located under:
Example: set(CMAKE_C_FLAGS "${CMAKE_C_FLAGS} -Wall -fdata-sections -fstack-usage -fcyclomatic-complexity -ffunction-sections") As for Cyclomatic Complexity view is not working for now for CMake with starm-clang toolchain because the flag “-fcyclomatic-complexity” is not yet recognized by st-arm clang. |
| 220348 | Debug is not possible with "Release" build type CMAKE_BUILD_TYPE=Release since the 'Release' mode is defined as '-Oz' in starm-clang.cmake using the LLVM Toolchain. In this case the release flag needs to be updated in the toolchain file. |
| 220942 | When importing an existing Cmake project with multicontext, the build operation will output all elf files (Secure, non-secure, other contexts...), so when starting a debug session on the root project (including all contexts), the user should select what elf file to debug (what is the project, secure or not secure or other because STM32CubeIDE cannot decide what is the application that user wants to debug. |
| 221076 | If GCC 14 toolchain is used, the startup assembly file may not be well formed, a quick fix is to declare symbols LoopCopyDataInit and LoopFillZerobss as functions.
Workaround:
|
| 221275 | After Importing project generated by STM32CubeMX [Using U385 TZ=1] in STM32CubeIDE and building it using UnixMakefiles, the build might finish unexpectedly if the following change is implemented: change Ninja" as the generator --> CMake Configure --> Delete and Reconfigure. |
| 221435 | Creating a CMake project with the static library Template, project generated incorrectly and compilation would fail, source files must be created. |
| 221611 | For STM32N6 family and if debug with semihosting feature is required the following needs to be added in the debug configuration startup tab in order to enable step Over and step into:
Workaround:
|
| 221739 | Using Ubuntu 22.04 or MacOS 15, opening the .ioc file of the imported STM32CubeMX project might fail. In this case:
|
| 221864 | While using LLVM as toolchain, Static stack analyser view may not have any output unless "-fstack-usage" in compliation flags is added manually in toolchain file.
For Cyclomatic view and while using Cmake +GCC, the flag "-fcyclomatic-complexity" in the compilation flags needs to be added in GCC toolchain file. Cyclomatic view however is not supported while using LLVM. |
| 227450 | In versions of ST Arm Clang up to 21.1.1+st.6 (included), when using Picolibc as the C library and printing a floating-point value with a function of the printf family, the linker picks up the wrong implementation of printf if the `l` length specifier isn't used in at least one floating-point format, causing the printed value to be incorrect (0.000000 in most cases).
The following workaround can be used:
Disable the automatic selection of a lesser printf variant by adding `-Wl,--no-auto-printf-variant-selection` to the linker flags in cmake/starm-clang.cmake. |
| TIDEC1-6907 | When a debug session is firstly started in STM32CubeIDE 2.1.1 after a fresh installation on macOS 15 or a later version, a pop-up window may appear with this message "stlink-server" is an app downloaded from internet, do you want to Open it ?", it is advised to click on "Open" button to allow debug operation to work as expected. |
| TIDEC1-6909 | When CubeIDE 2.1.1 is firstly launched after a fresh installation on macOS 15 or a later version, a pop-up window may appear asking to allow STM32CubeIDE to scan for devices on local networks.Click the ‘Allow’ button when this dialogue box appears, as STM32CubeIDE needs to establish a TCP connection and will interact with connected boards during debugging operations. |
5.2. STM32CubeCLT issues
| ID | Summary |
|---|---|
| 214938 | For MacOs install, no paths for "CLANG_GCC_CMSIS_COMPILER" and GCC_TOOLCHAIN_ROOT.
Workaround:
|
5.3. OS-specific issues
5.3.1. Linux®
| ID | Summary |
|---|---|
| 175176 | Using the generic Linux installer, the libncurses must be installed manually. Usage rpm_bundle.sh instead of deb_bundle.sh is recommended. |
5.4. Target-specific issues
5.4.1. STM32H7
| ID | Summary |
|---|---|
| 73552 | Serial Wire Viewer configuration is not reset for STM32H7 devices on the next launch if it was terminated with record active when using ST-LINK GDB server. |
| 79658 | ST-LINK GDB server reports being suspended on address: 0x05F0001 when debugging STM32H7 dual-core devices and the core under debug goes to sleep. |
| 81763 | OpenOCD does not support debugging STM32H7 dual-core devices when the core under debug goes to sleep. |
| 175966 | For H7RS project on Ubuntu with ExtMemLoader context configured, Postbuild commands cannot be passed successfully when STM32CubeIDE is installed with sudo.
Workarounds:
|
| 206638 | While using GCC13 in STM32CubeIDE 1.17.0 or 1.18.0, errors or warnings can be encountered while importing some projects. GCC12 usage is recommended in this scenario. |
5.4.2. STM32L0
| ID | Summary |
|---|---|
| 201878 | Errors will appear when building the imported project ADC_DMA_Transfer for NUCLEO-L010RB.
Workaround: syscall.c file needs to be added to the project. |
5.4.3. STM32MP1
| ID | Summary |
|---|---|
| 73895 | Debugging in production mode requires a network connection. If STM32CubeIDE is configured to use a network proxy, then the IP address of the STM32MP1 board needs to be added to the "Proxy bypass" list. |
| 73896 | The synchronization check between the IP-address entered in launch configuration and the IP-address of the target does not abort the launch in case of mismatch. |
| 212122 | For STM32MP135F-DK (Bare Metal) and while enabling FreeRTOS CMSIS_V2 and to avoid build errors, the RAM alias to DDR_BASE region needs to be assigned.
Workaround:
|
5.4.4. STM32N6
| ID | Summary |
|---|---|
| 192219 | GCC12 and earlier versions detect warning using OFast and O3 optimizations level.
Workaround:
|
| 208549 | If we use the “XSPI_PSRAM_MemoryMapped” example or any similar application, data stored in the external memory could not be viewed by the memory view in STM32CubeIDE. |
| 208579 | In order to read data stored in external memory map mode for STM32N6 family, memory view can be used with Hex rendering: in memory view, check the three dots then Table rendering preferences then switch from Automatic to Manual. |
| 210446 | If the Application context contains any break point even if it is disabled, the debug session will not start.
Workaround:
|
5.4.5. STM32WB0
| ID | Summary |
|---|---|
| 180379 | A false error could be detected on some BLE applications when is included some binary libraries.
The error should be: “missing .note.GNU-stack section implies executable stack” or “NOTE: This behaviour is deprecated and will be removed in a future version of the linker” Workaround:
|
| 183143 | An Error seems to be found once the ThreadX Option is activated for WB05/WB07/WB09. |
| 189888 | For STM32WB0x devices the connection Under Reset type is not supported. |
6. Upgrades
| ID | Summary |
|---|---|
| BusyBox | 1.31.0.st_20240131-1810 |
| Eclipse and CDT | Eclipse 2024-09
CDT 11.6.1 |
| GCC binaries | 14.3.rel1.20251027-0700 |
| JRE | Adoptium® Temurin™ 21.0.9+10 and JavaFX 21.0.9 |
| Make | 4.4.1_st_20231030-1220 |
| CMake | 3.30.8 |
| Ninja | 1.11.1 |
| OpenOCD | 0.12.0+dev-00645-g2306f32ee |
| RTOS Proxy | 0.18.0 |
| SEGGER J-Link | 9.24 |
| STARM-Clang | 21.1.1 |
| ST-LINKGDBServer | 7.13.0 |
| STLink Server | 2.1.2-1 (for MacOS installations)
2.1.1-2 (for others OS) |
| STM32CubeProgrammer | 2.22.0 |
If you have any questions or requests concerning this wiki, or if you see any pages with mistakes, report them using ST Support Center or ST Community MCU Forum.
All rights reserved © 2026 STMicroelectronics