1. Overview[edit source]
This first step explains how to unpack the STM32MP135x-DK Discovery kit and the additional equipment you need.
The following block diagram provides high-level information on how to connect them together.
2. Out-of-the-box kit[edit source]
3. Required equipment[edit source]
The following table lists the equipment required to start playing with your STM32MP135x-DK board.
Some of them are delivered within the STM32MP135x-DK Discovery kit. The others need to be purchased separately.
STM32MP135x-DK Discovery kit | Flexible development platform for STM32MP15 microprocessor devices | Delivered |
MicroSD card | To be populated with the OpenSTLinux Distribution (Linux software), and providing extra storage capacity. A 2-Gbyte minimum microSD card is required. |
Delivered |
USB Type-C™ to USB Type-C™ cable | Used to connect the STM32MP135x-DK Discovery kit to the power supply | Delivered |
Micro USB Type-B to USB Type-A cable | Used to connect the STM32MP135x-DK Discovery kit to the PC through the USB micro-B (ST-LINK/V2-1) |
Not delivered |
USB Type-C™ to USB Type-A cable | Used to connect the STM32MP135x-DK Discovery kit to a USB OTG device. | Not delivered |
5V/3A power supply | The power supply should be able to output 5V / 3A (15W) | Not delivered |
Laptop | A Linux PC running Ubuntu 16.04 is required. | Not delivered |
Ethernet cable (optional) | Used to connect the STM32MP135x-DK Discovery kit through ssh | Not delivered |
4. Connection[edit source]
- Connect your laptop to the board ST-LINK/V2-1 port through the micro USB Type-B to USB Type-A cable.
- Connect the USB Type-C™ to USB Type-C™ cable to the 5V/3A power supply.
- Connect your laptop to the board USB Type-C™ OTG port through the USB Type-C™ to USB Type-A cable.
- Optionally connect your Ethernet network to the board Ethernet port through the Ethernet cable.