Unpack the STM32MP257x-EV1 board

Revision as of 09:43, 13 September 2023 by Registered User

Applicable for STM32MP25x lines

STM32MP257F-EV1.jpg
Let's start Develop on Arm® Cortex®-A35
Step category in.png Unpack the board Step.png Populate the target and boot the image Step.png Execute basic commands Step.png Use the demo launcher Step category out.png


1. Overview[edit source]

This first step explains how to unpack the STM32MP257x-EV1 Evaluation board and the additional equipment you need.
The following block diagram provides high-level information on how to connect them together.

STM32MP1 connection block diagram

2. Out-of-the-box board[edit source]

STM32MP157x-EV1 back view
STM32MP157x-EV1 front view
STM32MP157x-EV1 with all delivered items

3. Required equipment[edit source]

The following table lists the equipment required to start playing with your STM32MP257x-EV1 board.
Some of them are delivered within the STM32MP257x-EV1 Evaluation board. The others need to be purchased separately.

STM32MP157x-EV1 Evaluation board Full-featured board for STM32MP15 microprocessor devices Delivered
MicroSD card To be populated with the OpenSTLinux Distribution (Linux software)
and providing extra storage capacity.
A 2-Gbyte minimum microSD card is needed
Delivered
5V/3A power supply The power supply should be able to output 5V / 3A (15W) Delivered
Micro USB Type-B to USB Type-A cable Used to connect the STM32MP157x-EV1 Evaluation board to the PC
through the USB micro-B (ST-LINK/V2-1)
Not delivered
Micro USB Type-B to USB Type-A cable Used to connect the STM32MP157x-EV1 Evautation board to an USB OTG device. Not delivered
Laptop A Linux PC running Ubuntu 16.04 is required. Not delivered
Ethernet cable (optional) Used to connect the STM32MP157x-EV1 Evaluation board through ssh Not delivered

4. Connection[edit source]

  • Connect your laptop to the board ST-LINK/V2-1 port through the micro USB Type-B to USB Type-A cable.
  • Connect the power supply.
  • Connect your laptop to the board USB Type-COTG port through the micro USB Type-B to USB Type-A.
  • Optionally connect your Ethernet network to the board Ethernet port through the Ethernet cable.
STM32MP157x-EV1 Evaluation board connection
  • Remove JP1 jumper and place JP4 and JP5 jumpers as shown below to enable debugging through ST-LINK/V2-1.
STM32MP157x-EV1 Jumper configuration
Info white.png Information
Press your fingers on the display to make sure it is correctly connected and screw the screws. The three LEDs located on the right side of the display should be green when the board is powered on.



Back button.png Overview button.png Next button.png