1. Overview[edit source]
This first stage explains the way to unpack the STM32MP157x-DK2 Discovery kit and the additional equipment you need.
The following block diagram provides high level information about how to connect them together.
![](/stm32mpu/nsfr_img_auth.php/e/e1/STM32MP1_connection_block_diagram.png)
STM32MP1 connection block diagram
2. Out of the box[edit source]
3. Equipment[edit source]
The following table lists the required equipment to start playing with your STM32MP157x-DK2 board.
Some of them are delivered with the STM32MP157x-DK2 Discovery kit. The other need to be purchased separately.
STM32MP157x-DK2 Discovery kit | Flexible development platform for the STM32MP15 microprocessor device | Delivered |
MicroSD card | To be populated with the OpenSTLinux Distribution (Linux software), and providing extra storage capacity. A 2-Gbyte minimum microSD card is needed |
Delivered |
USB Type-C™ to USB Type-C™ cable | Used to connect the STM32MP157x-DK2 Discovery kit to the power supply | Delivered |
Micro USB Type-B to USB Type-A cable | Used to connect the STM32MP157x-DK2 Discovery kit to the PC through the USB micro-B (ST-LINK/V2-1) |
Not delivered |
USB Type-C™ to USB Type-A cable | Used to connect the STM32MP157x-DK2 Discovery kit to an USB OTG device. | Not delivered |
Power Supply 5V/3A | The power supply should be able to output 5V / 3A (15W) | Not delivered |
Laptop | Assume a Linux PC running Ubuntu 16.04 | Not delivered |
Ethernet cable (optional) | Used to connect the STM32MP157x-DK2 Discovery kit through ssh | Not delivered |
4. Connection[edit source]
- Connect the micro USB Type-B to USB Type-A cable between your laptop and the ST-LINK/V2-1 port of the board
- Connect the USB Type-C™ to USB Type-C™ cable to the 5V/3A power supply
- Connect the USB Type-C™ to USB Type-A cable betweenn your laptop and the USB Type-C™ OTG port of the board
- Optionally connect the Ethernet cable between your Ethernet network and the Ethernet port of the board