Unpack the STM32MP257x-EV1 board

Revision as of 15:13, 17 November 2023 by Registered User (→‎Connection)

Applicable for STM32MP25x lines

STM32MP257F-EV1.jpg
Let's start Develop on Arm® Cortex®-A35
Step category in.png Unpack the board Step.png Populate the target and boot the image Step.png Execute basic commands Step.png Use the demo launcher Step category out.png


1. Overview[edit source]

This first step explains how to unpack the STM32MP257x-EV1 Evaluation board and the additional equipment you need.
The following block diagram provides high-level information on how to connect them together.

STM32MP2 connection block diagram


==Out-of-the-box board==

File:STM32MP257F-EV1 recto.jpg
STM32MP257F-EV1 front view
STM32MP257F-EV1 back view
File:STM32MP257F-EV1 delivered items.jpg
STM32MP257F-EV1 with all delivered items

2. Required equipment[edit source]

The following table lists the equipment required to start playing with your STM32MP257x-EV1 board.
Some of them are delivered within the STM32MP257x-EV1 Evaluation board. The others need to be purchased separately.

STM32MP257F-EV1 Evaluation board Full-featured board for STM32MP25 microprocessor devices Delivered
MicroSD card To be populated with the OpenSTLinux Distribution (Linux software)
and providing extra storage capacity.
A 2-Gbyte minimum microSD card is needed
Delivered
5V/3A power supply The power supply should be able to output 5V / 3A (15W) Delivered
USB Type-C cable Used to connect the STM32MP257F-EV1 Evaluation board to the PC
through the USB C (ST-LINK/V3)
Not delivered
USB Type-C to USB Type-A cable Used to connect the STM32MP257F-EV1 Evaluation board to an USB OTG device. Not delivered
Laptop A Linux PC running Ubuntu 22.04 is required. Not delivered
Ethernet cable (optional) Used to connect the STM32MP257F-EV1 Evaluation board through ssh (can be done with USB OTG) Not delivered

3. Connection[edit source]

  • Connect your laptop to the board ST-LINK/V3 port through the USB Type-C cable.
  • Connect the power supply.
  • Connect your laptop to the board USB Type-COTG port through the USB Type-C to USB Type-A.
  • Optionally connect your Ethernet network to the board Ethernet port through the Ethernet cable.
File:STM32MP257F-EV1 with power stlink flasher ethernet.jpg
STM32MP257F-EV1 Evaluation board connection
  • JP4 can be used to power up the board either with 5V supply (2-3 position, default) or through ST-LINK/V3-EC (1-2 position).
STM32MP157x-EV1 Jumper configuration
Info white.png Information
The LED located on the left side of the board should be green when the power is on.



Back button.png Overview button.png Next button.png