1. Overview[edit source]
This first step explains how to unpack the STM32MP157x-EV1 Evaluation board and the additional equipment you need.
The following block diagram provides high-level information on how to connect them together.
![](/stm32mpu/nsfr_img_auth.php/9/9d/STM32MP1_EV1_connection_block_diagram.png)
STM32MP1 connection block diagram
2. Out-of-the-box board[edit source]
3. Required equipment[edit source]
The following table lists the equipment required to start playing with your STM32MP157x-EV1 board.
Some of them are delivered within the STM32MP157x-EV1 Evaluation board. The others need to be purchased separately.
STM32MP157x-EV1 Evaluation board | Full-featured board for STM32MP15 microprocessor devices | Delivered |
MicroSD card | To be populated with the OpenSTLinux Distribution (Linux software) and providing extra storage capacity. A 2-Gbyte minimum microSD card is needed |
Delivered |
5V/3A power supply | The power supply should be able to output 5V / 3A (15W) | Delivered |
Micro USB Type-B to USB Type-A cable | Used to connect the STM32MP157x-EV1 Evaluation board to the PC through the USB micro-B (ST-LINK/V2-1) |
Not delivered |
Micro USB Type-B to USB Type-A cable | Used to connect the STM32MP157x-EV1 Evautation board to an USB OTG device. | Not delivered |
Laptop | A Linux PC running Ubuntu 16.04 is required. | Not delivered |
Ethernet cable (optional) | Used to connect the STM32MP157x-EV1 Evaluation board through ssh | Not delivered |
4. Connection[edit source]
- Connect your laptop to the board ST-LINK/V2-1 port through the micro USB Type-B to USB Type-A cable.
- Connect the power supply.
- Connect your laptop to the board USB Type-C™ OTG port through the micro USB Type-B to USB Type-A.
- Optionally connect the Ethernet cable between your Ethernet network and the Ethernet port of the board
- Remove JP1 jumper and place JP4 and JP5 jumpers as shown below to enable debugging through ST-LINK/V2-1.