1. Limitations
ID | Summary |
---|---|
Authentication issue | If you have encountered an authentication problem while using STM32CubeIDE, don't worry. You simply need to set your connection parameters. For more details see link below: https://community.st.com/t5/stm32-mcus/how-to-set-the-network-connection-parameters-for-stm32cubeide/ta-p/585694 |
133183 | Unable to debug using FreeRTOS aware with a J-LINK Ultra+ in STM32CubeIDE 1.10.1 |
138771 | To start debugging in the NS zone when the product status is TZ-Closed for the STM32H5 using ST-Link GDBServer, add the following script to "Run Commands" in the debugging configuration.
For the "Reset & Restart" button to work: - Add the same script - Select "None" as the type. |
143485 | Post build commands are restored by using one of the following two options :
restore the post-build command by applying a "code generation" change the default behavior of the command "restore Defaults". |
146043 | On STM32H745 Cortex-M4 Dual Core projects the pre-defined
breakpoint is maintained but not caught upon run |
152549 | From GCC11, the build can be in error with some functions:
_close, fstat, _getpid, _isatty, _kill, _lseek, _open, _read, _write, _gettimeofday It’s due to that a state is define using the system information. The application needs to define a way to track time. |
156539 | If the user needs to set a proxy to be authenticated, a check for connection should be done: Windows > Preferences > STM32Cube > Firmware Updater and then Check Connection. |
166245 | When using the STM32CubeMP13 bare-metal firmware and activating Azure® RTOS
ThreadX, the STM32CubeIDE linker file must contain the following section to avoid compilation issues:
|
171852 | The implemented toolchain is allocating to an enum type only as many bytes as it needs for the declared range of possible values. |
174727 | STM32CubeIDE cannot make the project build automatically after having changed the IP configuration, it cannot automatically control this configuration, the user needs to increase Flash size manually when needed depending on his configuration. |
189888 | For STM32WB05 et STM32WB09 devices the connection Under Reset type is not supported |
192219 | For cortex M55 (like STM32N6), GCC12 and earlier versions detect warning using OFast and O3 optimizations level.
Workaround:
|
198955 | STM32WB0x and STM32WBA5x products:
|
2. Fixed issues
ID | Summary |
---|---|
109764 | FreeRTOS™ kernel-aware debugging: Full stack traces off all tasks do not work if configUSE_PORT_OPTIMISED_TASK_SELECTION 1 |
158985 | “Connect Under Reset” is not working with STM32WBA |
176993 | Error on linker script for the STM32L412K8Tx MCU |
185617 | Due to an Eclipse issue, STM32CubeIDE on new Linux distribution such as Ubuntu 24.04 and Debian faced some performance issue linked to the limit value of allowed open files. |
189089 | Wrong range for TIMx ARR/CCR registers in STM32G474.svd |
191705 | For Mac OS, thread and queue names not displayed properly in STM32CubeIDE |
194595 | Typo in the popup of the "Do you want generate Code? |
3. Known issues
The known issues are split into general, STM32CubeCLT, OS-specific, and target-specific issues.
3.1. General issues
ID | Summary |
---|---|
59435 | Having a space or non-ASCII character in the project/workspace path or installation path is not fully supported. |
63624 | Some STM32CubeMX pop-up dialogs are not opened in front of the STM32CubeIDE workbench on all OS's. |
68184 | Hierarchical projects cannot be imported with the option Copy into workspace. |
68440 | Hierarchical projects cannot be renamed. |
89454 | Restart configuration only works for flash memory projects and not for RAM projects. Program Counter register is not set correctly. Manual work-around: In Restart configuration, manually set PC to the ResetHandler() in RAM: set $pc = 0x20000xxx. |
115928 | Editing live expressions while target is running does not work with SEGGER J-Link. |
124062- 152549 | GCC-10 is more strict with respect to declaration of global variables in header files. Read the GCC-10 porting guide, so many warnings and errors result. |
133183 | STM32CubeIDE cannot debug using FreeRTOS aware with J-LINK.
Work-arounds, if: Reset strategy == Connect under reset, requires Initialization commands:
Work-arounds, if: Reset strategy == None (attach mode), requires Initialization commands:
|
139637 | Creating new STM32Cube project inside STM32CubeIDE is not possible if ioc-editor is point at STM32CubeMX stand-alone |
156812 | Missing string table in Build Analyzer while showing the bytes of the size of the ".rodata" section . |
159507 | Issues detected when updating STM32CubeIDE version from 1.9.0 to 1.13.1. |
162500 | After programming a device in Run mode, STM32CubeIDE opens every time a new tab with startup file and give focus on that tab. |
169316 | When building an existing project, using GCC11 or GCC12, a warning should be noticed: “elf has a LOAD segment with RWX permissions”.
This warning highlights a vulnerability, to correct it and secure the data section, we suggest to update the linker files: From this kind of section:
To:
But it’s incompatible with GCC10 and earlier versions. |
170279 | Failure to compile embOS due to missing stack variable as a new section defining _stack_start__ and __stack_end__ in linker file need to be added in linker file once it is required by ThreadX. |
183033 | The restore default build configuration feature lost the build commands. |
189478 | On Ubuntu 22.04 while creating a new STM32 project, STM32CubeIDE stucks at MCU finder step. Issue can be avoided by starting STM32CubeIDE with "wayland" version, or start it with sudo mode. |
199067 | In STM32CubeIDE 1.17.0, Hex files are not generated, setting a post build command:
arm-none-eabi-objcopy -O ihex "project_name.elf" "project_name.hex" is required. |
197993 | In STM32CubeIDE 1.17.0, MP2 sources are not installable following project import steps, instead all update source need to be deactivated expect OpenSTLinux source first. |
200233 | Compilation error when using toolchain GCC 12.3 with CubeIDE 1.14.1.
As Workaround, I proposed to the customer to download GCC12 and load it from local by setting the toolchain
|
207337 | After updating the STM32CubeIDE from some versions to the patch 1.18.1 using the update site updater, the GUI of the integrated STM32CubeFinder and STM32CubeMX are the images of the old UI tools.
Workaround: reinstall STM32CubeIDE from the installer on st.com. |
3.2. OS-specific issues
3.2.1. Linux®
ID | Summary |
---|---|
139617 | The CAD view in the ioc-editor may not render. A restart of STM32CubeIDE is required. |
165338-
189478 |
Using Ubunto 22, the target selection doesn’t appear normally without sudo permission.
Workaround: start with sudo permission or start the wayland binary instead of STM32CubeIDE binary. |
175176 | Using the generic Linux installer, the libncurses must be installed independently. |
3.3. Target-specific issues
3.3.1. STM32G4
ID | Summary |
---|---|
194756 | Problem with project creation using STM32G411 with the 1.6.0 firmware.
Workaround: use the version 1.6.1 of the firmware. |
3.3.2. STM32H7
ID | Summary |
---|---|
73552 | Serial Wire Viewer configuration is not reset for STM32H7 devices on the next launch if it was terminated with record active when using ST-LINK GDB server. |
79658 | ST-LINK GDB server reports being suspended on address: 0x05F0001 when debugging STM32H7 dual-core devices and the core under debug goes to sleep. |
81763 | OpenOCD does not support debugging STM32H7 dual-core devices when the core under debug goes to sleep. |
175966 | H7RS project on Ubuntu with ExtMemLoader context configured: Postbuild commands cannot be passed successfully when STM32CubeIDE is installed with sudo.
Workarounds:
|
202605 | For the STM32H7Rx/7Sx microcontrollers in the STM32H7 series and when activating TRACER_EMB, the NONCACHEABLE region size in the linker file need to be increased to fit TRACER buffer.
To add into the section: __RAM_NONCACHEABLEBUFFER_SIZE = 0x400; |
3.3.3. STM32MP1
ID | Summary |
---|---|
73895 | Debugging in production mode requires a network connection. If STM32CubeIDE is configured to use a network proxy, then the IP address of the STM32MP1 board needs to be added to the "Proxy bypass" list. |
73896 | The synchronization check between the IP-address entered in launch configuration and the IP-address of the target does not abort the launch in case of mismatch. |
3.3.4. STM32N6
ID | Summary |
---|---|
192219 | GCC12 and earlier versions detect warning using OFast and O3 optimizations level.
Workaround:
|
3.3.5. STM32WB
ID | Summary |
---|---|
196779 | Issue with the import project using "B-WB1M-WPAN1-BLE_HR_p2pServer" example from Example Selector.
Workaround: import from file system using the menu "File -> Open Porject from file system" |
3.3.6. STM32WB0
ID | Summary |
---|---|
180379 | A false error could be detected on some BLE applications when is included some binary libraries.
The error should be: “missing .note.GNU-stack section implies executable stack” or “NOTE: This behaviour is deprecated and will be removed in a future version of the linker” Workaround: Use the linker option: -z noexecstack More information: https://lists.gnu.org/archive/html/info-gnu/2022-08/msg00002.html |
183143 | An Error seems to be found once the ThreadX Option is activated for WB05/WB07/WB09. |
189888 | For STM32WB0x devices the connection Under Reset type is not supported. |
198955 |
|
3.3.7. STM32WBA
ID | Summary |
---|---|
198955 |
|
4. Upgrades
ID | Summary |
---|---|
BusyBox | 1.31.0.st_20240131-1810 |
Eclipse and CDT | Eclipse 2024-09
CDT 11.6.1 |
GCC1 binaries | 13.3.rel1.20240926-1715 |
JRE | Adoptium® Temurin™ 21.0.3_9 and JavaFX 21.0.3 |
JxBrowser | 7.41.4 |
Make | 4.4.1_st_20231030-1220 |
OpenOCD | v0.12.0+dev-00608-gd8ed48fef |
RTOS Proxy | 0.17.0 |
SEGGER J-Link | V8.12c |
ST-LINKGDBServer | 7.10.0 |
STLink Server | 2.1.1-2 |
STM32CubeMX | 6.14.0 |
STM32CubeProgrammer | 2.19.0 |
STM32CubeIDE errata
If you have any question or request concerning this wiki or if you see some pages with some mistake, you can report them using ST Support Center or ST Community MCU Forum. All rights reserved (c) 2024 STMicroelectronics Privacy policy Manage cookies Terms of use