1. Introduction
LevelX is a library offering the wear leveling and bad block management features for flash memories. LevelX is not intended to provide FileSytem APIs but only, low-level API to read, write, erase sectors in flash memories. Combined with FileX, it allows seamlessly using NAND and NOR flash memories as media storage devices.
LevelX is designed in a modular way, that facilitates the support of any flash memory. In fact, LevelX requires a low-level driver interacting with the Flash memory to support the basic raw API, read blocks, write blocks, Erase blocks and check errors. These raw APIs are then logically combined to offer a more user-friendly high-level APIs. The main features offered by LevelX are:
- Data Read/Write
- Flash erase
- Flash defragmentation
- Wear leveling
- Error checks
Further details are available in the LevelX official documentation
2. STM32 Integration
LevelX is targeting, mainly, the following types of memories:
- NOR memories (SPI/QSPI/OSPI): this type of memories, is one of the key target devices. As it requires specific LevelX features (wear-leveling, bad block management) to store data efficiently.
- NAND flash memories: NAND memories are also impacted by wearing and block damage. Currently there isn't an STM32 board equipped with a NAND flash memory. A custom driver needs to be implemented by the user to support it.
- SRAM memories: it covers any MCU internal memory (DTCM, AXISRAM…). This is useful for fast prototyping and testing. Applications using this configuration are product-dependent. Thus, a specific care shall be dedicated to the memory configuration relative to each device.
2.1. Known Limitations
- NAND memory driver and example are not provided in STM32 packages as STM32 evaluation boards do not currently embed such memory.
More details are in the official LevelX official documentation
3. How To Use
LevelX shall be used alongside with FileX. Please refer to FileX page "How To Use" section for more details about how to use LevelX
LevelX requires low-level interfaces to support the above-mentioned HW devices:
- “lx_stm32_xxx_driver_template.c/stm32_lx_xxx_driver_template.h”: An empty interface, provided as skeleton that can be modified by the user to support a custom flash memory.
- “lx_stm32_*_driver.c”: LevelX driver patterns that are ready to use by the application. They are delivered as part of the LevelX source code. The drivers may differ between STM32 series depending on the supported features.
- “lx_stm32_*_driver_template.h”: A template configuration header file to tune the corresponding driver for specific STM32 MCU/Board. This file should be copied in the application source tree and renamed to “lx_stm32_*_driver.h” then customized according to the driver needs.
Configuration flags can be defined by user in the “xxx_driver_template.h” file. Below LevelX driver OCTO-SPI header template file as an example:
4. STM32 LevelX Applications
To be Updated.
STM32 Packages provide the following set of applications (supported applications list may differ between products and boards):
Application | Short Description |
---|---|
App1 | Description |
App2 | Description |
App3 | Description |