![]() |
Coming soon |
1. STM32CubeMX overview
STM32CubeMX is a graphical tool that allows a very easy configuration of STM32 microcontrollers and microprocessors, as well as the generation of the corresponding initialization C code for the Arm® Cortex®-M core or a partial Linux® Device Tree for Arm® Cortex®-A core), through a step-by-step process.
The first step consists in selecting the STMicroelectronics STM32 microcontroller or microprocessor that matches the required set of peripherals.
For microprocessors, the second step allows to configure the GPIOs and the clock setup for the whole system, and to interactively assign peripherals either to the Arm® Cortex®-M or to the Cortex®A world. Specific utilities, such as DDR configuration and tuning, make it easy to get started with STM32 microprocessors. For Cortex®-M core, the configuration includes additional steps that are exactly similar to those described for microcontrollers.
For microcontrollers and microprocessor Arm® Cortex®-M, the second step consists in configuring each required embedded software thanks to a pinout-conflict solver, a clock-tree setting helper, a power-consumption calculator, and an utility that configures the peripherals (such as GPIO or USART) and the middleware stacks (such as USB or TCP/IP).
Eventually the user launches the generation that matches the selected configuration choices. This step provides the initialization C code for the Arm® Cortex®-M, ready to be used within several development environments, or a partial Linux® device tree for the Arm® Cortex®-A.
STM32CubeMX is delivered within STM32Cube.
2. Getting started with STM32 and STM32CubeMX
STM32 and STM8 software development tools
Getting started with STM32CubeMX
How to build a “Blink LED” project from STM32CubeMX for ST/Atollic TrueSTUDIO® for STM32™
4. STMicroelectronics Resources
UM1718
STM32CubeMX for STM32 configuration and initialization C code generation
5. Examples
The area where FAE's, collab... can put examples (linked to Github)