Registered User mNo edit summary |
Registered User mNo edit summary |
||
(9 intermediate revisions by 2 users not shown) | |||
Line 1: | Line 1: | ||
=== Introduction === | === Introduction === | ||
LevelX is a library offering wear- | Azure<sup>®</sup> RTOS LevelX is a library offering wear-levelling and bad-block management features for Flash memories. | ||
LevelX is not intended to provide FileSytem APIs, but only low-level APIs to read, write, and erase sectors in Flash memories. Combined with FileX, it allows seamless use of NAND and NOR Flash memories as media storage devices. | LevelX is not intended to provide FileSytem APIs, but only low-level APIs to read, write, and erase sectors in Flash memories. Combined with FileX, it allows seamless use of NAND and NOR Flash memories as media storage devices. | ||
Line 10: | Line 10: | ||
* Flash erase | * Flash erase | ||
* Flash defragmentation | * Flash defragmentation | ||
* Wear | * Wear levelling | ||
* Error checks | * Error checks | ||
Line 17: | Line 17: | ||
=== STM32 Integration=== | === STM32 Integration=== | ||
LevelX mainly targets the following memory types: | LevelX mainly targets the following memory types: | ||
* '''NOR''' memories (SPI/ | * '''NOR''' Flash memories (SPI/Quad-SPI/Octo-SPI), making use of wear-levelling and bad-block management features | ||
* '''NAND''' memories, also making use of wear- | * '''NAND''' Flash memories, also making use of wear-levelling and bad-block management features | ||
* ''' | * '''SRAMs''': covering any MCU internal volatile memory (such as DTCM and AXI SRAM). This is useful specifically for fast prototyping and testing. | ||
Line 26: | Line 26: | ||
=== How to use === | === How to use === | ||
LevelX | LevelX must be used alongside with FileX. | ||
Please refer to the [[FILEX overview|FileX page]] "How To Use" section for more details about how to use LevelX | Please refer to the [[FILEX overview|FileX page]] "How To Use" section for more details about how to use LevelX | ||
LevelX requires low-level interfaces to support the above-mentioned | LevelX requires low-level interfaces to support the above-mentioned hardware devices: | ||
* '''''lx_stm32_xxx_driver_template.c/stm32_lx_xxx_driver_template.h''''' An empty interface, provided as skeleton that can be modified by the user to support a custom Flash memory. | * '''''lx_stm32_xxx_driver_template.c/stm32_lx_xxx_driver_template.h''''': An empty interface, provided as skeleton that can be modified by the user to support a custom Flash memory. | ||
* '''''lx_stm32_*_driver.c''''': LevelX driver patterns that are ready to use by the application. They are delivered as part of the LevelX source code. The drivers may differ between STM32 | * '''''lx_stm32_*_driver.c''''': LevelX driver patterns that are ready to use by the application. They are delivered as part of the LevelX source code. The drivers may differ between STM32 Series depending on the supported features. | ||
* '''''lx_stm32_*_driver_template.h''''': A template configuration header file to tune the corresponding driver for specific STM32 MCU/board. This file should be copied to the application source tree and renamed to “lx_stm32_*_driver.h”, then customized according to the driver needs. | * '''''lx_stm32_*_driver_template.h''''': A template configuration header file to tune the corresponding driver for specific STM32 MCU/board. This file should be copied to the application source tree and renamed to “lx_stm32_*_driver.h”, then customized according to the driver needs. | ||
Line 39: | Line 39: | ||
[[File:LevelX LowLayer.png|frameless|center|LevelX LowLayer]] | [[File:LevelX LowLayer.png|frameless|center|LevelX LowLayer]] | ||
Configuration flags can be defined by the user in the “xxx_driver_template.h” file. The LevelX driver | Configuration flags can be defined by the user in the “xxx_driver_template.h” file. The LevelX driver Octo-SPI header template file below is an example: | ||
<syntaxhighlight lang="c"> | <syntaxhighlight lang="c"> | ||
Line 55: | Line 55: | ||
/* Exported types ------------------------------------------------------------*/ | /* Exported types ------------------------------------------------------------*/ | ||
/* Exported constants --------------------------------------------------------*/ | /* Exported constants --------------------------------------------------------*/ | ||
/* the | /* the Quad-SPI instance ,default value set to 0 */ | ||
#define QSPI_INSTANCE 0 | #define QSPI_INSTANCE 0 | ||
#define DEFAULT_BLOCK_SIZE (4 * 1024) | #define DEFAULT_BLOCK_SIZE (4 * 1024) | ||
/* when set to 1, the | /* when set to 1, the Quad-SPI init is done by the driver, otherwise it is up to the application to intialize it */ | ||
#define LX_DRIVER_CALLS_QSPI_INIT 1 | #define LX_DRIVER_CALLS_QSPI_INIT 1 | ||
#if (LX_DRIVER_CALLS_QSPI_INIT == 1) | #if (LX_DRIVER_CALLS_QSPI_INIT == 1) | ||
/* allow the driver to fully erase the | /* allow the driver to fully erase the Quad-SPI chip. This should be used carefully. | ||
* the call is blocking and takes a while. by default it is set to 0. | * the call is blocking and takes a while. by default it is set to 0. | ||
* When creating a fresh file system on the NOR Flash this flag should be enabled. | * When creating a fresh file system on the NOR Flash this flag should be enabled. | ||
Line 96: | Line 96: | ||
<noinclude> | <noinclude> | ||
[[Category: | [[Category:STM32 middleware | 40]] | ||
{{ArticleBasedOnModel | Example tech domain article}} | {{ArticleBasedOnModel | Example tech domain article}} | ||
{{PublicationRequestId | 21118 | 2021-14-09 | To assign}} | |||
{{PublicationRequestId | 19008 | 2021-02-17 | Philip SAGE}} | {{PublicationRequestId | 19008 | 2021-02-17 | Philip SAGE}} | ||
</noinclude> | </noinclude> |
Latest revision as of 13:54, 7 June 2022
1. Introduction
Azure® RTOS LevelX is a library offering wear-levelling and bad-block management features for Flash memories. LevelX is not intended to provide FileSytem APIs, but only low-level APIs to read, write, and erase sectors in Flash memories. Combined with FileX, it allows seamless use of NAND and NOR Flash memories as media storage devices.
LevelX is designed in a modular way that facilitates the support of any Flash memory. In fact, LevelX requires a low-level driver interacting with the Flash memory to support the basic raw API, read blocks, write blocks, erase blocks, and check errors. These raw APIs are then logically combined to offer more user-friendly high-level APIs. The main features offered by LevelX are:
- Data read/write
- Flash erase
- Flash defragmentation
- Wear levelling
- Error checks
Further details are available in the LevelX official documentation
2. STM32 Integration
LevelX mainly targets the following memory types:
- NOR Flash memories (SPI/Quad-SPI/Octo-SPI), making use of wear-levelling and bad-block management features
- NAND Flash memories, also making use of wear-levelling and bad-block management features
- SRAMs: covering any MCU internal volatile memory (such as DTCM and AXI SRAM). This is useful specifically for fast prototyping and testing.
2.1. Known limitations
- No known limitations so far. More details are in the official LevelX official documentation
3. How to use
LevelX must be used alongside with FileX. Please refer to the FileX page "How To Use" section for more details about how to use LevelX
LevelX requires low-level interfaces to support the above-mentioned hardware devices:
- lx_stm32_xxx_driver_template.c/stm32_lx_xxx_driver_template.h: An empty interface, provided as skeleton that can be modified by the user to support a custom Flash memory.
- lx_stm32_*_driver.c: LevelX driver patterns that are ready to use by the application. They are delivered as part of the LevelX source code. The drivers may differ between STM32 Series depending on the supported features.
- lx_stm32_*_driver_template.h: A template configuration header file to tune the corresponding driver for specific STM32 MCU/board. This file should be copied to the application source tree and renamed to “lx_stm32_*_driver.h”, then customized according to the driver needs.
Configuration flags can be defined by the user in the “xxx_driver_template.h” file. The LevelX driver Octo-SPI header template file below is an example:
#ifndef LX_STM32_QSPI_DRIVER_H
#define LX_STM32_QSPI_DRIVER_H
#ifdef __cplusplus
extern "C" {
#endif
/* Includes ------------------------------------------------------------------*/
#include "lx_api.h"
#include "stm32h747i_discovery_qspi.h"
/* Exported types ------------------------------------------------------------*/
/* Exported constants --------------------------------------------------------*/
/* the Quad-SPI instance ,default value set to 0 */
#define QSPI_INSTANCE 0
#define DEFAULT_BLOCK_SIZE (4 * 1024)
/* when set to 1, the Quad-SPI init is done by the driver, otherwise it is up to the application to intialize it */
#define LX_DRIVER_CALLS_QSPI_INIT 1
#if (LX_DRIVER_CALLS_QSPI_INIT == 1)
/* allow the driver to fully erase the Quad-SPI chip. This should be used carefully.
* the call is blocking and takes a while. by default it is set to 0.
* When creating a fresh file system on the NOR Flash this flag should be enabled.
*/
#define LX_DRIVER_ERASES_QSPI_AFTER_INIT 1
#endif
/* Exported macro ------------------------------------------------------------*/
/* Exported functions prototypes ---------------------------------------------*/
UINT lx_stm32_qspi_initialize(LX_NOR_FLASH *nor_flash);
/* Private defines -----------------------------------------------------------*/
#ifdef __cplusplus
}
#endif
#endif /* LX_STM32_QSPI_DRIVER_H */
4. STM32 LevelX applications
To be Updated.
STM32 Packages provide the following set of applications (the supported applications list may differ between products and boards):
Application | Short description |
---|---|
Fx_NAND_Write_Read_File | Demonstrates how to create a Fat File system on NAND Flash using FileX alongside LevelX. The application is designed to execute file operations on the Micron MT29F2G16ABAEAWP NAND Flash device, the code provides all the required software code to properly manage it. [readme] |