This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.This section gives an overview of Linux® kernel drivers (UPPERCASE in the figure) implemented for the STM32MP15 support, with their respective software frameworks (lowercase in the figure).
The components are grouped per functional domains.
Each Linux framework is further described in Linux operating system category articles.
Each STM32 MPU peripheral is introduced in peripherals overview articles.
Both those sections are reusing the same functional domain split.
The color code, explained in the legend, allows to see the code origin for each component.
![](/stm32mpu-ecosystem-v3/nsfr_img_auth.php/3/37/STM32MP15_Linux_kernel.png)
STM32MP15 Linux kernel overview
![OpenSTLinux BSP legend.png](/stm32mpu-ecosystem-v3/nsfr_img_auth.php/6/6a/OpenSTLinux_BSP_legend.png)